Difference between revisions of "Sysstat tool suite"

[quality revision] [unchecked revision]
Template:ArticleMainWriter

Template:ArticleApprovedVersion

1 Article purpose[edit]

This article provides the basic information needed to start using the sysstat[1] tool suite providing a collection of Linux tools:

  • main tools: iostat, mpstat and pidstat
  • others tools: sar, sadf

2 Introduction[edit]

The following table provides a brief description of the tool, as well as its availability depending on the software packages:

Yes: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.

No: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.

Under construction.png Coming soon
Tool STM32MPU Embedded Software distribution STM32MPU Embedded Software distribution for Android™
Name Category Purpose Starter Package Developer Package Distribution Package Starter Package Developer Package Distribution Package
sysstat Monitoring tools The sysstat [1] tool suite contains utilities to monitor the system performance and usage activity.

It contains various utilities, common to many commercial Unix distributions, as well as tools that can be scheduled (via a scheduler such as cron) to collect and historize performance and activity data:

  • iostat: reports CPU statistics and input/output statistics for block devices and partitions.
  • mpstat: reports individual or combined processor related statistics.
  • pidstat: reports statistics for Linux tasks (processes): I/O, CPU, memory, etc.
  • sar: collects, reports and saves system activity information (CPU, memory, disks, interrupts, network interfaces, TTY, kernel tables,etc.)
  • sadf: displays data collected by sar in multiple formats (CSV, XML, JSON, etc.). This command can also be used to exchange data with other programs or to draw graphs illustrating the various activities collected by sar using SVG (Scalable Vector Graphics) format.
Yes Yes Yes No No No

3 Installing the trace and debug tool on the target board[edit]

3.1 Using the STM32MPU Embedded Software distribution[edit]

The Sysstat tools are installed by default (/usr/bin/) and ready to be used with all STM32MPU OpenSTLinux Packages.

It is integrated in weston image distribution through meta-st package: meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb.

RDEPENDS_packagegroup-framework-tools-core = "\
   grep            \
   ...
   e2fsprogs       \
   e2fsprogs-resize2fs \
   sysstat         \
   minicom         \
   ...
   "
3.2 Using the STM32MPU Embedded Software distribution for Android™[edit]
Under construction.png Coming soon

4 Getting started[edit]

4.1 Using iostat[edit]

The iostat command is used for monitoring system input/output device loading by observing the time the devices are active in relation to their average transfer rates. The iostat command generates reports that can be used to change system configuration to better balance the input/output load between physical disks (Source: official website[2]).

/proc filesystem must be mounted for iostat to work. This is the case on STM32MPU Embedded Software.

  • Command line options. Please refer to manual page[2] for details.
 iostat --help
Usage: iostat [ options ] [ <interval> [ <count> ] ]
Options are:
[ -c ] [ -d ] [ -h ] [ -k | -m ] [ -N ] [ -s ] [ -t ] [ -V ] [ -x ] [ -y ] [ -z ]
[ -j { ID | LABEL | PATH | UUID | ... } ] [ --human ] [ -o JSON ]
[ [ -H ] -g <group_name> ] [ -p [ <device> [,...] | ALL ] ]
[ <device> [...] | ALL ]
  • Basic command to display a single history since boot report for all CPU and devices:
 iostat
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

avg-cpu:  %user   %nice %system %iowait  %steal   %idle
           0.11    0.00    0.60    0.05    0.00   99.25

Device             tps    kB_read/s    kB_wrtn/s    kB_read    kB_wrtn
mmcblk0           0.59         5.44         0.85      58539       9128
mmcblk1           0.03         0.31         0.00       3320          0
mmcblk1boot1      0.00         0.01         0.00        104          0
mmcblk1boot0      0.00         0.01         0.00        104          0

Note: by adding <interval> and <count> parameters, you can have a regular refresh during a given time interval:

 iostat <interval> <count>

  • Complex command to display statistics for block devices and all their partitions that are used by the system:
 iostat -N -p ALL
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

avg-cpu:  %user   %nice %system %iowait  %steal   %idle
          0.11    0.00    0.61    0.05    0.00   99.23

Device             tps    kB_read/s    kB_wrtn/s    kB_read    kB_wrtn
ram0              0.00         0.00         0.00          0          0
ram1              0.00         0.00         0.00          0          0
ram2              0.00         0.00         0.00          0          0
ram3              0.00         0.00         0.00          0          0
ram4              0.00         0.00         0.00          0          0
ram5              0.00         0.00         0.00          0          0
ram6              0.00         0.00         0.00          0          0
ram7              0.00         0.00         0.00          0          0
ram8              0.00         0.00         0.00          0          0
ram9              0.00         0.00         0.00          0          0
ram10             0.00         0.00         0.00          0          0
ram11             0.00         0.00         0.00          0          0
ram12             0.00         0.00         0.00          0          0
ram13             0.00         0.00         0.00          0          0
ram14             0.00         0.00         0.00          0          0
ram15             0.00         0.00         0.00          0          0
loop0             0.00         0.00         0.00          0          0
loop1             0.00         0.00         0.00          0          0
loop2             0.00         0.00         0.00          0          0
loop3             0.00         0.00         0.00          0          0
loop4             0.00         0.00         0.00          0          0
loop5             0.00         0.00         0.00          0          0
loop6             0.00         0.00         0.00          0          0
loop7             0.00         0.00         0.00          0          0
mtdblock0         0.00         0.00         0.00          0          0
mtdblock1         0.00         0.00         0.00          0          0
mtdblock2         0.00         0.00         0.00          0          0
mtdblock3         0.00         0.00         0.00          0          0
mtdblock4         0.00         0.00         0.00          0          0
mtdblock5         0.00         0.00         0.00          0          0
mtdblock6         0.00         0.00         0.00          0          0
mtdblock7         0.00         0.00         0.00          0          0
mmcblk0           0.66         6.02         0.94      58539       9128
mmcblk0p1         0.00         0.04         0.00        344          0
mmcblk0p2         0.00         0.02         0.00        220          0
mmcblk0p3         0.00         0.01         0.00         72          0
mmcblk0p4         0.03         0.21         0.00       2065          1
mmcblk0p5         0.60         5.46         0.94      53175       9126
mmcblk0p6         0.02         0.21         0.00       2087          1
mmcblk1           0.04         0.34         0.00       3320          0
mmcblk1p1         0.00         0.01         0.00         64          0
mmcblk1p2         0.00         0.00         0.00         44          0
mmcblk1p3         0.00         0.00         0.00         44          0
mmcblk1p4         0.01         0.11         0.00       1032          0
mmcblk1p5         0.01         0.11         0.00       1032          0
mmcblk1boot1      0.00         0.01         0.00        104          0
mmcblk1boot0      0.00         0.01         0.00        104          0

4.2 Using mpstat[edit]

The mpstat command writes to standard output activities for each available processor, processor 0 being the first one (Source: official website[3]).

  • Command line options. Please refer to manual page[3] for details.
 mpstat --help
Usage: mpstat [ options ] [ <interval> [ <count> ] ]
Options are:
[ -A ] [ -n ] [ -u ] [ -V ] [ -I { SUM | CPU | SCPU | ALL } ]
[ -N { <node_list> | ALL } ] [ -o JSON ] [ -P { <cpu_list> | ON | ALL } ]
  • Basic command to display three reports of global statistics for all processors at one second intervals:
 mpstat 1 3
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

15:45:26     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
15:45:27     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
15:45:28     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
15:45:29     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
Average:     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
  • Other command to display three reports of statistics for all processors at one second intervals:
 mpstat -P ALL 1 3
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

15:48:32     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
15:48:33     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
15:48:33       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
15:48:33       1    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00

15:48:33     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
15:48:34     all    0.00    0.00    0.50    0.00    0.00    0.00    0.00    0.00    0.00   99.50
15:48:34       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
15:48:34       1    0.00    0.00    0.99    0.00    0.00    0.00    0.00    0.00    0.00   99.01

15:48:34     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
15:48:35     all    0.00    0.00    0.50    0.00    0.00    0.00    0.00    0.00    0.00   99.50
15:48:35       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
15:48:35       1    0.00    0.00    0.99    0.00    0.00    0.00    0.00    0.00    0.00   99.01

Average:     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
Average:     all    0.00    0.00    0.33    0.00    0.00    0.00    0.00    0.00    0.00   99.67
Average:       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
Average:       1    0.00    0.00    0.66    0.00    0.00    0.00    0.00    0.00    0.00   99.34

4.3 Using pidstat[edit]

The pidstat command is used for monitoring individual tasks currently being managed by the Linux kernel (Source: official website[4]).

  • Command line options. Please refer to manual page[4] for details.
 pidstat --help
Usage: pidstat [ options ] [ <interval> [ <count> ] ]
Options are:
[ -d ] [ -h ] [ -I ] [ -l ] [ -R ] [ -r ] [ -s ] [ -t ] [ -U [ <username> ] ]
[ -u ] [ -V ] [ -v ] [ -w ] [ -C <command> ] [ -G <process_name> ] [ --human ]
[ -p { <pid> [,...] | SELF | ALL } ] [ -T { TASK | CHILD | ALL } ]
  • Basic command to display CPU statistic for all tasks:
 pidstat
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

15:58:48      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
15:58:48        0         1    0.03    0.12    0.00    0.05    0.14     0  systemd
15:58:48        0         2    0.00    0.00    0.00    0.00    0.00     1  kthreadd
15:58:48        0         7    0.00    0.01    0.00    0.01    0.01     0  ksoftirqd/0
15:58:48        0         8    0.04    0.00    0.00    0.02    0.04     1  rcu_preempt
15:58:48        0        15    0.00    0.01    0.00    0.00    0.01     1  ksoftirqd/1
15:58:48        0        18    0.00    0.00    0.00    0.00    0.00     1  kdevtmpfs
15:58:48        0        19    0.00    0.00    0.00    0.00    0.00     0  kworker/0:1
15:58:48        0        72    0.00    0.00    0.00    0.00    0.00     0  irq/82-mfx
15:58:48        0        77    0.00    0.06    0.00    0.01    0.06     1  mmcqd/0
15:58:48        0        83    0.00    0.00    0.00    0.00    0.00     0  mmcqd/1
15:58:48        0        85    0.00    0.00    0.00    0.00    0.00     0  mmcqd/1boot0
15:58:48        0        86    0.00    0.00    0.00    0.00    0.00     0  mmcqd/1boot1
15:58:48        0        91    0.00    0.63    0.00    0.00    0.63     0  kmemleak
15:58:48        0        93    0.00    0.00    0.00    0.00    0.00     0  kworker/0:3
15:58:48        0        95    0.00    0.01    0.00    0.00    0.01     1  irq/73-5a001000
15:58:48        0        98    0.00    0.00    0.00    0.00    0.00     0  kworker/0:1H
15:58:48        0        99    0.00    0.00    0.00    0.00    0.00     1  kworker/1:1H
15:58:48        0       100    0.00    0.00    0.00    0.00    0.00     0  jbd2/mmcblk0p5-
15:58:48        0       150    0.01    0.02    0.00    0.02    0.02     0  systemd-journal
15:58:48        0       189    0.01    0.01    0.00    0.03    0.01     1  systemd-udevd
15:58:48        0       201    0.00    0.00    0.00    0.00    0.00     0  kworker/u4:2
15:58:48      993       203    0.01    0.09    0.00    0.00    0.11     1  systemd-timesyn
15:58:48      998       273    0.09    0.04    0.00    0.02    0.14     0  avahi-daemon
15:58:48        0       276    0.00    0.00    0.00    0.00    0.00     1  systemd-logind
15:58:48        0       277    0.00    0.00    0.00    0.00    0.00     1  klogd
15:58:48      996       279    0.00    0.00    0.00    0.00    0.00     0  dbus-daemon
15:58:48        0       301    0.00    0.00    0.00    0.00    0.00     1  syslogd
15:58:48      992       312    0.00    0.00    0.00    0.00    0.00     1  systemd-network
15:58:48        0       314    0.00    0.00    0.00    0.00    0.00     0  weston-launch
15:58:48        0       319    0.01    0.01    0.00    0.00    0.01     1  weston
15:58:48      991       324    0.00    0.00    0.00    0.00    0.00     0  systemd-resolve
15:58:48        0       327    0.03    0.03    0.00    0.00    0.05     0  tcf-agent
15:58:48        0       332    0.00    0.00    0.00    0.00    0.00     1  login
15:58:48        0       333    0.00    0.00    0.00    0.00    0.00     0  agetty
15:58:48      997       334    0.00    0.00    0.00    0.00    0.00     1  named
15:58:48        0       340    0.00    0.00    0.00    0.00    0.00     0  weston-keyboard
15:58:48        0       342    0.01    0.00    0.00    0.00    0.01     0  weston-desktop-
15:58:48        0       345    0.00    0.01    0.00    0.00    0.01     1  systemd
15:58:48        0       350    0.00    0.00    0.00    0.00    0.00     0  sh
15:58:48        0       374    0.02    0.00    0.00    0.00    0.02     1  kworker/1:1
15:58:48        0       420    0.00    0.00    0.00    0.00    0.00     1  kworker/1:0
15:58:48        0       423    0.00    0.00    0.00    0.00    0.00     1  kworker/1:2
15:58:48        0       424    0.00    0.00    0.00    0.00    0.00     1  pidstat
  • Basic command to display 3 reports of CPU statistics for every active task in the system at one second intervals.:
 pidstat 1 3
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

15:59:56      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
15:59:57        0       426    3.67    4.59    0.00    0.00    8.26     1  pidstat

15:59:57      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
15:59:58        0       426    0.99    6.93    0.00    0.00    7.92     1  pidstat

15:59:58      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
15:59:59        0        15    0.00    0.99    0.00    0.00    0.99     1  ksoftirqd/1
15:59:59        0       426    1.98    5.94    0.00    0.99    7.92     1  pidstat

Average:      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
Average:        0        15    0.00    0.32    0.00    0.00    0.32     -  ksoftirqd/1
Average:        0       426    2.25    5.79    0.00    0.32    8.04     -  pidstat
  • Basic command to report statistics for a specific process with all associated threads:
 pidstat -t -p `pidof weston-launch`
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

16:00:59      UID      TGID       TID    %usr %system  %guest   %wait    %CPU   CPU  Command
16:00:59        0       314         -    0.00    0.00    0.00    0.00    0.00     0  weston-launch
16:00:59        0         -       314    0.00    0.00    0.00    0.00    0.00     0  |__weston-launch

4.4 Using sar[edit]

The sar command collects, reports, or saves system activity information (Source: official website[5]).

  • Command line options. Please refer to manual page[5] for details.
 sar --help
Usage: sar [ options ] [ <interval> [ <count> ] ]
Options are:
[ -A ] [ -B ] [ -b ] [ -C ] [ -D ] [ -d ] [ -F [ MOUNT ] ] [ -H ] [ -h ]
[ -p ] [ -q ] [ -r [ ALL ] ] [ -S ] [ -t ] [ -u [ ALL ] ] [ -V ]
[ -v ] [ -W ] [ -w ] [ -y ] [ --human ] [ --sadc ]
[ -I { <int_list> | SUM | ALL } ] [ -P { <cpu_list> | ALL } ]
[ -m { <keyword> [,...] | ALL } ] [ -n { <keyword> [,...] | ALL } ]
[ -j { ID | LABEL | PATH | UUID | ... } ]
[ -f [ <filename> ] | -o [ <filename> ] | -[0-9]+ ]
[ -i <interval> ] [ -s [ <hh:mm[:ss]> ] ] [ -e [ <hh:mm[:ss]> ] ]

Main used options for activity report:

sar option Description
-u CPU utilization of ALL CPUs
-P CPU utilization of individual CPU or core
-r Statistics for memory utilization
-S Statistics for swap space utilization
-b Statistics for I/O and transfer rate
-F Statistics for currently mounted filesystems
-d Activities for individual Block Device I/O
-w Activities for task creation and system switching
-q Information about task run queue and load average
-n Statistics for network activities

4.4.1 Interactive mode[edit]

Two modes for using sar:

  • Interactive mode (detailed here): sar is launched by the user using a command line on the console
  • Non-interactive mode (detailed in To go further chapter): sar is launched by a script (/usr/lib/sa/sa1, which is part of sysstat tools suite) that can be managed by a scheduler daemon like cron[6]

Interactive mode is used as soon as [ <interval> [ <count> ] ] parameters are present, otherwise non-interactive mode is used. In interactive mode, the command is executed immediately by taking into account the values.

As example, for getting CPU utilization of ALL CPUs, 5 times every 3s:

 sar -u 3 5
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

12:30:20        CPU     %user     %nice   %system   %iowait    %steal     %idle
12:30:23        all      0.00      0.00      0.50      0.00      0.00     99.50
12:30:26        all      0.00      0.00      0.50      0.00      0.00     99.50
12:30:29        all      0.17      0.00      0.17      0.00      0.00     99.67
12:30:32        all      0.66      0.00      2.49      0.00      0.00     96.84
12:30:35        all      0.33      0.00      3.16      0.00      0.00     96.51
Average:        all      0.23      0.00      1.36      0.00      0.00     98.41

-o <filename> can be used to store information into a file in binary format, which cat be later read with sadf.

4.5 Using sadf[edit]

The sadf command is used for displaying the contents of data files created by the sar command (Source: official website[7]): sar in interactive mode by using -o option, or file created in non-interactive mode in /var/log/sa/ directory.

  • Command line options. Please refer to manual page[7] for details.
 sadf --help
Usage: sadf [ options ] [ <interval> [ <count> ] ] [ <datafile> | -[0-9]+ ]
Options are:
[ -C ] [ -c | -d | -g | -j | -p | -r | -x ] [ -H ] [ -h ] [ -T | -t | -U ] [ -V ]
[ -O <opts> [,...] ] [ -P { <cpu> [,...] | ALL } ]
[ -s [ <hh:mm[:ss]> ] ] [ -e [ <hh:mm[:ss]> ] ]
[ -- <sar_options> ]

Main used format for activity report:

sadf option Description
-d Print the contents of the data file in a format that can be easily ingested by a relational database system. The output consists of fields separated by a semicolon (i.e. MSExcel)
-g From v11.3.1
Print the contents of the data file in SVG (Scalable Vector Graphics) format.
Use the follwing syntax:
 sadf -g sar_datafile [ -- <sar_options> ] > output.svg
Take care about giving the right sar_options, i.e. when checking for memory utilization, "-- -r" have to be given in the command.
-j Print the contents of the data file in JSON (JavaScript Object Notation) format
-t Display timestamp in the original local time of the data file creator instead of UTC (Coordinated Universal Time)
-x Print the contents of the data file in XML format

5 To go further[edit]

5.1 Using sar non-interactive mode[edit]

In non-interactive mode a scheduler daemon is used to plan activity record.

Recommended environment is using cron[6] daemon and sysstat script /usr/lib/sa/sa1 present when the tool suite is installed. Please refer to sa1 web page[8] for detail.

cron is not installed by default, and is part of cronie yocto package to be integrated:

  • With the Distribution Package of the STM32MPU Embedded Software distribution (st-image-weston):
 echo 'IMAGE_INSTALL_append += "cronie"' >> meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend
Then rebuild the st-image-weston image.
  • With the Distribution Package of the STM32MPU Embedded Software distribution for Android™:
Under construction.png Coming soon

5.2 Format datas to be imported in MS-Excel[edit]

Example using sar command to get ALL CPUs usage, format datas into semicolumn text, then make a graph using MS-Excel:

  • Record CPUs usage data (10 iterations every 3-second interval)
 sar -u 3 10 -o test
Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

13:03:26        CPU     %user     %nice   %system   %iowait    %steal     %idle
13:03:29        all      4.82      0.00      3.16      0.66      0.00     91.36
13:03:32        all      3.82      0.00      3.49      0.00      0.00     92.69
13:03:35        all     18.77      0.00      7.81      5.81      0.00     67.61
13:03:38        all     11.96      0.00      4.98      0.00      0.00     83.06
13:03:41        all     36.21      0.00      8.97      0.00      0.00     54.82
13:03:44        all      1.50      0.00      1.66      0.83      0.00     96.01
13:03:47        all      1.00      0.00      1.83      1.33      0.00     95.85
13:03:50        all      9.63      0.00      4.82      0.00      0.00     85.55
13:03:53        all      3.49      0.00      5.32      0.00      0.00     91.20
13:03:56        all      4.15      0.00      4.98      4.65      0.00     86.21
Average:        all      9.53      0.00      4.70      1.33      0.00     84.44

File test is also created (binary format).

  • Create readable report format from test file, i.e. in semicolumn format, which can be imported in MSExcel graph:
 sadf -d test > test.cvs
 cat test.cvs
 # hostname;interval;timestamp;CPU;%user;%nice;%system;%iowait;%steal;%idle
 stm32mp1;3;2018-06-18 13:03:29 UTC;-1;4.82;0.00;3.16;0.66;0.00;91.36
 stm32mp1;3;2018-06-18 13:03:32 UTC;-1;3.82;0.00;3.49;0.00;0.00;92.69
 stm32mp1;3;2018-06-18 13:03:35 UTC;-1;18.77;0.00;7.81;5.81;0.00;67.61
 stm32mp1;3;2018-06-18 13:03:38 UTC;-1;11.96;0.00;4.98;0.00;0.00;83.06
 stm32mp1;3;2018-06-18 13:03:41 UTC;-1;36.21;0.00;8.97;0.00;0.00;54.82
 stm32mp1;3;2018-06-18 13:03:44 UTC;-1;1.50;0.00;1.66;0.83;0.00;96.01
 stm32mp1;3;2018-06-18 13:03:47 UTC;-1;1.00;0.00;1.83;1.33;0.00;95.85
 stm32mp1;3;2018-06-18 13:03:50 UTC;-1;9.63;0.00;4.82;0.00;0.00;85.55
 stm32mp1;3;2018-06-18 13:03:53 UTC;-1;3.49;0.00;5.32;0.00;0.00;91.20
 stm32mp1;3;2018-06-18 13:03:56 UTC;-1;4.15;0.00;4.98;4.65;0.00;86.21

Sadf cpugraph example.png

6 References[edit]

"External links"
Document link Document Type Description
sysstat documentation Standard Official webpage by Sebastien GODARD
sysstat tutorial User Guide Official webpage by Sebastien GODARD
sysstat git Sources Sysstat github


<noinclude>

{{ArticleBasedOnModel | [[Trace and debug tools article model]]}}
{{ArticleMainWriter | Jean-PhilippeR}}

{{ ArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT | No previous approved version  | BrunoB - 28Nov'18 - 9774 | 28Nov'18 }}

[[Category:Linux monitoring tools]]</noinclude>

== Article purpose ==
This article provides the basic information needed to start using the '''sysstat'''<ref name=sysstatpage/> tool suite providing a collection of Linux tools:
* main tools: '''iostat''', '''mpstat''' and '''pidstat'''
* others tools: '''sar''', '''sadf'''

== Introduction ==
{{:Trace_and_debug_tools_assignment_table_template}}<onlyinclude>

| [[Sysstat tool suite|sysstat]]
| [[:Category:Monitoring tools|Monitoring tools]]
| style="text-align:left;" | The '''sysstat''' <ref name=sysstatpage>http://sebastien.godard.pagesperso-orange.fr/</ref> tool suite contains utilities to monitor the system performance and usage activity.<br>

It contains various utilities, common to many commercial Unix distributions, as well as tools that can be scheduled (via a scheduler such as cron) to collect and historize performance and activity data:
* '''[[Sysstat_tool_suite#Using_iostat|iostat]]''': reports CPU statistics and input/output statistics for block devices and partitions.
* '''[[Sysstat_tool_suite#Using_mpstat|mpstat]]''': reports individual or combined processor related statistics.
* '''[[Sysstat_tool_suite#Using_pidstat|pidstat]]''': reports statistics for Linux tasks (processes): I/O, CPU, memory, etc. 
* '''[[Sysstat_tool_suite#Using_sar|sar]]''': collects, reports and saves system activity information (CPU, memory, disks, interrupts, network interfaces, TTY, kernel tables,etc.)
* '''[[Sysstat_tool_suite#Using_sadf|sadf]]''': displays data collected by sar in multiple formats (CSV, XML, JSON, etc.). This command can also be used to exchange data with other programs or to draw graphs illustrating the various activities collected by sar using SVG (Scalable Vector Graphics) format.
| {{Y}} || {{Y}} || {{Y}}
| colspan="3" | {{UnderConstruction}}
|{{N}} || {{N}} || {{N}}
|-</onlyinclude>

|}

== Installing the trace and debug tool on the target board ==
=== Using the STM32MPU Embedded Software distribution ===
The '''Sysstat tools''' are installed by default (/usr/bin/) and ready to be used with all STM32MPU OpenSTLinux Packages.

It is integrated in weston image distribution through meta-st package: ''meta-st/meta-st-openstlinux/recipes-st/packagegroups/packagegroup-framework-tools.bb''.
 RDEPENDS_packagegroup-framework-tools-core = "\
    grep            \
    ...
    e2fsprogs       \
    e2fsprogs-resize2fs \
    {{green|'''sysstat'''}}         \
    minicom         \
    ...
    "

=== Using the STM32MPU Embedded Software distribution for Android&trade; ===
{{UnderConstruction}}

==  Getting started ==

=== Using iostat ===
The '''iostat''' command is used for monitoring system input/output device loading by observing the time the devices are active in relation to their average transfer rates. The '''iostat''' command generates reports that can be used to change system configuration to better balance the input/output load between physical disks (''Source: official website<ref name=iostatpage>http://sebastien.godard.pagesperso-orange.fr/man_iostat.html</ref>'').

''/proc filesystem must be mounted for iostat to work. This is the case on STM32MPU Embedded Software.''

*Command line options. Please refer to manual page<ref name=iostatpage/> for details.
 {{Board$}} iostat --help
 Usage: iostat [ options ] [ <interval> [ <count> ] ]
 Options are:
 [ -c ] [ -d ] [ -h ] [ -k | -m ] [ -N ] [ -s ] [ -t ] [ -V ] [ -x ] [ -y ] [ -z ]
 [ -j { ID | LABEL | PATH | UUID | ... } ] [ --human ] [ -o JSON ]
 [ [ -H ] -g <group_name> ] [ -p [ <device> [,...] | ALL ] ]
 [ <device> [...] | ALL ]

*Basic command to display a single history since boot report for all CPU and devices:
 {{Board$}} iostat
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 avg-cpu:  %user   %nice %system %iowait  %steal   %idle
            0.11    0.00    0.60    0.05    0.00   99.25

 Device             tps    kB_read/s    kB_wrtn/s    kB_read    kB_wrtn
 mmcblk0           0.59         5.44         0.85      58539       9128
 mmcblk1           0.03         0.31         0.00       3320          0
 mmcblk1boot1      0.00         0.01         0.00        104          0
 mmcblk1boot0      0.00         0.01         0.00        104          0
Note: by adding {{orangeHighlightParam|''<interval>''}} and {{orangeHighlightParam|''<count>''}} parameters, you can have a regular refresh during a given time interval:
 {{Board$}} iostat {{orangeHighlightParam|''<interval>''}} {{orangeHighlightParam|''<count>''}}

*Complex command to display statistics for block devices and all their partitions that are used by the system:
 {{Board$}} iostat -N -p ALL
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 avg-cpu:  %user   %nice %system %iowait  %steal   %idle
           0.11    0.00    0.61    0.05    0.00   99.23

 Device             tps    kB_read/s    kB_wrtn/s    kB_read    kB_wrtn
 ram0              0.00         0.00         0.00          0          0
 ram1              0.00         0.00         0.00          0          0
 ram2              0.00         0.00         0.00          0          0
 ram3              0.00         0.00         0.00          0          0
 ram4              0.00         0.00         0.00          0          0
 ram5              0.00         0.00         0.00          0          0
 ram6              0.00         0.00         0.00          0          0
 ram7              0.00         0.00         0.00          0          0
 ram8              0.00         0.00         0.00          0          0
 ram9              0.00         0.00         0.00          0          0
 ram10             0.00         0.00         0.00          0          0
 ram11             0.00         0.00         0.00          0          0
 ram12             0.00         0.00         0.00          0          0
 ram13             0.00         0.00         0.00          0          0
 ram14             0.00         0.00         0.00          0          0
 ram15             0.00         0.00         0.00          0          0
 loop0             0.00         0.00         0.00          0          0
 loop1             0.00         0.00         0.00          0          0
 loop2             0.00         0.00         0.00          0          0
 loop3             0.00         0.00         0.00          0          0
 loop4             0.00         0.00         0.00          0          0
 loop5             0.00         0.00         0.00          0          0
 loop6             0.00         0.00         0.00          0          0
 loop7             0.00         0.00         0.00          0          0
 mtdblock0         0.00         0.00         0.00          0          0
 mtdblock1         0.00         0.00         0.00          0          0
 mtdblock2         0.00         0.00         0.00          0          0
 mtdblock3         0.00         0.00         0.00          0          0
 mtdblock4         0.00         0.00         0.00          0          0
 mtdblock5         0.00         0.00         0.00          0          0
 mtdblock6         0.00         0.00         0.00          0          0
 mtdblock7         0.00         0.00         0.00          0          0
 mmcblk0           0.66         6.02         0.94      58539       9128
 mmcblk0p1         0.00         0.04         0.00        344          0
 mmcblk0p2         0.00         0.02         0.00        220          0
 mmcblk0p3         0.00         0.01         0.00         72          0
 mmcblk0p4         0.03         0.21         0.00       2065          1
 mmcblk0p5         0.60         5.46         0.94      53175       9126
 mmcblk0p6         0.02         0.21         0.00       2087          1
 mmcblk1           0.04         0.34         0.00       3320          0
 mmcblk1p1         0.00         0.01         0.00         64          0
 mmcblk1p2         0.00         0.00         0.00         44          0
 mmcblk1p3         0.00         0.00         0.00         44          0
 mmcblk1p4         0.01         0.11         0.00       1032          0
 mmcblk1p5         0.01         0.11         0.00       1032          0
 mmcblk1boot1      0.00         0.01         0.00        104          0
 mmcblk1boot0      0.00         0.01         0.00        104          0

=== Using mpstat ===
The '''mpstat''' command writes to standard output activities for each available processor, processor 0 being the first one (''Source: official website<ref name=mpstatpage>http://sebastien.godard.pagesperso-orange.fr/man_mpstat.html</ref>'').

*Command line options. Please refer to manual page<ref name=mpstatpage/> for details.
 {{Board$}} mpstat --help
 Usage: mpstat [ options ] [ <interval> [ <count> ] ]
 Options are:
 [ -A ] [ -n ] [ -u ] [ -V ] [ -I { SUM | CPU | SCPU | ALL } ]
 [ -N { <node_list> | ALL } ] [ -o JSON ] [ -P { <cpu_list> | ON | ALL } ]

*Basic command to display three reports of global statistics for all processors at one second intervals:
 {{Board$}} mpstat 1 3
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 15:45:26     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
 15:45:27     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 15:45:28     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 15:45:29     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 Average:     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00

*Other command to display three reports of statistics for all processors at one second intervals:
 {{Board$}} mpstat -P ALL 1 3
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 15:48:32     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
 15:48:33     all    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 15:48:33       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 15:48:33       1    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00

 15:48:33     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
 15:48:34     all    0.00    0.00    0.50    0.00    0.00    0.00    0.00    0.00    0.00   99.50
 15:48:34       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 15:48:34       1    0.00    0.00    0.99    0.00    0.00    0.00    0.00    0.00    0.00   99.01

 15:48:34     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
 15:48:35     all    0.00    0.00    0.50    0.00    0.00    0.00    0.00    0.00    0.00   99.50
 15:48:35       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 15:48:35       1    0.00    0.00    0.99    0.00    0.00    0.00    0.00    0.00    0.00   99.01

 Average:     CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest  %gnice   %idle
 Average:     all    0.00    0.00    0.33    0.00    0.00    0.00    0.00    0.00    0.00   99.67
 Average:       0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
 Average:       1    0.00    0.00    0.66    0.00    0.00    0.00    0.00    0.00    0.00   99.34

=== Using pidstat ===
The '''pidstat''' command is used for monitoring individual tasks currently being managed by the Linux kernel (''Source: official website<ref name=pidstatpage>http://sebastien.godard.pagesperso-orange.fr/man_pidstat.html</ref>'').

*Command line options. Please refer to manual page<ref name=pidstatpage/> for details.
 {{Board$}} pidstat --help
 Usage: pidstat [ options ] [ <interval> [ <count> ] ]
 Options are:
 [ -d ] [ -h ] [ -I ] [ -l ] [ -R ] [ -r ] [ -s ] [ -t ] [ -U [ <username> ] ]
 [ -u ] [ -V ] [ -v ] [ -w ] [ -C <command> ] [ -G <process_name> ] [ --human ]
 [ -p { <pid> [,...] | SELF | ALL } ] [ -T { TASK | CHILD | ALL } ]

*Basic command to display CPU statistic for all tasks:
 {{Board$}} pidstat
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 15:58:48      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
 15:58:48        0         1    0.03    0.12    0.00    0.05    0.14     0  systemd
 15:58:48        0         2    0.00    0.00    0.00    0.00    0.00     1  kthreadd
 15:58:48        0         7    0.00    0.01    0.00    0.01    0.01     0  ksoftirqd/0
 15:58:48        0         8    0.04    0.00    0.00    0.02    0.04     1  rcu_preempt
 15:58:48        0        15    0.00    0.01    0.00    0.00    0.01     1  ksoftirqd/1
 15:58:48        0        18    0.00    0.00    0.00    0.00    0.00     1  kdevtmpfs
 15:58:48        0        19    0.00    0.00    0.00    0.00    0.00     0  kworker/0:1
 15:58:48        0        72    0.00    0.00    0.00    0.00    0.00     0  irq/82-mfx
 15:58:48        0        77    0.00    0.06    0.00    0.01    0.06     1  mmcqd/0
 15:58:48        0        83    0.00    0.00    0.00    0.00    0.00     0  mmcqd/1
 15:58:48        0        85    0.00    0.00    0.00    0.00    0.00     0  mmcqd/1boot0
 15:58:48        0        86    0.00    0.00    0.00    0.00    0.00     0  mmcqd/1boot1
 15:58:48        0        91    0.00    0.63    0.00    0.00    0.63     0  kmemleak
 15:58:48        0        93    0.00    0.00    0.00    0.00    0.00     0  kworker/0:3
 15:58:48        0        95    0.00    0.01    0.00    0.00    0.01     1  irq/73-5a001000
 15:58:48        0        98    0.00    0.00    0.00    0.00    0.00     0  kworker/0:1H
 15:58:48        0        99    0.00    0.00    0.00    0.00    0.00     1  kworker/1:1H
 15:58:48        0       100    0.00    0.00    0.00    0.00    0.00     0  jbd2/mmcblk0p5-
 15:58:48        0       150    0.01    0.02    0.00    0.02    0.02     0  systemd-journal
 15:58:48        0       189    0.01    0.01    0.00    0.03    0.01     1  systemd-udevd
 15:58:48        0       201    0.00    0.00    0.00    0.00    0.00     0  kworker/u4:2
 15:58:48      993       203    0.01    0.09    0.00    0.00    0.11     1  systemd-timesyn
 15:58:48      998       273    0.09    0.04    0.00    0.02    0.14     0  avahi-daemon
 15:58:48        0       276    0.00    0.00    0.00    0.00    0.00     1  systemd-logind
 15:58:48        0       277    0.00    0.00    0.00    0.00    0.00     1  klogd
 15:58:48      996       279    0.00    0.00    0.00    0.00    0.00     0  dbus-daemon
 15:58:48        0       301    0.00    0.00    0.00    0.00    0.00     1  syslogd
 15:58:48      992       312    0.00    0.00    0.00    0.00    0.00     1  systemd-network
 15:58:48        0       314    0.00    0.00    0.00    0.00    0.00     0  weston-launch
 15:58:48        0       319    0.01    0.01    0.00    0.00    0.01     1  weston
 15:58:48      991       324    0.00    0.00    0.00    0.00    0.00     0  systemd-resolve
 15:58:48        0       327    0.03    0.03    0.00    0.00    0.05     0  tcf-agent
 15:58:48        0       332    0.00    0.00    0.00    0.00    0.00     1  login
 15:58:48        0       333    0.00    0.00    0.00    0.00    0.00     0  agetty
 15:58:48      997       334    0.00    0.00    0.00    0.00    0.00     1  named
 15:58:48        0       340    0.00    0.00    0.00    0.00    0.00     0  weston-keyboard
 15:58:48        0       342    0.01    0.00    0.00    0.00    0.01     0  weston-desktop-
 15:58:48        0       345    0.00    0.01    0.00    0.00    0.01     1  systemd
 15:58:48        0       350    0.00    0.00    0.00    0.00    0.00     0  sh
 15:58:48        0       374    0.02    0.00    0.00    0.00    0.02     1  kworker/1:1
 15:58:48        0       420    0.00    0.00    0.00    0.00    0.00     1  kworker/1:0
 15:58:48        0       423    0.00    0.00    0.00    0.00    0.00     1  kworker/1:2
 15:58:48        0       424    0.00    0.00    0.00    0.00    0.00     1  pidstat

*Basic command to display 3 reports of CPU statistics for every active task in the system at one second intervals.:
 {{Board$}} pidstat 1 3
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 15:59:56      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
 15:59:57        0       426    3.67    4.59    0.00    0.00    8.26     1  pidstat

 15:59:57      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
 15:59:58        0       426    0.99    6.93    0.00    0.00    7.92     1  pidstat

 15:59:58      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
 15:59:59        0        15    0.00    0.99    0.00    0.00    0.99     1  ksoftirqd/1
 15:59:59        0       426    1.98    5.94    0.00    0.99    7.92     1  pidstat

 Average:      UID       PID    %usr %system  %guest   %wait    %CPU   CPU  Command
 Average:        0        15    0.00    0.32    0.00    0.00    0.32     -  ksoftirqd/1
 Average:        0       426    2.25    5.79    0.00    0.32    8.04     -  pidstat

*Basic command to report statistics for a specific process with all associated threads:
 {{Board$}} pidstat -t -p `pidof weston-launch`
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 16:00:59      UID      TGID       TID    %usr %system  %guest   %wait    %CPU   CPU  Command
 16:00:59        0       314         -    0.00    0.00    0.00    0.00    0.00     0  weston-launch
 16:00:59        0         -       314    0.00    0.00    0.00    0.00    0.00     0  |__weston-launch

=== Using sar ===
The '''sar''' command collects, reports, or saves system activity information (''Source: official website<ref name=sarpage>http://sebastien.godard.pagesperso-orange.fr/man_sar.html</ref>'').

*Command line options. Please refer to manual page<ref name=sarpage/> for details.
 {{Board$}} sar --help
 Usage: sar [ options ] [ <interval> [ <count> ] ]
 Options are:
 [ -A ] [ -B ] [ -b ] [ -C ] [ -D ] [ -d ] [ -F [ MOUNT ] ] [ -H ] [ -h ]
 [ -p ] [ -q ] [ -r [ ALL ] ] [ -S ] [ -t ] [ -u [ ALL ] ] [ -V ]
 [ -v ] [ -W ] [ -w ] [ -y ] [ --human ] [ --sadc ]
 [ -I { <int_list> | SUM | ALL } ] [ -P { <cpu_list> | ALL } ]
 [ -m { <keyword> [,...] | ALL } ] [ -n { <keyword> [,...] | ALL } ]
 [ -j { ID | LABEL | PATH | UUID | ... } ]
 [ -f [ <filename> ] | -o [ <filename> ] | -[0-9]+ ]
 [ -i <interval> ] [ -s [ <hh:mm[:ss]> ] ] [ -e [ <hh:mm[:ss]> ] ]

Main used options for activity report:
{|
!sar option
!Description
|-
| align=center | -u || CPU utilization of ALL CPUs
|-
| align=center | -P || CPU utilization of individual CPU or core
|-
| align=center | -r || Statistics for memory utilization
|-
| align=center | -S || Statistics for swap space utilization
|-
| align=center | -b || Statistics for I/O and transfer rate
|-
| align=center | -F || Statistics for currently mounted filesystems
|-
| align=center | -d || Activities for individual Block Device I/O
|-
| align=center | -w || Activities for task creation and system switching
|-
| align=center | -q || Information about task run queue and load average
|-
| align=center | -n || Statistics for network activities
|}

==== Interactive mode ====
Two modes for using '''sar''':
*<u>Interactive mode</u> (''detailed here''): '''sar''' is launched by the user using a command line on the console
*<u>Non-interactive mode</u> (''detailed in [[#To go further|To go further]] chapter''): '''sar''' is launched by a script (''/usr/lib/sa/sa1'', which is part of sysstat tools suite) that can be managed by a scheduler daemon like cron<ref name=cronwikipedia>https://en.wikipedia.org/wiki/Cron</ref>


Interactive mode is used as soon as {{orangeHighlightParam|''[ <interval> [ <count> ] ]''}} parameters are present, otherwise non-interactive mode is used. In interactive mode, the command is executed immediately by taking into account the values.

As example, for getting CPU utilization of ALL CPUs, 5 times every 3s:
 {{Board$}} sar -u 3 5
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 12:30:20        CPU     %user     %nice   %system   %iowait    %steal     %idle
 12:30:23        all      0.00      0.00      0.50      0.00      0.00     99.50
 12:30:26        all      0.00      0.00      0.50      0.00      0.00     99.50
 12:30:29        all      0.17      0.00      0.17      0.00      0.00     99.67
 12:30:32        all      0.66      0.00      2.49      0.00      0.00     96.84
 12:30:35        all      0.33      0.00      3.16      0.00      0.00     96.51
 Average:        all      0.23      0.00      1.36      0.00      0.00     98.41

{{orangeHighlightParam|''-o <filename>''}} can be used to store information into a file in binary format, which cat be later read with [[#Using sadf|sadf]].

=== Using sadf ===
The '''sadf''' command is used for displaying the contents of data files created by the sar command (''Source: official website<ref name=sadfpage>http://sebastien.godard.pagesperso-orange.fr/man_sadf.html</ref>''): sar in interactive mode by using {{orangeHighlightParam|''-o''}} option, or file created in non-interactive mode in ''/var/log/sa/'' directory.

*Command line options. Please refer to manual page<ref name=sadfpage/> for details.
 {{Board$}} sadf --help
 Usage: sadf [ options ] [ <interval> [ <count> ] ] [ <datafile> | -[0-9]+ ]
 Options are:
 [ -C ] [ -c | -d | -g | -j | -p | -r | -x ] [ -H ] [ -h ] [ -T | -t | -U ] [ -V ]
 [ -O <opts> [,...] ] [ -P { <cpu> [,...] | ALL } ]
 [ -s [ <hh:mm[:ss]> ] ] [ -e [ <hh:mm[:ss]> ] ]
 [ -- <sar_options> ]

Main used format for activity report:

{|
!sadf option
!Description
|-
| align=center | -d || Print the contents of the data file in a format that can be easily ingested by a relational database system. The output consists of fields separated by a semicolon (i.e. MSExcel)
|-
| align=center | -g || '''From v11.3.1'''<br/> Print the contents of the data file in SVG (Scalable Vector Graphics) format.<br/> Use the follwing syntax:
 {{Board$}} sadf -g {{orangeHighlightParam|''sar_datafile''}} [ -- <sar_options> ] > output.svg<br/>

 {{highlight|Take care about giving the right sar_options, i.e. when checking for memory utilization, "-- -r" have to be given in the command.}}
|-
| align=center | -j || Print the contents of the data file in JSON (JavaScript Object Notation) format
|-
| align=center | -t || Display timestamp in the original local time of the data file creator instead of UTC (Coordinated Universal Time)
|-
| align=center | -x || Print the contents of the data file in XML format
|}

== To go further ==
==== Using sar non-interactive mode ====
In non-interactive mode a scheduler daemon is used to plan activity record.

Recommended environment is using cron<ref name=cronwikipedia/> daemon and sysstat script ''/usr/lib/sa/sa1'' present when the tool suite is installed. Please refer to '''sa1''' web page<ref>http://sebastien.godard.pagesperso-orange.fr/man_sa1.html</ref> for detail.

{{highlight|cron is not installed by default}}, and is part of cronie yocto package to be integrated:
* With the Distribution Package of the STM32MPU Embedded Software distribution (''st-image-weston''):
 {{PC$}} echo 'IMAGE_INSTALL_append += "cronie"' >> meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bbappend
:Then [[STM32MP1_Distribution_Package#Building_the_OpenSTLinux_distribution|rebuild the st-image-weston image]].
* With the Distribution Package of the STM32MPU Embedded Software distribution for Android&trade;:
{{UnderConstruction}}

=== Format datas to be imported in MS-Excel ===
Example using sar command to get ALL CPUs usage, format datas into semicolumn text, then make a graph using MS-Excel:
*Record CPUs usage data (10 iterations every 3-second interval)
 {{Board$}} sar -u 3 10 -o test
 Linux 4.14.48 (stm32mp1) 	06/18/18 	_armv7l_	(2 CPU)

 13:03:26        CPU     %user     %nice   %system   %iowait    %steal     %idle
 13:03:29        all      4.82      0.00      3.16      0.66      0.00     91.36
 13:03:32        all      3.82      0.00      3.49      0.00      0.00     92.69
 13:03:35        all     18.77      0.00      7.81      5.81      0.00     67.61
 13:03:38        all     11.96      0.00      4.98      0.00      0.00     83.06
 13:03:41        all     36.21      0.00      8.97      0.00      0.00     54.82
 13:03:44        all      1.50      0.00      1.66      0.83      0.00     96.01
 13:03:47        all      1.00      0.00      1.83      1.33      0.00     95.85
 13:03:50        all      9.63      0.00      4.82      0.00      0.00     85.55
 13:03:53        all      3.49      0.00      5.32      0.00      0.00     91.20
 13:03:56        all      4.15      0.00      4.98      4.65      0.00     86.21
 Average:        all      9.53      0.00      4.70      1.33      0.00     84.44

File ''test'' is also created (binary format).

*Create readable report format from ''test'' file, i.e. in semicolumn format, which can be imported in MSExcel graph:
 {{Board$}} sadf -d test > test.cvs
 {{Board$}} cat test.cvs
  # hostname;interval;timestamp;CPU;%user;%nice;%system;%iowait;%steal;%idle
  stm32mp1;3;2018-06-18 13:03:29 UTC;-1;4.82;0.00;3.16;0.66;0.00;91.36
  stm32mp1;3;2018-06-18 13:03:32 UTC;-1;3.82;0.00;3.49;0.00;0.00;92.69
  stm32mp1;3;2018-06-18 13:03:35 UTC;-1;18.77;0.00;7.81;5.81;0.00;67.61
  stm32mp1;3;2018-06-18 13:03:38 UTC;-1;11.96;0.00;4.98;0.00;0.00;83.06
  stm32mp1;3;2018-06-18 13:03:41 UTC;-1;36.21;0.00;8.97;0.00;0.00;54.82
  stm32mp1;3;2018-06-18 13:03:44 UTC;-1;1.50;0.00;1.66;0.83;0.00;96.01
  stm32mp1;3;2018-06-18 13:03:47 UTC;-1;1.00;0.00;1.83;1.33;0.00;95.85
  stm32mp1;3;2018-06-18 13:03:50 UTC;-1;9.63;0.00;4.82;0.00;0.00;85.55
  stm32mp1;3;2018-06-18 13:03:53 UTC;-1;3.49;0.00;5.32;0.00;0.00;91.20
  stm32mp1;3;2018-06-18 13:03:56 UTC;-1;4.15;0.00;4.98;4.65;0.00;86.21

[[File:Sadf_cpugraph_example.png|600px|link=]]

== References ==<references />


{|
|+ "External links"
|-
! scope=col | Document link
! scope=col | Document Type
! scope=col | Description
|-
| [http://sebastien.godard.pagesperso-orange.fr/documentation.html sysstat documentation]
| Standard
| Official webpage by Sebastien GODARD
|-
| [http://sebastien.godard.pagesperso-orange.fr/tutorial.html sysstat tutorial]
| User Guide
| Official webpage by Sebastien GODARD
|-
| [https://github.com/sysstat/sysstat sysstat git]
| Sources
| Sysstat github
|}


{{ ArticleBasedOnModel | Trace and debug tools article model }}
{{ PublicationRequestId | 9774 | 28Nov'18 }}

[[Category:Linux monitoring tools]]
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Trace and debug tools article model]]}}
 
{{ArticleMainWriter | Jean-PhilippeR}}
 
 
{{ ArticleApprovedVersion | Jean-PhilippeR | Jean-ChristopheT | No previous approved version  | BrunoB - 28Nov'18 - 9774 | 28Nov'18 }}
 
 
[[Category:Linux monitoring tools]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
 
This article provides the basic information needed to start using the '''sysstat'''<ref name=sysstatpage/> tool suite providing a collection of Linux tools:
 
This article provides the basic information needed to start using the '''sysstat'''<ref name=sysstatpage/> tool suite providing a collection of Linux tools:
Line 26: Line 17:
 
* '''[[Sysstat_tool_suite#Using_sadf|sadf]]''': displays data collected by sar in multiple formats (CSV, XML, JSON, etc.). This command can also be used to exchange data with other programs or to draw graphs illustrating the various activities collected by sar using SVG (Scalable Vector Graphics) format.
 
* '''[[Sysstat_tool_suite#Using_sadf|sadf]]''': displays data collected by sar in multiple formats (CSV, XML, JSON, etc.). This command can also be used to exchange data with other programs or to draw graphs illustrating the various activities collected by sar using SVG (Scalable Vector Graphics) format.
 
| {{Y}} || {{Y}} || {{Y}}
 
| {{Y}} || {{Y}} || {{Y}}
| colspan="3" | {{UnderConstruction}}
+
| {{N}} || {{N}} || {{N}}
 
|-
 
|-
 
</onlyinclude>
 
</onlyinclude>
Line 45: Line 36:
 
     ...
 
     ...
 
     "
 
     "
 
=== Using the STM32MPU Embedded Software distribution for Android&trade; ===
 
{{UnderConstruction}}
 
   
 
== Getting started ==
 
== Getting started ==
Line 77: Line 65:
 
  mmcblk1boot1      0.00        0.01        0.00        104          0
 
  mmcblk1boot1      0.00        0.01        0.00        104          0
 
  mmcblk1boot0      0.00        0.01        0.00        104          0
 
  mmcblk1boot0      0.00        0.01        0.00        104          0
Note: by adding {{orange|''<interval>''}} and {{orange|''<count>''}} parameters, you can have a regular refresh during a given time interval:
+
Note: by adding {{HighlightParam|''<interval>''}} and {{HighlightParam|''<count>''}} parameters, you can have a regular refresh during a given time interval:
  {{Board$}} iostat {{orange|''<interval>''}} {{orange|''<count>''}}
+
  {{Board$}} iostat {{HighlightParam|''<interval>''}} {{HighlightParam|''<count>''}}
   
 
*Complex command to display statistics for block devices and all their partitions that are used by the system:
 
*Complex command to display statistics for block devices and all their partitions that are used by the system:
Line 313: Line 301:
 
*<u>Non-interactive mode</u> (''detailed in [[#To go further|To go further]] chapter''): '''sar''' is launched by a script (''/usr/lib/sa/sa1'', which is part of sysstat tools suite) that can be managed by a scheduler daemon like cron<ref name=cronwikipedia>https://en.wikipedia.org/wiki/Cron</ref>
 
*<u>Non-interactive mode</u> (''detailed in [[#To go further|To go further]] chapter''): '''sar''' is launched by a script (''/usr/lib/sa/sa1'', which is part of sysstat tools suite) that can be managed by a scheduler daemon like cron<ref name=cronwikipedia>https://en.wikipedia.org/wiki/Cron</ref>
   
Interactive mode is used as soon as {{orange|''[ <interval> [ <count> ] ]''}} parameters are present, otherwise non-interactive mode is used. In interactive mode, the command is executed immediately by taking into account the values.
+
Interactive mode is used as soon as {{HighlightParam|''[ <interval> [ <count> ] ]''}} parameters are present, otherwise non-interactive mode is used. In interactive mode, the command is executed immediately by taking into account the values.
   
 
As example, for getting CPU utilization of ALL CPUs, 5 times every 3s:
 
As example, for getting CPU utilization of ALL CPUs, 5 times every 3s:
Line 327: Line 315:
 
  Average:        all      0.23      0.00      1.36      0.00      0.00    98.41
 
  Average:        all      0.23      0.00      1.36      0.00      0.00    98.41
   
{{orange|''-o <filename>''}} can be used to store information into a file in binary format, which cat be later read with [[#Using sadf|sadf]].
+
{{HighlightParam|''-o <filename>''}} can be used to store information into a file in binary format, which cat be later read with [[#Using sadf|sadf]].
   
 
=== Using sadf ===
 
=== Using sadf ===
The '''sadf''' command is used for displaying the contents of data files created by the sar command (''Source: official website<ref name=sadfpage>http://sebastien.godard.pagesperso-orange.fr/man_sadf.html</ref>''): sar in interactive mode by using {{orange|''-o''}} option, or file created in non-interactive mode in ''/var/log/sa/'' directory.
+
The '''sadf''' command is used for displaying the contents of data files created by the sar command (''Source: official website<ref name=sadfpage>http://sebastien.godard.pagesperso-orange.fr/man_sadf.html</ref>''): sar in interactive mode by using {{HighlightParam|''-o''}} option, or file created in non-interactive mode in ''/var/log/sa/'' directory.
   
 
*Command line options. Please refer to manual page<ref name=sadfpage/> for details.
 
*Command line options. Please refer to manual page<ref name=sadfpage/> for details.
Line 350: Line 338:
 
|-
 
|-
 
| align=center | -g || '''From v11.3.1'''<br/> Print the contents of the data file in SVG (Scalable Vector Graphics) format.<br/> Use the follwing syntax:
 
| align=center | -g || '''From v11.3.1'''<br/> Print the contents of the data file in SVG (Scalable Vector Graphics) format.<br/> Use the follwing syntax:
  {{Board$}} sadf -g {{orange|''sar_datafile''}} [ -- <sar_options> ] > output.svg<br/>
+
  {{Board$}} sadf -g {{HighlightParam|''sar_datafile''}} [ -- <sar_options> ] > output.svg<br/>
 
  {{highlight|Take care about giving the right sar_options, i.e. when checking for memory utilization, "-- -r" have to be given in the command.}}
 
  {{highlight|Take care about giving the right sar_options, i.e. when checking for memory utilization, "-- -r" have to be given in the command.}}
 
|-
 
|-
Line 433: Line 421:
 
| Sysstat github
 
| Sysstat github
 
|}
 
|}
  +
  +
{{ ArticleBasedOnModel | Trace and debug tools article model }}
  +
{{ PublicationRequestId | 9774 | 28Nov'18 }}
  +
  +
[[Category:Linux monitoring tools]]