Template:ArticleApprovedVersion
1 Article purpose[edit source]
This article provides the basic information needed to start using the Linux kernel tool: sysprof[1].
2 Introduction[edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||||
---|---|---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package | ||
sysprof | Monitoring tools | sysprof[1] is a statistical, system-wide profiler for Linux. It helps in finding the functions in which a program spends most of its time. sysprof proposes a user interface available directly on the board display screen. |
|
3 Installing the trace and debug tool on your target board[edit source]
3.1 Using STM32MPU Embedded Software distribution[edit source]
sysprof is installed by default and ready to be used with all STM32MPU Embedded Software Packages.
which sysprof /usr/bin/sysprof
sysprof is integrated in weston image distribution through openembedded-core package: openembedded-core/meta/recipes-core/packagegroups/packagegroup-core-tools-profile.bb.
PROFILE_TOOLS_X = "${@bb.utils.contains('DISTRO_FEATURES', 'x11', 'sysprof', , d)}" ... RRECOMMENDS_${PN} = "\ ${PERF} \ trace-cmd \ blktrace \ ${PROFILE_TOOLS_X} \ ${PROFILE_TOOLS_SYSTEMD} \ "
3.2 Using STM32MPU Embedded Software distribution for Android™[edit source]
Coming soon |
4 Getting started[edit source]
- Starting sysprof on the board:
sysprof
- Sysprof proposes a User interface through the board X interface to the display. It might be more convenient to plug a mouse (and optionally a keyboard) to use the tool interface.
- Recording
- Clicking on the top left Record button launches the recording. Recording is stopped by clicking on the top left Stop button (that replaces the record button).
- The following report is then available on the board display:
5 To go further[edit source]
Several options are available to the user in order to filter the report, and then study the results:
- Possibility to browse on Functions list, Descendants list
- Possibility to select a certain period of the CPUs graph.
- Possibility to save traces, to make screen shots...
6 References[edit source]
- Useful external links
Document link | Document Type | Description |
---|---|---|
Sysprof from Gnome | Standard | Wiki page |
Profiling using Sysprof | User manual | Linux.com |