Registered User mNo edit summary |
Registered User (''e''•MMC) |
||
Line 65: | Line 65: | ||
* {{Highlight|'P'}} : '''Program the partition or the device''' | * {{Highlight|'P'}} : '''Program the partition or the device''' | ||
:[[U-Boot overview|U-Boot]] requests the binary to [[STM32CubeProgrammer]] and programs the partition or the Flash device. | :[[U-Boot overview|U-Boot]] requests the binary to [[STM32CubeProgrammer]] and programs the partition or the Flash device. | ||
:On block devices (SD card or | :On block devices (SD card or ''e''•MMC), the GPT partitioning is performed if all partitions of the device are selected with 'P'. | ||
:For the 'P' option, two optional modifiers can be added: | :For the 'P' option, two optional modifiers can be added: | ||
:* {{Highlight|'E'}} : '''Empty partition or device''', update is not requested (associated [[#Field2: Id |"Id"]] is skipped) | :* {{Highlight|'E'}} : '''Empty partition or device''', update is not requested (associated [[#Field2: Id |"Id"]] is skipped) | ||
Line 166: | Line 166: | ||
Name of the alternate setting of the USB DFU<ref>https://en.wikipedia.org/wiki/USB#Device_Firmware_Upgrade</ref> for U-Boot enumeration. This is a string descriptor that indicates the target memory segment (see ''Interface Descriptor'' in DFU spec <ref>http://www.usb.org/developers/docs/devclass_docs/DFU_1.1.pdf Universal Serial Bus Device Class Specification for Device Firmware Upgrade, Version 1.1</ref><ref>https://web.archive.org/web/20141011015811/http://www.usb.org/developers/docs/devclass_docs/DFU_1.1.pdf Archived from the original on 11 October 2014</ref>). | Name of the alternate setting of the USB DFU<ref>https://en.wikipedia.org/wiki/USB#Device_Firmware_Upgrade</ref> for U-Boot enumeration. This is a string descriptor that indicates the target memory segment (see ''Interface Descriptor'' in DFU spec <ref>http://www.usb.org/developers/docs/devclass_docs/DFU_1.1.pdf Universal Serial Bus Device Class Specification for Device Firmware Upgrade, Version 1.1</ref><ref>https://web.archive.org/web/20141011015811/http://www.usb.org/developers/docs/devclass_docs/DFU_1.1.pdf Archived from the original on 11 October 2014</ref>). | ||
This is also the name of the [[#GPT partition of block device: SD card / | This is also the name of the [[#GPT partition of block device: SD card / ''e''•MMC]]. | ||
The requirements for the GPT partition names are: | The requirements for the GPT partition names are: | ||
* FSBL for SD card boot: the name must start with 'fsbl'= fsbl, fsbl1, fsbl2... (ROM code requirement) | * FSBL for SD card boot: the name must start with 'fsbl'= fsbl, fsbl1, fsbl2... (ROM code requirement) | ||
* SSBL for | * SSBL for ''e''•MMC/SD card boot: the name must be 'ssbl' ([[TF-A_overview|TF-A]] requirement) | ||
These two requirements are not verified by [[U-Boot overview|U-Boot]] during the flash programming. If they are not fulfilled, the ROM code or TF-A does not find the boot stage binary and the boot from Flash memory fails. | These two requirements are not verified by [[U-Boot overview|U-Boot]] during the flash programming. If they are not fulfilled, the ROM code or TF-A does not find the boot stage binary and the boot from Flash memory fails. | ||
Line 176: | Line 176: | ||
Type is only used in [[U-Boot overview|U-Boot]] to select the part of Flash memory to be updated: | Type is only used in [[U-Boot overview|U-Boot]] to select the part of Flash memory to be updated: | ||
* one partition | * one partition | ||
** [[#Block device GPT partition: SD card / | ** [[#Block device GPT partition: SD card / ''e''•MMC]] | ||
** [[#Raw Flash device (NAND/NOR Flash memories) MTD partition]] : see [[MTD overview]] | ** [[#Raw Flash device (NAND/NOR Flash memories) MTD partition]] : see [[MTD overview]] | ||
* all the [[#Hardware device]] = RAWImage | * all the [[#Hardware device]] = RAWImage | ||
Line 184: | Line 184: | ||
! !! colspan="2" | GPT !! colspan="2" | MTD | ! !! colspan="2" | GPT !! colspan="2" | MTD | ||
|- | |- | ||
! Type !! SD card !! | ! Type !! SD card !! ''e''•MMC !! NAND Flash memory !! NOR Flash memory | ||
|- | |- | ||
| Binary || x || x || x || x | | Binary || x || x || x || x | ||
Line 197: | Line 197: | ||
|} | |} | ||
==== Block device GPT partition: SD card / | ==== Block device GPT partition: SD card / ''e''•MMC ==== | ||
Refer to GPT standard for details <ref name="GPT">https://en.wikipedia.org/wiki/GUID_Partition_Table</ref>. | Refer to GPT standard for details <ref name="GPT">https://en.wikipedia.org/wiki/GUID_Partition_Table</ref>. | ||
Line 217: | Line 217: | ||
Export the associated device as one alternate setting by using Type='''RAWImage'''. | Export the associated device as one alternate setting by using Type='''RAWImage'''. | ||
* For SD card, NOR and NAND Flash memories: all the devices | * For SD card, NOR and NAND Flash memories: all the devices | ||
* For | * For ''e''•MMC: the user data area of ''e''•MMC (see [[#Field6: Offset]] for access to the boot area partitions) | ||
For RAWImage, Offset=0x0 and PartId >= 0x10 | For RAWImage, Offset=0x0 and PartId >= 0x10 | ||
Line 223: | Line 223: | ||
=== Field5: Device === | === Field5: Device === | ||
Select the targeted device and the instance (starting at 0) as defined by [[U-Boot overview|U-Boot]] device tree: | Select the targeted device and the instance (starting at 0) as defined by [[U-Boot overview|U-Boot]] device tree: | ||
* '''mmc + instance''' : 'mmc0'<br/>It is used for | * '''mmc + instance''' : 'mmc0'<br/>It is used for ''e''•MMC or SD card on SDMMC. In the below examples: | ||
** SD card = mmc0 (SDMMC1) | ** SD card = mmc0 (SDMMC1) | ||
** | ** ''e''•MMC = mmc1 (SDMMC2) | ||
* '''nor + instance''' : 'nor0'<br/>It is used for NOR on QUADSPI. | * '''nor + instance''' : 'nor0'<br/>It is used for NOR on QUADSPI. | ||
* '''nand + instance''' : 'nand0'<br/>It is used for parallel NAND Flash memories on FMC or serial NAND memories on QUADSPI. | * '''nand + instance''' : 'nand0'<br/>It is used for parallel NAND Flash memories on FMC or serial NAND memories on QUADSPI. | ||
Line 235: | Line 235: | ||
=== Field6: Offset === | === Field6: Offset === | ||
The supported values are: | The supported values are: | ||
* boot1: first boot area partition of | * boot1: first boot area partition of ''e''•MMC (offset is 0x0) | ||
* boot2: second boot area partition of | * boot2: second boot area partition of ''e''•MMC (offset is 0x0) | ||
* Offset in bytes: offset in Flash memory area (in the user data area for | * Offset in bytes: offset in Flash memory area (in the user data area for ''e''•MMC)<br/> | ||
Refer to [[#Partition sizes]] for offset constraints. | Refer to [[#Partition sizes]] for offset constraints. | ||
Line 248: | Line 248: | ||
=== GPT partuuid of rootfs partition === | === GPT partuuid of rootfs partition === | ||
If [[#Field3: Name]] = "rootfs" for block device (SD card / | If [[#Field3: Name]] = "rootfs" for block device (SD card / ''e''•MMC), U-Boot also sets a unique partition guid <ref name="GUID"/>(PARTUUID) for each instance: | ||
* mmc0: PARTUUID = "e91c4e10-16e6-4c0e-bd0e-77becf4a3582" | * mmc0: PARTUUID = "e91c4e10-16e6-4c0e-bd0e-77becf4a3582" | ||
* mmc1: PARTUUID = "491f6117-415d-4f53-88c9-6e0de54deac6" | * mmc1: PARTUUID = "491f6117-415d-4f53-88c9-6e0de54deac6" | ||
Line 292: | Line 292: | ||
All the partitions need to be present in the FlashLayout file, even if they are not selected or empty.<br/> | All the partitions need to be present in the FlashLayout file, even if they are not selected or empty.<br/> | ||
Then the offset and size of each partition are compared with: | Then the offset and size of each partition are compared with: | ||
* pre-existing GPT partitioning, for updates on block devices ( | * pre-existing GPT partitioning, for updates on block devices (''e''•MMC or SD card) | ||
* predefined partitioning for [[MTD_overview|MTD]] devices (NOR and NAND): see mtdparts environment variable in [[U-Boot overview|U-Boot]] for more information. | * predefined partitioning for [[MTD_overview|MTD]] devices (NOR and NAND): see mtdparts environment variable in [[U-Boot overview|U-Boot]] for more information. | ||
Line 301: | Line 301: | ||
Each GPT partition must be aligned to: | Each GPT partition must be aligned to: | ||
* 512 bytes (LBA) | * 512 bytes (LBA) | ||
* | * ''e''•MMC erase group size | ||
The first partition starts after 17 kbytes (default size of GPT header for 128 entries in U-Boot). | The first partition starts after 17 kbytes (default size of GPT header for 128 entries in U-Boot). | ||
Line 353: | Line 353: | ||
Warning: Start and end are indicated in mutiple of LBA (512 bytes by default). | Warning: Start and end are indicated in mutiple of LBA (512 bytes by default). | ||
To check the | To check the ''e''•MMC erase group size in U-Boot, select the mmc device (here 1) and use the command "mmc info" in U-Boot. | ||
{{Board$}} mmc dev 1 | {{Board$}} mmc dev 1 | ||
Line 553: | Line 553: | ||
|} | |} | ||
=== | === ''e''•MMC === | ||
[[TF-A_overview|TF-A]] copied in the two boot area partitions of | [[TF-A_overview|TF-A]] copied in the two boot area partitions of ''e''•MMC (hidden partition). | ||
GPT partitioning is used on the user area. [[U-Boot overview|U-Boot]] starts just after the GPT header at 17-Kbyte offset. | GPT partitioning is used on the user area. [[U-Boot overview|U-Boot]] starts just after the GPT header at 17-Kbyte offset. | ||
Line 716: | Line 716: | ||
|} | |} | ||
=== | === ''e''•MMC with TEE === | ||
{| class="wikitable" | {| class="wikitable" | ||
Line 957: | Line 957: | ||
|} | |} | ||
To erase all other devices, including the | To erase all other devices, including the ''e''•MMC boot partition, proceed as follows: | ||
{| class="wikitable" | {| class="wikitable" | ||
Line 1,005: | Line 1,005: | ||
Update SD card (mmc0 on SDMMC1). The GPT partition is created since all partitions are selected and Userfs is deleted and empty. | Update SD card (mmc0 on SDMMC1). The GPT partition is created since all partitions are selected and Userfs is deleted and empty. | ||
Erase all other devices, including | Erase all other devices, including ''e''•MMC hidden boot partition. | ||
{| class="wikitable" | {| class="wikitable" |
Revision as of 15:22, 10 October 2019
1. Article purpose[edit source]
This article describes the FlashLayout file format.
This file is used as an input by STM32CubeProgrammer tool in order to:
- define the Flash memory partitions (see STM32MP15_Flash_mapping)
- select the files used to boot (see Boot chains overview) and then populate each partition.
The embedded programming service processes this file on the device and interacts with STM32CubeProgrammer to update the Flash memory.
This is done by the stm32prog command in U-Boot. This command is automatically executed for USB boot. However you can launch it manually from the U-boot console.
The next chapter:
- describes the #FlashLayout file format and
- gives #Typical FlashLayout file for boot scenario without TEE and #Typical FlashLayout file with TEE
FSBL and SSBL definitions can be found in the Boot chains overview.
2. FlashLayout file format[edit source]
The FlashLayout is a text file with a tab-separated-value format (tsv). It includes the below elements:
- one line per partition or device
- seven columns, one for each field, provided in the following order:
The lines beginning with the '#' character are ignored and treated as comments.
The "Binary" last column is not used by U-Boot. It is used by STM32CubeProgrammer on the host computer to select the files to be sent to the target.
Several tabulations (<tab>) can be used to allow the correct column alignment in the editor. They are ignored by STM32CubeProgrammer and by U-Boot.
Empty fields are not allowed. The FlashLayout file format supports the 'none' reserved word.
2.1. Examples[edit source]
Below some valid FlashLayout files:
#opt Id Name Type Device Offset Binary
P 0x01 fsbl1 Binary mmc0 0x00004400 fsbl.stm32
P 0x02 fsbl2 Binary mmc0 0x00044400 fsbl.stm32
P 0x03 ssbl Binary mmc0 0x00084400 ssbl.stm32
P 0x10 bootfs System mmc0 0x00284400 bootfs.ext4.bin
P 0x11 rootfs FileSystem mmc0 0x08284400 rootfs.ext4.bin
PE 0x12 userfs FileSystem mmc0 0x28284400 none
Above, the first line contains only header information. This is not mandatory, as shown below:
- 0x01 fsbl_boot Binary none 0x0 fsbl.stm32
- 0x03 ssbl_boot Binary none 0x0 ssbl.stm32
P 0x32 sdcard RawImage mmc0 0x0 sdcard.bin
2.2. Field1: Options[edit source]
The Options field defines the operations to perform with a combination of characters: - P D E provided in any order;
First select the line of the FlashLayout with '-' or 'P':
- '-' : none option, the partition or the device is not modified (mandatory if #Field5: Device = none)
- 'P' : Program the partition or the device
- U-Boot requests the binary to STM32CubeProgrammer and programs the partition or the Flash device.
- On block devices (SD card or e•MMC), the GPT partitioning is performed if all partitions of the device are selected with 'P'.
- For the 'P' option, two optional modifiers can be added:
- 'E' : Empty partition or device, update is not requested (associated "Id" is skipped)
- 'D' : Delete partition or device
The only supported combinations are the following (with character in any order):
- '-' : no action
- 'P' : update = program the partition or the flash device
- 'PE' : do not update (also 'EP') : allow GPT partitioning with empty partition for block device but equivalent to '-' for RAW flash device
- 'PD' : delete and update (also 'DP')
- 'PDE' : delete and keep empty (also 'PED' / 'DPE' / 'DEP' / 'EPD' / 'EDP')
All other combinations are invalid.
2.3. Field2: Id[edit source]
Id identifies in a unique way the "download phase" requested by the device to STM32CubeProgrammer.
It is used by the embedded programming service to identify the next binary that is downloaded to the device:
- ROM code and FSBL: binary loaded in RAM
- SSBL (U-Boot): binary populated in Flash memory
The FlashLayout supported ranges are :
Range | Partition |
---|---|
0x01 to 0x0F | Boot partitions with STM32 header: SSBL, FSBL, other (TEE, Cortex-M4 firmware) |
0x10 to 0xF0 | user partitions programmed without header (uimage, dtb, rootfs, vendorfs, userfs) |
The Id 0x01 and 0x03 are reserved for FSBL and SSBL, respectively. They are loaded in RAM by ROM code and by FSBL.
2.3.1. Reserved Id[edit source]
The reserved values are the following:
Code | Partition |
---|---|
0x00 | FlashLayout (used internally, cannot be used in FlashLayout file) |
0x01 | FSBL (first copy) : used by ROM code (load in RAM) |
0x03 | SSBL : used by FSBL=TF-A (load in RAM) |
0xF1 to 0xFD | "virtual partition": used internally |
0xF1 | Command GetPhase |
0xF2 | OTP |
0xF3 | SSP |
0xF4 | PMIC NVM |
0xFE | End of operation |
0xFF | Reset |
2.3.2. Using Id for boot partition[edit source]
In normal use cases, the same FSBL and SSBL binaries are loaded in RAM and programmed in Flash memory. A simple mapping is used:
Code | Partition |
---|---|
0x01 (reserved) | FSBL (first copy) |
0x02 (default) | FSBL (second copy) |
0x03 (reserved) | SSBL |
However, in the FlashLayout file, any other Id lower than 0x10 (boot partition with STM32 header) can identify the FSBL and SSBL binaries to be programmed in Flash memory.
It enables having different binaries loaded in RAM and programed in Flash memory, for example when an updated feature is deactivated in the binaries to be programmed in Flash memory.
You can then use the boot partitions:
Code | Partition |
---|---|
0x01 (reserved) | FSBL to boot : load by ROM code |
0x03 (reserved) | SSBL to boot : loaded by FSBL |
0x02 | FSBL to program in Flash memory (first copy) |
0x04 | FSBL to program in Flash memory (second copy) |
0x05 | SSBL to program in Flash memory |
2.4. Field3: Name[edit source]
Name of the alternate setting of the USB DFU[1] for U-Boot enumeration. This is a string descriptor that indicates the target memory segment (see Interface Descriptor in DFU spec [2][3]).
This is also the name of the #GPT partition of block device: SD card / e•MMC.
The requirements for the GPT partition names are:
- FSBL for SD card boot: the name must start with 'fsbl'= fsbl, fsbl1, fsbl2... (ROM code requirement)
- SSBL for e•MMC/SD card boot: the name must be 'ssbl' (TF-A requirement)
These two requirements are not verified by U-Boot during the flash programming. If they are not fulfilled, the ROM code or TF-A does not find the boot stage binary and the boot from Flash memory fails.
2.5. Field4: Type[edit source]
Type is only used in U-Boot to select the part of Flash memory to be updated:
- one partition
- all the #Hardware device = RAWImage
The supported values are:
GPT | MTD | |||
---|---|---|---|---|
Type | SD card | e•MMC | NAND Flash memory | NOR Flash memory |
Binary | x | x | x | x |
Binary(N) | ssbl | |||
FileSystem | x | x | x | x |
System | x | x | UBI | UBI |
RAWImage | x | user data | x | x |
2.5.1. Block device GPT partition: SD card / e•MMC[edit source]
Refer to GPT standard for details [4].
The supported values, with associated partition type GUID (globally unique identifiers[5]), are:
- Binary : raw data / linux reserved
(GUID = 8DA63339-0007-60C0-C436-083AC8230908) - FileSystem : Linux filesystem data
(GUID = 0FC63DAF-8483-4772-8E79-3D69D8477DE4)
ext2/ext4/fat file system - System : FileSystem partition marked as bootable and used by U-Boot to find extlinux.conf configuration file (normally only one in the device, generic DISTRO feature)
For a Block device, the GPT header is updated only if all the partitions of this device are selected with the 'P' option (full update).
2.5.2. Raw Flash device (NAND/NOR Flash memories) MTD partition[edit source]
The supported values are:
- Binary: raw data, skip bad block (partition erase is not needed)
- Binary(N): raw data, skip bad block. The loaded binary is repeated N times.
It is only supported for NAND Flash memories. It is used to avoid disturbances during the first boot (uncorrectable ECC errors).
The first good block is read from NAND and duplicated N times in the same partition (write skip bad block). - FileSystem: unspecified File system, raw data
- System: normally UBI volume, U-Boot erases all the blocks following the last data in the MTD partition to avoid mount errors.
2.5.3. Hardware device[edit source]
Export the associated device as one alternate setting by using Type=RAWImage.
- For SD card, NOR and NAND Flash memories: all the devices
- For e•MMC: the user data area of e•MMC (see #Field6: Offset for access to the boot area partitions)
For RAWImage, Offset=0x0 and PartId >= 0x10
2.6. Field5: Device[edit source]
Select the targeted device and the instance (starting at 0) as defined by U-Boot device tree:
- mmc + instance : 'mmc0'
It is used for e•MMC or SD card on SDMMC. In the below examples:- SD card = mmc0 (SDMMC1)
- e•MMC = mmc1 (SDMMC2)
- nor + instance : 'nor0'
It is used for NOR on QUADSPI. - nand + instance : 'nand0'
It is used for parallel NAND Flash memories on FMC or serial NAND memories on QUADSPI. - none for partition only used to load the binary in RAM
It is allowed only for the reserved boot partition (FSBL=0x1 and SSBL=0x3). In this case, the only allowed fields are :
- Type=Binary, Offset=0x0 and option='-'.
Several devices can be mixed in the same FlashLayout file.
2.7. Field6: Offset[edit source]
The supported values are:
- boot1: first boot area partition of e•MMC (offset is 0x0)
- boot2: second boot area partition of e•MMC (offset is 0x0)
- Offset in bytes: offset in Flash memory area (in the user data area for e•MMC)
Refer to #Partition sizes for offset constraints.
2.8. Field7: Binary[edit source]
This file is used by STM32CubeProgrammer to find the file associated to each Id when it is requested by embedded programming service .
The file can be absent (Binary='none' in the tsv file) only for skipped partitions tagged with the 'E' option. In all other cases, this file is sent to U-Boot to update the Flash memory only for the partitions selected with the 'P' option.
2.9. GPT partuuid of rootfs partition[edit source]
If #Field3: Name = "rootfs" for block device (SD card / e•MMC), U-Boot also sets a unique partition guid [5](PARTUUID) for each instance:
- mmc0: PARTUUID = "e91c4e10-16e6-4c0e-bd0e-77becf4a3582"
- mmc1: PARTUUID = "491f6117-415d-4f53-88c9-6e0de54deac6"
- mmc2: PARTUUID = "fd58f1c7-be0d-4338-8ee9-ad8f050aeb18"
This partition PARTUUID is distinct from the filesystem UUID and it is persistent.
Refer to GPT standard for details. [4]
This value can be used with the "root" argument in the kernel bootargs to identify the partition used for the "Root filesystem". For instance, "root=PARTUID=e91c4e10-16e6-4c0e-bd0e-77becf4a3582" [6] starts with the partition named rootfs on mmc0.
2.10. Partition operations[edit source]
To update only one partition, use the same FlashLayout file, keep the #Field1: Options='P' for the partition to update and change the others to '-'.
To update ssbl partition:
- 0x01 fsbl1 Binary mmc0 0x00004400 fsbl.stm32
- 0x02 fsbl2 Binary mmc0 0x00044400 fsbl.stm32
P 0x03 ssbl Binary mmc0 0x00084400 ssbl.stm32
- 0x10 bootfs System mmc0 0x00284400 bootfs.ext4.bin
- 0x11 rootfs FileSystem mmc0 0x08284400 rootfs.ext4.bin
- 0x12 userfs FileSystem mmc0 0x28284400 userfs.ext4.bin
To delete only one partition, add the 'DE' option on the corresponding line.
To delete ssbl partition:
- 0x01 fsbl1 Binary mmc0 0x00004400 fsbl.stm32
- 0x02 fsbl2 Binary mmc0 0x00044400 fsbl.stm32
PDE 0x03 ssbl Binary mmc0 0x00084400 ssbl.stm32
- 0x10 bootfs System mmc0 0x00284400 bootfs.ext4.bin
- 0x11 rootfs FileSystem mmc0 0x08284400 rootfs.ext4.bin
- 0x12 userfs FileSystem mmc0 0x28284400 userfs.ext4.bin
2.11. Partition sizes[edit source]
The partitions are contiguous (no holes in Flash memory).
The last partition continues until the end of the selected Flash memory.
To reduce the size of the last partition, use an 'Empty' partition and leave it unused.
All the partitions need to be present in the FlashLayout file, even if they are not selected or empty.
Then the offset and size of each partition are compared with:
- pre-existing GPT partitioning, for updates on block devices (e•MMC or SD card)
- predefined partitioning for MTD devices (NOR and NAND): see mtdparts environment variable in U-Boot for more information.
In case of partition size error, compare the existing partition size in U-Boot with the offset in the FlashLayout file.
2.11.1. GPT partition sizes[edit source]
Each GPT partition must be aligned to:
- 512 bytes (LBA)
- e•MMC erase group size
The first partition starts after 17 kbytes (default size of GPT header for 128 entries in U-Boot).
Prior to updating partitions in a block device, check the partition size by executing the U-Boot command "part list" on the selected device:
part list mmc 0
MMC device 0 -- Partition Type: EFI Part Start LBA End LBA Name Attributes Type GUID Partition GUID 1 0x00000022 0x00000221 "fsbl1" attrs: 0x0000000000000000 type: ebd0a0a2-b9e5-4433-87c0-68b6b72699c7 type: data guid: 8ef917d1-2c6f-4bd0-a5b2-331a19f91cb2 2 0x00000222 0x00000421 "fsbl2" attrs: 0x0000000000000000 type: ebd0a0a2-b9e5-4433-87c0-68b6b72699c7 type: data guid: 77877125-add0-4374-9e60-02cb591c9737 3 0x00000422 0x00001821 "ssbl" attrs: 0x0000000000000000 type: ebd0a0a2-b9e5-4433-87c0-68b6b72699c7 type: data guid: b4b84b8a-04e3-48ae-8536-aff5c9c495b1 4 0x00001822 0x00021821 "bootfs" attrs: 0x0000000000000004 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 35219908-c613-4b08-9322-3391ff571e19 5 0x00021822 0x00029821 "vendorfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 8e123a33-e3d3-4db9-92f4-d3ebd9b3224f 6 0x00029822 0x001a9821 "rootfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 02a90af2-5d1c-4a29-9177-97a513e3cae4 7 0x001a9822 0x003a9fdc "userfs" attrs: 0x0000000000000000 type: 0fc63daf-8483-4772-8e79-3d69d8477de4 type: linux guid: 3d5088db-a534-413e-836d-c757cb682814Partition Map for
Warning: Start and end are indicated in mutiple of LBA (512 bytes by default).
To check the e•MMC erase group size in U-Boot, select the mmc device (here 1) and use the command "mmc info" in U-Boot.
mmc dev 1
switch to partitions #0, OK
mmc1(part 0) is current device
mmc info
OEM: 100 Name: 004G6 Bus Speed: 52000000 Mode : MMC High Speed (52MHz) Rd Block Len: 512 MMC version 5.0 High Capacity: Yes Capacity: 3.7 GiB Bus Width: 8-bit Erase Group Size: 512 KiB HC WP Group Size: 4 MiB User Capacity: 3.7 GiB WRREL Boot Capacity: 2 MiB ENH RPMB Capacity: 512 KiB ENHDevice: STM32 SDMMC2 Manufacturer ID: 11
2.11.2. MTD Partition sizes[edit source]
Each MTD partition must be aligned to the device erase block size (NOR/NAND Flash memory).
In U-Boot command :
nand info
Device 0: nand0, sector size 256 KiB
Page size 4096 b
OOB size 224 b
Erase size 262144 b
subpagesize 4096 b
options 0x00084200
bbt options 0x00060000
sf probe
SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB
For MTD, the mtdparts variable is built dynamically (in board_mtdparts_default() under CONFIG_SYS_MTDPARTS_RUNTIME). Execute the U-Boot command mtparts to known the current value, for example when NOR and NAND Flash memories are supported:
mtdparts
SF: Detected mx25l51235f with page size 256 Bytes, erase size 64 KiB, total 64 MiB
device nor0 <nor0>, # parts = 5
#: name size offset mask_flags
0: fsbl1 0x00040000 0x00000000 0
1: fsbl2 0x00040000 0x00040000 0
2: ssbl 0x00200000 0x00080000 0
3: u-boot-env 0x00040000 0x00280000 0
4: nor_user 0x03d40000 0x002c0000 0
device nand0 <nand0>, # parts = 4
#: name size offset mask_flags
0: fsbl 0x00200000 0x00000000 0
1: ssbl1 0x00200000 0x00200000 0
2: ssbl2 0x00200000 0x00400000 0
3: UBI 0x3fa00000 0x00600000 0
active partition: nor0,0 - (fsbl1) 0x00040000 @ 0x00000000
defaults:
mtdids : nor0=nor0,nand0=nand0
mtdparts: mtdparts=nor0:256k(fsbl1),256k(fsbl2),2m(ssbl),256k(u-boot-env),-(nor_user);nand0:2m(fsbl),2m(ssbl1),2m(ssbl2),-(UBI)
NOR Flash last partition, named 'nor_user', is a free MTD partition.
To change the MTD partitioning on NOR and NAND Flash memories, update this variable in U-Boot.
3. Typical FlashLayout file[edit source]
This chapter describes the Layout file for the typical boot use cases based on STM32MP15_Flash_mapping when TEE is not used and associated partitions are absent (teeh, teed and teex).
Data are presented in tables for better readability despite the Layout file is plain text.
In the example, the trusted boot chain is used together with the following files:
- FSBL = tf-a.stm32
- SSBL = u-boot.stm32
3.1. Basic boot chain support[edit source]
The layout in NVM is the same for the basic boot chain (see STM32MP15_Flash_mapping).
The files that must be programmed in NVM for the basic boot chain are:
- FSBL = u-boot-spl.stm32 (instead of tf-a.stm32)
- SSBL = u-boot.img (instead of u-boot.stm32).
However, the basic boot chain does not support the STM32CubeProgrammer (use the trusted bootloaders to program the basic boot chain bootloaders in Flash memory) and the SSBL is programmed wihout STM32 header (with PhaseId ≥ 0x10).
3.2. NOR Flash memory and SD card[edit source]
NOR Flash memory in RAW: Bootloaders = FSBL. It uses two copies (for failsafe update) and one copy for SSBL.
SD card using GPT: several user EXT4 partitions.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary | nor0 | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary | nor0 | 0x40000 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | nor0 | 0x80000 | u-boot.stm32 |
PE | 0x20 | u-boot-env | Binary | nor0 | 0x280000 | none |
PE | 0x21 | unused | Binary | nor0 | 0X2C0000 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00004400 | bootfs.ext4.bin |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04284400 | vendorfs.ext4.bin |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05284400 | rootfs.ext4.bin |
P | 0x13 | userfs | FileSystem | mmc0 | 0x35284400 | userfs.ext4.bin |
The PartId 0x20 is empty/free in nor0, no logo is provided.
The PartId 0x21 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot
3.3. NOR and NAND Flash memories[edit source]
NOR Flash memory in RAW: TF-A uses several partitions for failsafe update, then U-Boot.
NAND Flash memory in UBI: only one large MTD partition for UBI volumes and UBIFS.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary | nor0 | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary | nor0 | 0x40000 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | nor0 | 0x80000 | u-boot.stm32 |
PE | 0x20 | u-boot-env | Binary | nor0 | 0x280000 | none |
PE | 0x21 | unused | Binary | nor0 | 0x2C0000 | none |
P | 0x10 | UBI | FileSystem | nand0 | 0x0 | ubi.bin |
The PartId 0x21 is an empty/free user partition associated to 'nor_user' MTD partition in U-Boot.
Warning: for compatility with NAND-only use case and U-Boot configuration on ST board, the offset of UBI in nand0 is set to 0x00600000.
3.4. NAND Flash memory[edit source]
BootLoader using RAW and then file system in UBI volume.
3.4.1. FSBL:RAW & SSBL:UBI[edit source]
FSBL (TF-A) uses two RAW copies to avoid NAND Flash memory disturbances inside one partition.
SSBL (U-Boot) is present in a RAW volume of the UBI partition.
The binary is also present in FlashLayout file to be loaded in RAM (Opt='-', Part=0x3, Device='none').
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl | Binary(2) | nand0 | 0x0 | tf-a.stm32 |
- | 0x03 | ssbl | Binary | none | 0x0 | u-boot.stm32 |
P | 0x10 | UBI | FileSystem | nand0 | 0x00200000 | ubi.bin |
Warning: The MTD partitioning must be changed in U-Boot.
3.4.2. FSBL+SSBL:RAW[edit source]
FSBL (TF-A) uses two copies in two partitions (for failsafe update) to avoid NAND Flash memory disturbances.
SSBL (U-Boot) uses two copies in two partitions (and not in a UBI volume).
One MTD partition for UBI with several volumes: boot, rootfs and userfs.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary(2) | nand0 | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary(2) | nand0 | 0x100000 | tf-a.stm32 |
P | 0x03 | ssbl1 | Binary | nand0 | 0x200000 | u-boot.bin |
P | 0x04 | ssbl2 | Binary | nand0 | 0x400000 | u-boot.bin |
P | 0x10 | UBI | FileSystem | nand0 | 0x600000 | ubi.bin |
3.5. e•MMC[edit source]
TF-A copied in the two boot area partitions of e•MMC (hidden partition).
GPT partitioning is used on the user area. U-Boot starts just after the GPT header at 17-Kbyte offset.
The userfs partition is pre-populated with ext4 partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary | mmc1 | boot1 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary | mmc1 | boot2 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | mmc1 | 0x00080000 | u-boot.stm32 |
P | 0x10 | bootfs | System | mmc1 | 0x00280000 | bootfs.ext4.stm32 |
P | 0x11 | vendorfs | FileSytem | mmc1 | 0x04280000 | vendorfs.ext4.bin |
P | 0x12 | rootfs | FileSytem | mmc1 | 0x05280000 | rootfs.ext4.bin |
P | 0x13 | userfs | FileSytem | mmc1 | 0x35280000 | userfs.ext4.bin |
3.6. SD card[edit source]
RAW partition: two TF-A partitions, then U-Boot. GPT partitioning is used so fsbl1 starts just after GPT header at 17-Kbyte offset.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary | mmc0 | 0x4400 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | mmc0 | 0x00084400 | u-boot.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x00284400 | bootfs.ext4.bin |
P | 0x11 | vendorfs | FileSytem | mmc0 | 0x04284400 | vendorfs.ext4.bin |
P | 0x12 | rootfs | FileSytem | mmc0 | 0x05284400 | rootfs.ext4.bin |
P | 0x13 | userfs | FileSytem | mmc0 | 0x35284400 | userfs.ext4.bin |
4. Typical FlashLayout file with TEE[edit source]
This chapter describes the Layout file with TEE partitions for the trusted typical boot use case based on STM32MP15_Flash_mapping.
Since TF-A binary for OPTEE does not yet support STM32CubeProgrammer, two different FSBL binaries are used:
- to boot = tf-a.stm32 (no TEE support but programmer support)
- to flash = tf-a-optee.stm32
Since the MTD partitionning is hardcoded in U-Boot, the optee variant is used : u-boot-optee.stm32.
4.1. NOR Flash memory and SD card with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl1 | Binary | nor0 | 0x0 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | nor0 | 0x40000 | tf-a-optee.stm32 |
P | 0x03 | ssbl | Binary | nor0 | 0x80000 | u-boot-optee.stm32 |
PE | 0x20 | u-boot-env | Binary | nor0 | 0x280000 | none |
P | 0x05 | teeh | Binary | nor0 | 0x002C0000 | tee-header.stm32 |
P | 0x06 | teed | Binary | nor0 | 0x00300000 | tee-pageablee.stm32 |
P | 0x07 | teex | Binary | nor0 | 0x00340000 | tee-pager.stm32 |
PE | 0x21 | unused | Binary | nor0 | 0x380000 | none |
P | 0x10 | bootfs | System | mmc0 | 0x00004400 | bootfs.ext4.bin |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04284400 | vendorfs.ext4.bin |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05284400 | rootfs.ext4.bin |
P | 0x13 | userfs | FileSystem | mmc0 | 0x35284400 | userfs.ext4.bin |
4.2. NOR and NAND Flash memories with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl1 | Binary | nor0 | 0x0 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | nor0 | 0x40000 | tf-a-optee.stm32 |
P | 0x03 | ssbl | Binary | nor0 | 0x80000 | u-boot-optee.stm32 |
PE | 0x20 | u-boot-env | Binary | nor0 | 0x280000 | none |
P | 0x05 | teeh | Binary | nor0 | 0x002C0000 | tee-header.stm32 |
P | 0x06 | teed | Binary | nor0 | 0x00300000 | tee-pageablee.stm32 |
P | 0x07 | teex | Binary | nor0 | 0x00340000 | tee-pager.stm32 |
PE | 0x21 | unused | Binary | nor0 | 0x380000 | none |
P | 0x10 | UBI | FileSystem | nand0 | 0x0 | ubi.bin |
4.3. NAND Flash memory with TEE[edit source]
4.3.1. FSBL:RAW & SSBL:UBI with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl | Binary(2) | nand0 | 0x0 | tf-a-optee.stm32 |
- | 0x03 | ssbl | Binary | none | 0x0 | u-boot-optee.stm32 |
P | 0x10 | UBI | FileSystem | nand0 | 0x00200000 | ubi.bin |
4.3.2. FSBL+SSBL:RAW with TEE[edit source]
WARNING: the 'tee' partitions are not duplicated in the next example (possible issue with NAND disturbance).
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
P | 0x05 | fsbl1 | Binary(2) | nand0 | 0x0 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary(2) | nand0 | 0x100000 | tf-a-optee..stm32 |
P | 0x03 | ssbl1 | Binary | nand0 | 0x200000 | u-boot-optee.bin |
P | 0x02 | ssbl2 | Binary | nand0 | 0x400000 | u-boot-optee.bin |
P | 0x06 | teeh | Binary | nand0 | 0x600000 | tee-header.stm32 |
P | 0x07 | teed | Binary | nand0 | 0x680000 | tee-pageable.stm32 |
P | 0x08 | teex | Binary | nand0 | 0x700000 | tee-pager.stm32 |
P | 0x10 | UBI | FileSystem | nand0 | 0x780000 | ubi.bin |
4.4. e•MMC with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl1 | Binary | mmc1 | boot1 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | mmc1 | boot2 | tf-a-optee.stm32 |
P | 0x03 | ssbl | Binary | mmc1 | 0x00080000 | u-boot-optee.stm32 |
P | 0x05 | teeh | Binary | mmc1 | 0x00280000 | tee-header.stm32 |
P | 0x06 | teed | Binary | mmc1 | 0x00300000 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | mmc1 | 0x00380000 | tee-pager.stm32 |
P | 0x10 | bootfs | System | mmc1 | 0x00400000 | bootfs.ext4.stm32 |
P | 0x11 | vendorfs | FileSytem | mmc1 | 0x04400000 | vendorfs.ext4.bin |
P | 0x12 | rootfs | FileSytem | mmc1 | 0x05400000 | rootfs.ext4.bin |
P | 0x13 | userfs | FileSytem | mmc1 | 0x35400000 | userfs.ext4.bin |
4.5. SD card with TEE[edit source]
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl1 | Binary | mmc0 | 0x4400 | tf-a-optee.stm32 |
P | 0x04 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-optee.stm32 |
P | 0x03 | ssbl | Binary | mmc0 | 0x00084400 | u-boot-optee.stm32 |
P | 0x05 | teeh | Binary | mmc0 | 0x00284400 | tee-header.stm32 |
P | 0x06 | teed | Binary | mmc0 | 0x00294400 | tee-pageable.stm32 |
P | 0x07 | teex | Binary | mmc0 | 0x002C4400 | tee-pager.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x00304400 | bootfs.ext4.bin |
P | 0x11 | vendorfs | FileSytem | mmc0 | 0x04304400 | vendorfs.ext4.bin |
P | 0x12 | rootfs | FileSytem | mmc0 | 0x05304400 | rootfs.ext4.bin |
P | 0x13 | userfs | FileSytem | mmc0 | 0x35304400 | userfs.ext4.bin |
5. Using provided FlashLayout files[edit source]
The binary and the associated pre-defined FlashLayout file are provided by ST in the Discovery kit.
For example, in STM32MP15 Discovery kits, you can find the distribution images as well as the file FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv:
#Opt Id Name Type Device Offset Binary
P 0x01 fsbl1 Binary mmc0 0x00004400 tf-a-stm32mp15c-ev1-trusted.stm32
P 0x02 fsbl2 Binary mmc0 0x00044400 tf-a-stm32mp15c-ev1-trusted.stm32
P 0x03 ssbl Binary mmc0 0x00084400 u-boot-stm32mp15c-ev1-trusted.stm32
P 0x10 bootfs System mmc0 0x00294400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x11 vendorfs FileSystem mmc0 0x00294400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x12 rootfs FileSystem mmc0 0x02294400 st-image-core-openstlinux-weston-stm32mp1.ext4
P 0x13 userfs FileSystem mmc0 0x22295800 st-image-userfs-openstlinux-weston-stm32mp1.ext4
You can use these FlashLayout files as a starting point and simply modify them:
5.1. Updating partitions[edit source]
To update only some partitions, change the FlashLayout and only "select" the partitions that need to be updated:
Options field inside the FlashLayout is kept to 'P' for partition(s) that need to be updated, others are changed to '-'.
Then execute STM32CubeProgrammer as before.
Example to update only U-Boot binary and st-image-bootfs filesystem :
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl1 | Binary | mmc0 | 0x00004400 | tf-a-stm32mp15c-ev1-trusted.stm32 |
- | 0x02 | fsbl2 | Binary | mmc0 | 0x00044400 | tf-a-stm32mp15c-ev1-trusted.stm32 |
P | 0x03 | ssbl | Binary | mmc0 | 0x00084400 | u-boot-stm32mp15c-ev1-trusted.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x00304400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
- | 0x11 | vendorfs | FileSystem | mmc0 | 0x04304400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
- | 0x12 | rootfs | FileSystem | mmc0 | 0x05304400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
- | 0x13 | userfs | FileSystem | mmc0 | 0x35304400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type Device Offset Binary
- 0x01 fsbl1 Binary mmc0 0x00004400 tf-a-stm32mp15c-ev1-trusted.stm32
- 0x02 fsbl2 Binary mmc0 0x00044400 tf-a-stm32mp15c-ev1-trusted.stm32
P 0x03 ssbl Binary mmc0 0x00084400 u-boot-stm32mp15c-ev1-trusted.stm32
P 0x10 bootfs System mmc0 0x00294400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
- 0x11 vendorfs FileSystem mmc0 0x00294400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
- 0x12 rootfs FileSystem mmc0 0x02294400 st-image-core-openstlinux-weston-stm32mp1.ext4
- 0x13 userfs FileSystem mmc0 0x22295800 st-image-userfs-openstlinux-weston-stm32mp1.ext4
5.2. Updating partitions using official ST bootloaders[edit source]
If bootloader, FSBL or SSBL are modified, and the STM32CubeProgrammer support is lost for any reason (for example if the stm32prog command is removed), you can still program these new files by selecting the correct binary setting for the partitions 0x01 and 0x03 with Device='none' and change the Id for the binaries to program in flash, as indicated in chapter "Field2: Id".
For example, with ST board, you can flash Customer-modified binary by using ST original file. The new Layout file is:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl-boot | Binary | none | 0x0 | tf-a-stm32mp15c-ev1-trusted.stm32 |
- | 0x03 | ssbl-boot | Binary | none | 0x0 | u-boot-stm32mp15c-ev1-trusted.stm32 |
P | 0x02 | fsbl2 | Binary | mmc0 | 0x00004400 | <Customer-tf-a>.stm32 |
P | 0x04 | fsbl1 | Binary | mmc0 | 0x00044400 | <Customer-tf-a>.stm32 |
P | 0x05 | ssbl | Binary | mmc0 | 0x00084400 | <Customer-u-boot>.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x00304400 | st-image-bootfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x11 | vendorfs | FileSystem | mmc0 | 0x04304400 | st-image-vendorfs-openstlinux-weston-stm32mp1.ext4 |
P | 0x12 | rootfs | FileSystem | mmc0 | 0x05304400 | st-image-core-openstlinux-weston-stm32mp1.ext4 |
P | 0x13 | userfs | FileSystem | mmc0 | 0x35304400 | st-image-userfs-openstlinux-weston-stm32mp1.ext4 |
The associated text file becomes :
#Opt Id Name Type Device Offset Binary
- 0x01 fsbl1 Binary none 0x0 tf-a-stm32mp15c-ev1-trusted.stm32
- 0x03 ssbl Binary none 0x0 u-boot-stm32mp15c-ev1-trusted.stm32
P 0x02 fsbl1 Binary mmc0 0x00004400 tf-a.stm32
P 0x04 fsbl2 Binary mmc0 0x00044400 tf-a.stm32
P 0x05 ssbl Binary mmc0 0x00084400 u-boot.stm32
P 0x10 bootfs System mmc0 0x00294400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x11 vendorfs System mmc0 0x00294400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x12 rootfs FileSystem mmc0 0x02294400 st-image-core-openstlinux-weston-stm32mp1.ext4
P 0x13 userfs FileSystem mmc0 0x22295800 st-image-userfs-openstlinux-weston-stm32mp1.ext4
6. Other FlashLayout examples[edit source]
6.1. SD card: FAT[edit source]
Below an example with FAT bootfs partition (kernel and RAMFS) and an empty userfs partition (deleted and formatted by Linux on first boot):
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary | mmc0 | 0x0 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary | mmc0 | 0x40000 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | mmc0 | 0x80000 | u-boot.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x200000 | bootfs.vfat.bin |
PED | 0x11 | userfs | Empty | mmc0 | 0x400000 | none |
6.2. Load and program different binaries[edit source]
Same example as above with the first two partitions (named "2boot"). They are not programmed and only loaded in RAM.
Userfs is empty but not deleted.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl2boot | Binary | none | 0x0 | tf-a2boot.stm32 |
- | 0x03 | ssbl2boot | Binary | none | 0x0 | u-boot2boot.stm32 |
P | 0x02 | fsbl1 | Binary | mmc0 | 0x40000 | tf-a.stm32 |
P | 0x04 | fsbl2 | Binary | mmc0 | 0x0 | tf-a.stm32 |
P | 0x05 | ssbl | Binary | mmc0 | 0x80000 | u-boot.stm32 |
P | 0x10 | rootfs | System | mmc0 | 0x200000 | rootfs.vfat.bin |
PE | 0x11 | userfs | FileSytem | mmc0 | 0x400000 | none |
6.3. RAWImage[edit source]
The SD card content is exported as RAW device and updated with the image.sdcard file:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | Binary | none | 0x0 | tf-a.stm32 |
- | 0x03 | ssbl | Binary | none | 0x0 | u-boot.stm32 |
P | 0x10 | sdcard | RawImage | mmc0 | 0x0 | image.sdcard |
You can also erase the device before performing the update, by adding 'D' in option.
6.4. Deleting device content[edit source]
For example, NOR and NAND Flash memories are deleted with:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl | none | none | 0x0 | tf-a.stm32 |
- | 0x03 | ssbl | none | none | 0x0 | u-boot.stm32 |
PDE | 0x10 | nor | RawImage | nor0 | 0x0 | none |
PDE | 0x11 | nand | RawImage | nand0 | 0x0 | none |
To erase all other devices, including the e•MMC boot partition, proceed as follows:
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
- | 0x01 | fsbl1 | Binary | none | 0x0 | tf-a.stm32 |
- | 0x03 | ssbl | Binary | none | 0x0 | u-boot.stm32 |
PDE | 0x10 | sdcard | RawImage | mmc0 | 0x0 | none |
PED | 0x20 | emmc_boot1 | Binary | mmc1 | boot1 | none |
DPE | 0x21 | emmc_boot2 | Binary | mmc1 | boot2 | none |
EPD | 0x22 | emmc | RawImage | mmc1 | 0x0 | none |
DPE | 0x30 | nand | RawImage | nand0 | 0x0 | none |
PDE | 0x40 | nor | RawImage | nor0 | 0x0 | none |
Warning: A timeout may occur in STM32CubeProgrammer since deleting NOR Flash memory might be slow. To avoid this issue you can delete only the used partitions (Option=PED), for example:
#Opt Id Name Type Device Offset Binary
- 0x01 fsbl_boot Binary none 0x0 fsbl.stm32
- 0x03 ssbl_boot Binary none 0x0 ssbl.stm32
#delete ALL devices
EPD 0x10 sdcard RawImage mmc0 0x0 none
PED 0x02 emmc_b1 Binary mmc1 boot1 none
PED 0x04 emmc_b2 Binary mmc1 boot2 none
PED 0x20 emmc RawImage mmc1 0x0 none
PED 0x30 nand RawImage nand0 0x0 none
# on NOR (slow device): delete ALL used partitions
PE 0x40 nor RawImage nor0 0x0 none
PED 0x41 fsbl1_nor Binary nor0 0x00000000 none
PED 0x42 fsbl2_nor Binary nor0 0x00040000 none
PED 0x43 ssbl_nor Binary nor0 0x00080000 none
PED 0x44 u-boot-env_nor Binary nor0 0x00280000 none
PE 0x45 unused Binary nor0 0x002C0000 none
6.5. Complex use case[edit source]
Update SD card (mmc0 on SDMMC1). The GPT partition is created since all partitions are selected and Userfs is deleted and empty.
Erase all other devices, including e•MMC hidden boot partition.
Opt | Part | Name | Type | Device | Offset | Binary |
---|---|---|---|---|---|---|
P | 0x01 | fsbl1 | Binary | mmc0 | 0x04400 | tf-a.stm32 |
P | 0x02 | fsbl2 | Binary | mmc0 | 0x44400 | tf-a.stm32 |
P | 0x03 | ssbl | Binary | mmc0 | 0x84400 | u-boot.stm32 |
P | 0x10 | bootfs | System | mmc0 | 0x284400 | bootfs.stm32 |
P | 0x11 | rootfs | FileSytem | mmc0 | 0x08284400 | rootfs.ext4.bin |
DEP | 0x12 | userfs | FileSytem | mmc0 | 0x28284400 | none |
PED | 0x60 | emmc_boot1 | Binary | mmc1 | boot1 | none |
DPE | 0x61 | emmc_boot2 | Binary | mmc1 | boot2 | none |
EPD | 0x62 | emmc | RawImage | mmc1 | 0x0 | none |
D | 0x10 | nand | RawImage | nand0 | 0x0 | none |
7. Reference list[edit source]
- ↑ https://en.wikipedia.org/wiki/USB#Device_Firmware_Upgrade
- ↑ http://www.usb.org/developers/docs/devclass_docs/DFU_1.1.pdf Universal Serial Bus Device Class Specification for Device Firmware Upgrade, Version 1.1
- ↑ https://web.archive.org/web/20141011015811/http://www.usb.org/developers/docs/devclass_docs/DFU_1.1.pdf Archived from the original on 11 October 2014
- ↑ Jump up to: 4.0 4.1 https://en.wikipedia.org/wiki/GUID_Partition_Table
- ↑ Jump up to: 5.0 5.1 https://en.wikipedia.org/wiki/Universally_unique_identifier
- ↑ https://wiki.archlinux.org/index.php/persistent_block_device_naming