- Last edited 2 years ago ago
RNG device tree configuration
Contents
1 Article purpose[edit]
This article explains how to configure the RNG internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the Hardware random framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the RNG peripheral, used by the STM32 RNG Linux driver.
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2 DT bindings documentation[edit]
The RNG is represented by the STM32 RNG device tree bindings[1]
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
The RNG node is declared in stm32mp157c.dtsi[2]. It describes the hardware register address, clock and reset.
rng1: rng@54003000 { Comments compatible = "st,stm32-rng"; reg = <0x54003000 0x400>; --> Register location and length clocks = <&rcc RNG1_K>; resets = <&rcc RNG1_R>; status = "disabled"; };
3.2 DT configuration (board level)[edit]
This part is used to enable the RNG used on a board which is done by setting the status property to okay.
A clock-error-detect property is available depending the clock choosen for entropy. It can be enabled to manage the clock detection.
3.3 DT configuration examples[edit]
&rng1 { status = "okay"; clock-error-detect; };
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information: