deleted>Frq08988 |
Registered User m (Cleanup) |
||
Line 1: | Line 1: | ||
== Article purpose == | == Article purpose == | ||
This article explains how to configure the [[RNG internal peripheral|'''RNG''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[Hardware random overview|Hardware random framework]]. | This article explains how to configure the [[RNG internal peripheral|'''RNG''' internal peripheral]] when it is assigned to the Linux<sup>®</sup> OS. In that case, it is controlled by the [[Hardware random overview|Hardware random framework]]. | ||
Line 52: | Line 43: | ||
<references/> | <references/> | ||
<noinclude> | |||
{{ArticleBasedOnModel|[[Peripheral or framework device tree configuration model]]}} | |||
{{PublicationRequestId | 8900 | 2018-10-08 | AlainF}} | |||
[[Category:Device tree configuration]] | |||
[[Category:Security]] | |||
</noinclude> |
Revision as of 16:02, 24 September 2019
1. Article purpose[edit source]
This article explains how to configure the RNG internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the Hardware random framework.
The configuration is performed using the device tree mechanism that provides a hardware description of the RNG peripheral, used by the STM32 RNG Linux driver.
2. DT bindings documentation[edit source]
The RNG is represented by the STM32 RNG device tree bindings[1]
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1. DT configuration (STM32 level)[edit source]
The RNG node is declared in stm32mp157c.dtsi[2]. It describes the hardware register address, clock and reset.
Template:Highlight compatible = "st,stm32-rng"; reg = <0x54003000 0x400>; Template:Highlight clocks = <&rcc RNG1_K>; resets = <&rcc RNG1_R>; status = "disabled"; };rng1: rng@54003000 {
3.2. DT configuration (board level)[edit source]
This part is used to enable the RNG used on a board which is done by setting the status property to okay.
A clock-error-detect property is available depending the clock choosen for entropy. It can be enabled to manage the clock detection.
3.3. DT configuration examples[edit source]
&rng1 {
status = "okay";
clock-error-detect;
};
4. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
5. References[edit source]
Please refer to the following links for additional information: