Last edited 4 years ago

NVMEM overview

Template:ArticleBasedOnModel Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


SUMMARY

This article introduces how NVMEM Linux® framework manages BSEC OTP data and how to read/write from/to it.

1. Framework purpose[edit source]

The NVMEM Linux® framework provides a generic interface for the device non-volatile memory data such as:

  • OTP (one-time programmable) fuses
  • EEPROM

It offers kernel space and user space interfaces to read and/or write data such as analog calibration data or MAC address.

2. System overview[edit source]

Template:ImageMap

2.1. Component description[edit source]

  • NVMEM user (user space)

The user can use the NVMEM sysfs interface, from a user terminal or a custom application, to read/write data from/to NVMEM device(s) from user space.

  • NVMEM user (kernel space)

User drivers can use the NVMEM API to read/write data from/to NVMEM device(s) from kernel space (such as the analog calibration data used by an ADC driver).

  • NVMEM framework (kernel space)

The NVMEM core provides sysfs interface and NVMEM API. They can be used to implement NVMEM user and NVMEM controller drivers.

  • NVMEM drivers (kernel space)

Provider drivers such as BSEC Linux® driver that exposes OTP data to the core.

  • NVMEM hardware

NVMEM controller(s) such as the BSEC internal peripheral[1]

2.2. API description[edit source]

The NVMEM kernel documentation[2] describes:

  • Kernel space API for NVMEM providers and NVMEM consumers.
  • Userspace binary interface (sysfs).

See also sysfs-bus-nvmem[3] ABI documentation.

3. Configuration[edit source]

3.1. Kernel configuration[edit source]

Activate NVMEM framework in the kernel configuration through the Linux® menuconfig tool, Menuconfig or how to configure kernel (CONFIG_NVMEM=y):

Device Drivers  --->
   [*] NVMEM Support  --->

3.2. Device tree configuration[edit source]

The NVMEM data device tree bindings[4] describe:

  • The location of non-volatile memory data
  • The NVMEM data providers
  • The NVMEM data consumers

4. How to use the framework[edit source]

4.1. How to use NVMEM with sysfs interface[edit source]

The available NVMEM devices can be listed in sysfs:

Template:Board$ ls /sys/bus/nvmem/devices/                                            # Template:Highlight
stm32-romem0

The data content of an NVMEM device can be dumped to a binary file:

Template:Board$ cat /sys/bus/nvmem/devices/stm32-romem0/nvmem > file                  # Template:Highlight

The data content of an NVMEM device can be displayed:

Template:Board$ hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem

Template:Warning The full data content of an NVMEM device can be written as follows:

Template:Board$ cat file > /sys/bus/nvmem/devices/stm32-romem0/nvmem                  # Template:Highlight

Example of 32-bit data word writing (filling it with ones) in OTP n°95:

Template:Board$ dd if=/dev/zero count=1 bs=4 | tr '\000' '\377' > file                # Create a 4 bytes length file filled with ones, e.g. 0xffffffff)
Template:Board$ dd if=file bs=4 seek=95 of=/sys/bus/nvmem/devices/stm32-romem0/nvmem  # Write it (32-bits, e.g. 4bytes) to OTP data 95

5. How to trace and debug the framework[edit source]

5.1. How to trace[edit source]

Ftrace can be used to trace the NVMEM framework:

Template:Board$ cd /sys/kernel/debug/tracing
Template:Board$ cat available_filter_functions | grep nvmem                           # Show available filter functions
rtc_nvmem_register
rtc_nvmem_unregister
nvmem_reg_read
bin_attr_nvmem_read
...

Enable the kernel function tracer, then start using nvmem and display the result:

Template:Board$ echo function > current_tracer
Template:Board$ echo "*nvmem*" > set_ftrace_filter                                    # Trace all nvmem filter functions
Template:Board$ echo 1 > tracing_on                                                   # start ftrace
Template:Board$ hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem               # dump nvmem
00000000  17 00 00 00 01 80 00 00  00 00 00 00 00 00 00 00  |................|
...
Template:Board$ echo 0 > tracing_on                                                   # stop ftrace
Template:Board$ cat trace
# tracer: function
#
#                              _-----=> irqs-off
#                             / _----=> need-resched
#                            | / _---=> hardirq/softirq
#                            || / _--=> preempt-depth
#                            ||| /     delay
#           TASK-PID   CPU#  ||||    TIMESTAMP  FUNCTION
#              | |       |   ||||       |         |
         hexdump-478   [000] ....   423.502278: bin_attr_nvmem_read <-sysfs_kf_bin_read
         hexdump-478   [000] ....   423.502290: nvmem_reg_read <-bin_attr_nvmem_read
         hexdump-478   [000] ....   423.515804: bin_attr_nvmem_read <-sysfs_kf_bin_read

6. References[edit source]

  1. BSEC internal peripheral
  2. Template:CodeSource, NVMEM subsytem kernel documentation
  3. Template:CodeSource, NVMEM ABI documentation
  4. Template:CodeSource, NVMEM data device tree bindings