imported>Cayale |
Registered User mNo edit summary |
||
(35 intermediate revisions by 5 users not shown) | |||
Line 1: | Line 1: | ||
==Article purpose== | ==Article purpose== | ||
This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the [[OpenEmbedded - devtool|devtool]] and [[BitBake cheat sheet|BitBake]] tools: | This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the [[OpenEmbedded - devtool|devtool]] and [[BitBake cheat sheet|BitBake]] tools: | ||
Line 39: | Line 25: | ||
To start modification with a module, you need to initialize your Distribution Package environment. | To start modification with a module, you need to initialize your Distribution Package environment. | ||
{{PC$}} cd <working directory path of distribution> | {{PC$}} cd <working directory path of distribution> | ||
{{PC$}} DISTRO=openstlinux-weston MACHINE=stm32mp1 source meta-st/scripts/envsetup.sh | {{PC$}} DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh | ||
You are now in the build directory, identified by <build dir> in the following paragraphs. | |||
Initialize devtool for kernel component: | Initialize devtool for kernel component: | ||
Line 58: | Line 46: | ||
{{Info| The source code of kernel is located on <build dir>/workspace/sources. You can change the path where the source code is extracted by customizing the devtool modify command }} | {{Info| The source code of kernel is located on <build dir>/workspace/sources. You can change the path where the source code is extracted by customizing the devtool modify command }} | ||
{{Info| For all the work around the kernel, we strongly encourage some usage for deploying the binaries on board | {{Info| For all the work around the kernel, we strongly encourage some usage for deploying the binaries on board | ||
* Kernel image, device tree: use bitbake deploy command and scp (see [[#modifying kernel configuration]] )) | * Kernel image, device tree: use bitbake deploy command and scp (see [[#modifying kernel configuration]] )) | ||
Line 131: | Line 116: | ||
please can you refer to this wiki page and following section | please can you refer to this wiki page and following section | ||
3.2 Adding kernel driver or device tree modifications | 3.2 Adding kernel driver or device tree modifications | ||
<br/>W2015: CPR: the goal of this page are not to integrate some change but to cross compile some changes and test it. | |||
)}} | |||
* Go to the build directory | |||
{{PC$}} cd <build dir> | |||
If this update is accepted, then to report in other paragraph of this page}} | |||
* Generate the device tree blobs (''*.dtb'') | * Generate the device tree blobs (''*.dtb'') | ||
{{PC$}} bitbake | {{PC$}} bitbake virtual/kernel -C compile | ||
{{Info|we use here bitbake command instead of '''devtool build''' because the '''build''' makes '''compile''', '''compile_kernemodules''' and '''install''' commands whereas we only need only '''compile''' command to generate the kernel image and the device tree }} | |||
* Update the device tree blobs on the board | * Update the device tree blobs on the board | ||
{{PC$}} scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot | {{PC$}} scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot | ||
Line 176: | Line 162: | ||
} | } | ||
* Go to the | * Go to the build directory | ||
{{PC$}} cd <build | {{PC$}} cd <build dir> | ||
* Cross-compile the Linux kernel | * Cross-compile the Linux kernel | ||
{{PC$}} bitbake | {{PC$}} bitbake virtual/kernel -C compile | ||
* Update the Linux kernel image on board | * Update the Linux kernel image on board | ||
Line 229: | Line 215: | ||
} | } | ||
* Go to the | * Go to the build directory | ||
{{PC$}} cd <build | {{PC$}} cd <build dir> | ||
* Cross-compile the Linux kernel modules | * Cross-compile the Linux kernel modules | ||
{{PC$}} bitbake | {{PC$}} bitbake virtual/kernel -C compile | ||
* Update the vivid kernel module on the board | * Update the vivid kernel module on the board | ||
{{PC$}} devtool deploy-target -Ss <name of kernel recipe> root@<board ip address>:/ | {{PC$}} devtool deploy-target -Ss <name of kernel recipe> root@<board ip address>:/ | ||
{{ReviewsComments|YCO W908: the command failed with my config (openstlinux-4.19-thud-mp1-19-02-20)<br> | |||
it seems to be link to the strip option, the error displayed is : <br> TypeError: strip_execs() missing 1 required positional argument: 'd' }} | |||
* Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory | * Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory | ||
Line 269: | Line 249: | ||
* Create the source code file for this kernel module example: ''kernel_module_example.c'' | * Create the source code file for this kernel module example: ''kernel_module_example.c'' | ||
< | <syntaxhighlight lang="c"> | ||
// SPDX-identifier: GPL-2.0 | // SPDX-identifier: GPL-2.0 | ||
/* | /* | ||
Line 299: | Line 279: | ||
MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>"); | MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>"); | ||
MODULE_LICENSE("GPL v2"); | MODULE_LICENSE("GPL v2"); | ||
</ | </syntaxhighlight > | ||
* Create the makefile for this kernel module example: ''Makefile'' | * Create the makefile for this kernel module example: ''Makefile'' | ||
Line 324: | Line 304: | ||
* Add a new recipe to the workspace | * Add a new recipe to the workspace | ||
{{PC$}} cd <build | {{PC$}} cd <build dir> | ||
{{PC$}} devtool add mymodule kernel_module_example/ | {{PC$}} devtool add mymodule kernel_module_example/ | ||
Line 330: | Line 310: | ||
{{PC$}} devtool edit-recipe mymodule | {{PC$}} devtool edit-recipe mymodule | ||
:Modify the recipe according the following changes (see highlighted lines) | :Modify the recipe according the following changes (see highlighted lines) | ||
< | |||
<syntaxhighlight lang="c" line highlight="21-22,24-25,27,40-41"> | |||
# Recipe created by recipetool | # Recipe created by recipetool | ||
# This is the basis of a recipe and may need further editing in order to be fully functional. | # This is the basis of a recipe and may need further editing in order to be fully functional. | ||
Line 372: | Line 353: | ||
# NOTE: unable to determine what to put here - there is a Makefile but no | # NOTE: unable to determine what to put here - there is a Makefile but no | ||
# target named "install", so you will need to define this yourself | # target named "install", so you will need to define this yourself | ||
install -d ${D}/lib/modules/${KERNEL_VERSION} | install -d ${D}/lib/modules/${KERNEL_VERSION} | ||
install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/ | install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/ | ||
} | } | ||
</ | </syntaxhighlight > | ||
* Go to the | * Go to the build directory | ||
{{PC$}} cd <build | {{PC$}} cd <build dir> | ||
* Generated kernel module example | * Generated kernel module example | ||
Line 400: | Line 381: | ||
==Modifying the U-Boot== | ==Modifying the U-Boot== | ||
This simple example adds unconditional log information when U-Boot starts. Within the scope of the [[Boot | This simple example adds unconditional log information when U-Boot starts. Within the scope of the [[Boot chain overview|trusted boot chain]], U-Boot is used as second stage boot loader (SSBL). | ||
* Have a look at the U-Boot log information when the board reboots | * Have a look at the U-Boot log information when the board reboots | ||
Line 412: | Line 393: | ||
[...] | [...] | ||
* Go to | * Go to the build directory | ||
{{PC$}} cd <build | {{PC$}} cd <build dir> | ||
* Search U-boot recipe | * Search U-boot recipe | ||
{{PC$}} devtool search u-boot* | {{PC$}} devtool search u-boot* | ||
u-boot-stm32mp-extlinux Generate 'extlinux.conf' file for U-boot | u-boot-stm32mp-extlinux Generate 'extlinux.conf' file for U-boot | ||
u-boot | u-boot-stm32mp Universal Boot Loader for embedded devices for stm32mp | ||
On this example, the recipe name is '''u-boot | On this example, the recipe name is '''u-boot-stm32mp''' | ||
* Start to work with u-boot | * Start to work with u-boot | ||
{{PC$}} devtool modify u-boot | {{PC$}} devtool modify u-boot-stm32mp | ||
Example: | Example: | ||
{{PC$}} cd <build | {{PC$}} cd <build dir>/workspace/sources/u-boot-stm32mp | ||
* Edit the ''./board/st/stm32mp1/stm32mp1.c'' source file | * Edit the ''./board/st/stm32mp1/stm32mp1.c'' source file | ||
* Add a log information in the ''checkboard'' function | * Add a log information in the ''checkboard'' function | ||
Line 440: | Line 421: | ||
* Cross-compile the U-Boot: trusted boot | * Cross-compile the U-Boot: trusted boot | ||
{{PC$}} devtool build u-boot | {{PC$}} devtool build u-boot-stm32mp | ||
{{PC$}} bitbake u-boot | {{PC$}} bitbake u-boot-stm32mp -c deploy | ||
* Go to the directory in which the compilation results are stored | * Go to the directory in which the compilation results are stored | ||
Line 486: | Line 467: | ||
==Modifying the TF-A== | ==Modifying the TF-A== | ||
This simple example adds unconditional log information when the TF-A starts. Within the scope of the [[Boot | This simple example adds unconditional log information when the TF-A starts. Within the scope of the [[Boot chain overview|trusted boot chain]], TF-A is used as first stage boot loader (FSBL). | ||
* Have a look at the TF-A log information when the board reboots | * Have a look at the TF-A log information when the board reboots | ||
Line 495: | Line 476: | ||
[...] | [...] | ||
* Go to | * Go to the build directory | ||
{{PC$}} cd <build | {{PC$}} cd <build dir> | ||
* Search TF-A recipe | * Search TF-A recipe | ||
{{PC$}} devtool search tf-a* | {{PC$}} devtool search tf-a* | ||
Line 515: | Line 496: | ||
{{PC$}} devtool modify tf-a-stm32mp | {{PC$}} devtool modify tf-a-stm32mp | ||
* Go to | * Go to <build dir>/workspace/sources/tf-a-stm32mp | ||
{{PC$}} cd <build | {{PC$}} cd <build dir>/workspace/sources/tf-a-stm32mp | ||
* Edit the ''./plat/st/stm32mp1/bl2_io_storage.c'' source file | * Edit the ''./plat/st/stm32mp1/bl2_io_storage.c'' source file | ||
Line 584: | Line 565: | ||
* Create the source code file for this user space example: ''hello_world_example.c'' | * Create the source code file for this user space example: ''hello_world_example.c'' | ||
< | <syntaxhighlight lang="c"> | ||
// SPDX-identifier: GPL-2.0 | // SPDX-identifier: GPL-2.0 | ||
/* | /* | ||
Line 610: | Line 591: | ||
return(0); | return(0); | ||
} | } | ||
</ | </syntaxhighlight> | ||
* Add a new recipe to the workspace | |||
{{PC$}} cd <build dir> | |||
{{PC$}} cd <build | |||
{{PC$}} devtool add myhelloword hello_world_example/ | {{PC$}} devtool add myhelloword hello_world_example/ | ||
Line 620: | Line 600: | ||
{{PC$}} devtool edit-recipe myhelloword | {{PC$}} devtool edit-recipe myhelloword | ||
:Modify the recipe according the following changes (see highlighted lines) | :Modify the recipe according the following changes (see highlighted lines) | ||
< | <syntaxhighlight lang="c" line highlight="27-28,33-34"> | ||
# Recipe created by recipetool | # Recipe created by recipetool | ||
# This is the basis of a recipe and may need further editing in order to be fully functional. | # This is the basis of a recipe and may need further editing in order to be fully functional. | ||
Line 656: | Line 636: | ||
install -m 755 ${S}/hello_word_example ${D}${bindir}/ | install -m 755 ${S}/hello_word_example ${D}${bindir}/ | ||
} | } | ||
</ | </syntaxhighlight> | ||
* Compile binary | |||
{{PC$}} devtool build myhelloword | |||
* Push this binary on board | * Push this binary on board | ||
Line 682: | Line 665: | ||
* Attach the boot file system found under ''/dev/mmcblk0p4'' in the directory ''/boot'' | * Attach the boot file system found under ''/dev/mmcblk0p4'' in the directory ''/boot'' | ||
{{Board$}} mount /dev/mmcblk0p4 /boot | {{Board$}} mount /dev/mmcblk0p4 /boot | ||
<noinclude> | |||
[[Category:How to build software]] | |||
[[Category:Distribution Package]] | |||
{{PublicationRequestId | 10439 | 2019-01-24 | AlainF}} | |||
{{UpdateNeededForNewRelease|Please check regularly that the commands work fine}} | |||
{{ReviewsComments|JCT W826: general remark: | |||
* sometimes, you use "devtool build" to cross-compile, and sometimes, you use "bitbake <name of recipe> -C compile". | |||
* sometimes, you use "devtool deploy-target" to deploy, and sometimes, you use "bitbake <name of kernel recipe> -c deploy" | |||
It might be interesting to explain the reasons why different methods are used if there are such reasons. If there's no special reason (it's just that there are several methods possible, it might be interesting to indicate it}} | |||
</noinclude> |
Latest revision as of 11:32, 25 September 2020
1. Article purpose[edit source]
This article provides simple examples for the Distribution Package of the OpenSTLinux distribution, that illustrate the cross-compilation with the devtool and BitBake tools:
- modification with Linux® Kernel (configuration, device tree, driver, ...)
- modification of an external in-tree Linux Kernel module
- modification of U-Boot
- modification of TF-A
- addition of software
These examples also show how to deploy the results of the cross-compilation on the target, through a network connection to the host machine.
2. Prerequisites[edit source]
The prerequisites from Installing the OpenSTLinux distribution must be executed.
The board and the host machine are connected through an Ethernet link, and a remote terminal program is started on the host machine: see How to get Terminal.
The target is started, and its IP address (<board ip address>) is known.
3. Modification with kernel[edit source]
3.1. Preamble[edit source]
To start modification with a module, you need to initialize your Distribution Package environment.
cd <working directory path of distribution>
DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
You are now in the build directory, identified by <build dir> in the following paragraphs.
Initialize devtool for kernel component:
devtool modify virtual/kernel
NOTE: Starting bitbake server...
NOTE: Creating workspace layer in /mnt/internal_storage/oetest/oe_openstlinux_rocko/build-openstlinuxweston-stm32mp1/workspace
NOTE: Enabling workspace layer in bblayers.conf
Parsing recipes: 100% |########################################################################################| Time: 0:00:54
Parsing of 2401 .bb files complete (0 cached, 2401 parsed). 3282 targets, 88 skipped, 0 masked, 0 errors.
NOTE: Mapping virtual/kernel to linux-stm32mp
NOTE: Resolving any missing task queue dependencies
...
3.2. Modifying kernel configuration[edit source]
This simple example modifies the kernel configuration via menuconfig for the CMA size.
- Get the current value of the CMA size (128 Mbytes here) through the analysis of the target boot log
dmesg | grep -i cma
[ 0.000000] cma: Reserved 128 MiB at 0xf0000000
- Start the Linux kernel configuration menu: see Menuconfig or how to configure kernel
- Navigate to "Device Drivers - Generic Driver Options"
- select "Size in Megabytes"
- modify its value to 256
- exit and save the new configuration
- Check that the configuration file (.config) has been modified
grep -i CONFIG_CMA_SIZE_MBYTES <build dir>/workspace/sources/<name of kernel recipe>/.config.new
CONFIG_CMA_SIZE_MBYTES=256
- Cross-compile the Linux kernel: see Menuconfig or how to configure kernel
- Update the Linux kernel image on board: see Menuconfig or how to configure kernel
- Reboot the board: see Menuconfig or how to configure kernel
- Get the new value of the CMA size (256 Mbytes) through the analysis of the target boot log
256 MiB at 0xe0000000dmesg | grep -i cma [ 0.000000] cma: Reserved
3.3. Modifying the Linux kernel device tree[edit source]
This simple example modifies the default status of a user LED.
- With the board started; check that the user LED (LD3) is disabled
- Go to the <build dir>/workspace/sources/<name of kernel recipe>/ directory
cd <build dir>/workspace/sources/<name of kernel recipe>/
- Edit the arch/arm/boot/dts/stm32mp157c-ed1.dts Device Tree Source file for evaluation board or
Edit the arch/arm/boot/dts/stm32mp157c-dk2.dts Device Tree Source file for discovery board or
- Change the status of the "stm32mp:green:user" led to "okay", and set its default state to "on"
okay"; red { label = "stm32mp:red:status"; gpios = <&gpioa 13 GPIO_ACTIVE_LOW>; status = "disabled"; }; green { label = "stm32mp:green:user"; gpios = <&gpioa 14 GPIO_ACTIVE_LOW>; default-state = "on"; status = "okay"; }; };led { compatible = "gpio-leds"; status = "
- Go to the build directory
cd <build dir>
If this update is accepted, then to report in other paragraph of this page}}
- Generate the device tree blobs (*.dtb)
bitbake virtual/kernel -C compile
- Update the device tree blobs on the board
scp <build dir>/tmp-glibc/deploy/images/<machine name>/*.dtb root@<board ip address>:/boot
- Reboot the board
cd /boot; sync; systemctl reboot
- Check that the user LED (LD3) is enabled (green)
3.4. Modifying a built-in Linux kernel device driver[edit source]
This simple example adds unconditional log information when the display driver is probed.
- Check that there is no log information when the display driver is probed
dmesg | grep -i stm_drm_platform_probe
- Go to the <build dir>/workspace/sources/<name of kernel recipe>/
cd <build dir>/workspace/sources/<name of kernel recipe>/
- Edit the ./drivers/gpu/drm/stm/drv.c source file
- Add a log information in the stm_drm_platform_probe function
DRM_INFO("Simple example - %s\n", __func__); return 0; [...] }static int stm_drm_platform_probe(struct platform_device *pdev) { struct device *dev = &pdev->dev; struct drm_device *ddev; int ret; [...]
- Go to the build directory
cd <build dir>
- Cross-compile the Linux kernel
bitbake virtual/kernel -C compile
- Update the Linux kernel image on board
scp <build dir>/tmp-glibc/deploy/images/<machine name>/uImage root@<board ip address>:/boot
- Reboot the board
cd /boot; sync; systemctl reboot
- Check that there is now log information when the display driver is probed
Simple example - stm_drm_platform_probedmesg | grep -i stm_drm_platform_probe [ 5.005833] [drm]
3.5. Modifying/adding an external Linux kernel module[edit source]
Most device drivers (modules) in the Linux kernel can be compiled either into the kernel itself (built-in/internal module) or as Loadable Kernel Modules (LKM/external module) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).
This simple example adds an unconditional log information when the virtual video test driver (vivid) kernel module is probed or removed.
- Go to the <build dir>/workspace/sources/<name of kernel recipe>/
cd <build dir>/workspace/sources/<name of kernel recipe>/
- Edit the ./drivers/media/platform/vivid/vivid-core.c source file
- Add log information in the vivid_probe and vivid_remove functions
pr_info("Simple example - %s\n", __func__); return ret; }static int vivid_probe(struct platform_device *pdev) { const struct font_desc *font = find_font("VGA8x16"); int ret = 0, i; [...] /* n_devs will reflect the actual number of allocated devices */ n_devs = i;
pr_info("Simple example - %s\n", __func__); return 0; }static int vivid_remove(struct platform_device *pdev) { struct vivid_dev *dev; unsigned int i, j; [...]
- Go to the build directory
cd <build dir>
- Cross-compile the Linux kernel modules
bitbake virtual/kernel -C compile
- Update the vivid kernel module on the board
devtool deploy-target -Ss <name of kernel recipe> root@<board ip address>:/
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a
sync
- Insert the vivid kernel module into the Linux kernel
Simple example - vivid_probemodprobe vivid [...] [ 3412.784638]
- Remove the vivid kernel module from the Linux kernel
Simple example - vivid_removermmod vivid [...] [ 3423.708517]
4. Adding an external out-of-tree Linux kernel module[edit source]
This simple example adds a "Hello World" external out-of-tree Linux kernel module to the Linux kernel.
- Create a directory for this kernel module example
mkdir kernel_module_example
cd kernel_module_example
- Create the source code file for this kernel module example: kernel_module_example.c
// SPDX-identifier: GPL-2.0
/*
* Copyright (C) STMicroelectronics SA 2018
*
* Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
*
*/
#include <linux/module.h> /* for all kernel modules */
#include <linux/kernel.h> /* for KERN_INFO */
#include <linux/init.h> /* for __init and __exit macros */
static int __init kernel_module_example_init(void)
{
printk(KERN_INFO "Kernel module example: hello world from STMicroelectronics\n");
return 0;
}
static void __exit kernel_module_example_exit(void)
{
printk(KERN_INFO "Kernel module example: goodbye from STMicroelectronics\n");
}
module_init(kernel_module_example_init);
module_exit(kernel_module_example_exit);
MODULE_DESCRIPTION("STMicroelectronics simple external out-of-tree Linux kernel module example");
MODULE_AUTHOR("Jean-Christophe Trotin <jean-christophe.trotin@st.com>");
MODULE_LICENSE("GPL v2");
- Create the makefile for this kernel module example: Makefile
Linux kernel module example # Object file(s) to be built obj-m := kernel_module_example.o # Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= <Linux kernel path> # Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) default: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules clean: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean# Makefile for simple external out-of-tree
- Add a new recipe to the workspace
cd <build dir>
devtool add mymodule kernel_module_example/
- Adapt recipe to kernel module build
devtool edit-recipe mymodule
- Modify the recipe according the following changes (see highlighted lines)
# Recipe created by recipetool
# This is the basis of a recipe and may need further editing in order to be fully functional.
# (Feel free to remove these comments when editing.)
# Unable to find any files that looked like license statements. Check the accompanying
# documentation and source headers and set LICENSE and LIC_FILES_CHKSUM accordingly.
#
# NOTE: LICENSE is being set to "CLOSED" to allow you to at least start building - if
# this is not accurate with respect to the licensing of the software being built (it
# will not be in most cases) you must specify the correct value before using this
# recipe for anything other than initial testing/development!
LICENSE = "CLOSED"
LIC_FILES_CHKSUM = ""
# No information for SRC_URI yet (only an external source tree was specified)
SRC_URI = ""
# NOTE: this is a Makefile-only piece of software, so we cannot generate much of the
# recipe automatically - you will need to examine the Makefile yourself and ensure
# that the appropriate arguments are passed in.
DEPENDS = "virtual/kernel"
inherit module
EXTRA_OEMAKE = "ARCH=arm"
EXTRA_OEMAKE += "KERNEL_DIR=${STAGING_KERNEL_BUILDDIR}"
S = "${WORKDIR}"
do_configure () {
# Specify any needed configure commands here
:
}
do_compile () {
# You will almost certainly need to add additional arguments here
oe_runmake
}
do_install () {
# NOTE: unable to determine what to put here - there is a Makefile but no
# target named "install", so you will need to define this yourself
install -d ${D}/lib/modules/${KERNEL_VERSION}
install -m 0755 ${B}/kernel_module_example.ko ${D}/lib/modules/${KERNEL_VERSION}/
}
- Go to the build directory
cd <build dir>
- Generated kernel module example
devtool build mymodule
- Push this kernel module example on board
devtool deploy-target -Ss mymodule root@<board ip address>
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a
sync
- Insert the kernel module example into the Linux kernel
Kernel module example: hello world from STMicroelectronicsmodprobe kernel_module_example [18167.821725]
- Remove the kernel module example from the Linux kernel
Kernel module example: goodbye from STMicroelectronicsrmmod kernel_module_example [18180.086722]
5. Modifying the U-Boot[edit source]
This simple example adds unconditional log information when U-Boot starts. Within the scope of the trusted boot chain, U-Boot is used as second stage boot loader (SSBL).
- Have a look at the U-Boot log information when the board reboots
U-Boot <U-Boot version> CPU: STM32MP1 rev1.0 Model: STMicroelectronics STM32MP157C [...] Board: stm32mp1 in trusted mode [...]reboot [...]
- Go to the build directory
cd <build dir>
- Search U-boot recipe
devtool search u-boot*
u-boot-stm32mp-extlinux Generate 'extlinux.conf' file for U-boot
u-boot-stm32mp Universal Boot Loader for embedded devices for stm32mp
On this example, the recipe name is u-boot-stm32mp
- Start to work with u-boot
devtool modify u-boot-stm32mp
Example:
cd <build dir>/workspace/sources/u-boot-stm32mp
- Edit the ./board/st/stm32mp1/stm32mp1.c source file
- Add a log information in the checkboard function
printf("U-Boot simple example\n"); return 0; }int checkboard(void) { char *mode; [...] printf("Board: stm32mp1 in %s mode\n", mode);
- Cross-compile the U-Boot: trusted boot
devtool build u-boot-stm32mp
bitbake u-boot-stm32mp -c deploy
- Go to the directory in which the compilation results are stored
cd <build dir>/tmp-glibc/deploy/images/<machine name>/
- Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot: 0
STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
- On the host machine, check the partition associated with the secondary stage boot loader (ssbl): sdc3 here
ssbl -> ../../sdc3 lrwxrwxrwx 1 root root 10 Jan 17 18:05 userfs -> ../../sdc6ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 10 Jan 17 18:05 bootfs -> ../../sdc4 lrwxrwxrwx 1 root root 10 Jan 17 18:05 fsbl1 -> ../../sdc1 lrwxrwxrwx 1 root root 10 Jan 17 18:05 fsbl2 -> ../../sdc2 lrwxrwxrwx 1 root root 10 Jan 17 18:05 rootfs -> ../../sdc5 lrwxrwxrwx 1 root root 10 Jan 17 18:05
- Copy the binary (u-boot.stm32) to the dedicated partition
dd if=u-boot-<board name>-trusted.stm32 of=/dev/sdc3 bs=1M conv=fdatasync
(here u-boot-stm32mp157c-ev1-trusted.stm32 or u-boot-stm32mp157c-dk2-trusted.stm32)
- Reset the U-Boot shell
STM32MP> reset
- Have a look at the new U-Boot log information when the board reboots
U-Boot <U-Boot version> CPU: STM32MP1 rev1.0 Model: STMicroelectronics STM32MP157C [...] Board: stm32mp1 in trusted mode U-Boot simple example [...][...]
6. Modifying the TF-A[edit source]
This simple example adds unconditional log information when the TF-A starts. Within the scope of the trusted boot chain, TF-A is used as first stage boot loader (FSBL).
- Have a look at the TF-A log information when the board reboots
MPU (MPSYSRST) INFO: Using SDMMC [...]reboot [...] INFO: System reset generated by
- Go to the build directory
cd <build dir>
- Search TF-A recipe
Linux Trace Toolkit Control gettext Utilities and libraries for producing multi-lingual messages glibc GLIBC (GNU C Library) tf-a-stm32mp Trusted Firmware-A for STM32MP1 gnutls GNU Transport Layer Security Library gstreamer1.0 GStreamer 1.0 multimedia framework harfbuzz Text shaping library glibc-locale Locale data from glibc kbd Keytable files and keyboard utilitiesdevtool search tf-a* babeltrace Babeltrace - Trace Format Babel Tower libunistring Library for manipulating C and Unicode strings lttng-tools
On this example, the recipe name is tf-a-stm32mp
- Start to work with tf-a
devtool modify tf-a-stm32mp
- Go to <build dir>/workspace/sources/tf-a-stm32mp
cd <build dir>/workspace/sources/tf-a-stm32mp
- Edit the ./plat/st/stm32mp1/bl2_io_storage.c source file
- Add a log information in the stm32mp1_io_setup function
TF-A simple example"); [...] }void stm32mp1_io_setup(void) { int io_result; [...] /* Add a trace about reset reason */ print_reset_reason(); INFO("
- Cross-compile the TF-A
devtool build tf-a-stm32mp
bitbake tf-a-stm32mp -c deploy
- Go to the directory in which the compilation results are stored
cd <build dir>/tmp-glibc/deploy/images/<machine name>/
- Reboot the board, and hit any key to stop in the U-boot shell
reboot
[...]
Hit any key to stop autoboot: 0
STM32MP>
- Connect a USB cable between the host machine and the board via the USB OTG ports
- In the U-Boot shell, call the USB mass storage function
STM32MP> ums 0 mmc 0
- On the host machine, check the partition associated with the first stage boot loader (fsbl1 and fsbl2 as backup): sdc1 and sdc2 (as backup) here
sfsbl1 -> ../../sdc1 lrwxrwxrwx 1 root root 10 Jan 17 18:05 sfsbl2 -> ../../sdc2 lrwxrwxrwx 1 root root 10 Jan 17 18:05 rootfs -> ../../sdc5 lrwxrwxrwx 1 root root 10 Jan 17 18:05 ssbl -> ../../sdc3 lrwxrwxrwx 1 root root 10 Jan 17 18:05 userfs -> ../../sdc6ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 10 Jan 17 18:05 bootfs -> ../../sdc4 lrwxrwxrwx 1 root root 10 Jan 17 18:05
- Copy the binary (tf-a-stm32mp157c-ev1-trusted.stm32) to the dedicated partition; to test the new TF-A binary, it might be useful to keep the old TF-A binary in the backup FSBL (fsbl2)
dd if=tf-a-<board name>-trusted.stm32 of=/dev/sdc1 bs=1M conv=fdatasync
(here tf-a-stm32mp157c-ev1-trusted.stm32 or tf-a-stm32mp157c-dk2-trusted.stm32)
- Reset the U-Boot shell
STM32MP> reset
- Have a look at the new TF-A log information when the board reboots
MPU (MPSYSRST) INFO: TF-A simple example INFO: Using SDMMC [...][...] INFO: System reset generated by
7. Adding a "hello world" user space example[edit source]
This chapter shows how to compile and execute a simple "hello world" example.
- Create a directory for this user space example
mkdir hello_world_example
cd hello_world_example
- Create the source code file for this user space example: hello_world_example.c
// SPDX-identifier: GPL-2.0
/*
* Copyright (C) STMicroelectronics SA 2018
*
* Authors: Jean-Christophe Trotin <jean-christophe.trotin@st.com>
*
*/
#include <stdio.h>
#include <unistd.h>
int main(int argc, char **argv)
{
int i =11;
printf("\nUser space example: hello world from STMicroelectronics\n");
setbuf(stdout,NULL);
while (i--) {
printf("%i ", i);
sleep(1);
}
printf("\nUser space example: goodbye from STMicroelectronics\n");
return(0);
}
- Add a new recipe to the workspace
cd <build dir>
devtool add myhelloword hello_world_example/
- Adapt recipe
devtool edit-recipe myhelloword
- Modify the recipe according the following changes (see highlighted lines)
# Recipe created by recipetool
# This is the basis of a recipe and may need further editing in order to be fully functional.
# (Feel free to remove these comments when editing.)
# Unable to find any files that looked like license statements. Check the accompanying
# documentation and source headers and set LICENSE and LIC_FILES_CHKSUM accordingly.
#
# NOTE: LICENSE is being set to "CLOSED" to allow you to at least start building - if
# this is not accurate with respect to the licensing of the software being built (it
# will not be in most cases) you must specify the correct value before using this
# recipe for anything other than initial testing/development!
LICENSE = "CLOSED"
LIC_FILES_CHKSUM = ""
# No information for SRC_URI yet (only an external source tree was specified)
SRC_URI = ""
# NOTE: no Makefile found, unable to determine what needs to be done
do_configure () {
# Specify any needed configure commands here
:
}
do_compile () {
# Specify compilation commands here
cd ${S}
${CC} hello_world_example.c -o hello_word_example
}
do_install () {
# Specify install commands here
install -d ${D}${bindir}
install -m 755 ${S}/hello_word_example ${D}${bindir}/
}
- Compile binary
devtool build myhelloword
- Push this binary on board
devtool deploy-target -s myhelloword root@<board ip address>
- Execute this user space example
User space example: hello world from STMicroelectronics 10 9 8 7 6 5 4 3 2 1 0 User space example: goodbye from STMicroelectronics/usr/bin/hello_world_example
8. Tips[edit source]
8.1. Creating a mounting point[edit source]
The objective is to create a mounting point for the boot file system (bootfs partition)
- Find the partition label associated with the boot file system
bootfs -> ../../mmcblk0p4 lrwxrwxrwx 1 root root 15 Dec 13 12:31 fsbl1 -> ../../mmcblk0p1 lrwxrwxrwx 1 root root 15 Dec 13 12:31 fsbl2 -> ../../mmcblk0p2 lrwxrwxrwx 1 root root 15 Dec 13 12:31 rootfs -> ../../mmcblk0p5 lrwxrwxrwx 1 root root 15 Dec 13 12:31 ssbl -> ../../mmcblk0p3 lrwxrwxrwx 1 root root 15 Dec 13 12:31 userfs -> ../../mmcblk0p6ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 15 Dec 13 12:31
- Attach the boot file system found under /dev/mmcblk0p4 in the directory /boot
mount /dev/mmcblk0p4 /boot