Last edited 5 years ago

How to configure a wlan interface on hotspot mode

The printable version is no longer supported and may have rendering errors. Please update your browser bookmarks and please use the default browser print function instead.

1. Configure a wlan interface on hotspot mode[edit source]

  • Configure the wlan interface for systemd/netword

Add the following rule on /lib/systemd/network/

 cat /lib/systemd/network/hostapd.network
[Match]
Name=wlan0

[Network]
Address=192.168.72.1/24
DHCPServer=yes
IPForward=ipv4
IPMasquerade=yes

192.168.72.1/24: ip address affected to the hotspot device.

This configuration supports dhcpserver, ip forward and ip masquerade for this wlan interface: wlan0.

  • Create the hotspot configuration by replacing /etc/hostapd.config content by the following lines
 cat /etc/hostapd.conf
interface=wlan0
driver=nl80211
# mode Wi-Fi (a = IEEE 802.11a, b = IEEE 802.11b, g = IEEE 802.11g)
hw_mode=g
ssid=STExampleNetwork
channel=7
wmm_enabled=0
macaddr_acl=0
# Wi-Fi closed, need an authentication
auth_algs=1
ignore_broadcast_ssid=0
wpa=2
wpa_passphrase=ExamplePassphareNetwork
wpa_key_mgmt=WPA-PSK
wpa_pairwise=TKIP
rsn_pairwise=CCMP

STExampleNetwork is the visible name of the new wlan hotspot (SSID).

ExamplePassphareNetwork is the passphare associated to the wlan hotspot (SSID).

  • Correct one issue with systemd-networkd.service which does not enable the wifi link by default

Add the highlighted line in /lib/systemd/system/hostapd.service file

 cat /lib/systemd/system/hostapd.service
[Service]
ExecStartPre=/sbin/ip link set wlan0 up
ExecStart=/usr/sbin/hostapd /etc/hostapd.conf -P /run/hostapd.pid -B
  • Enable systemd service
 systemctl enable  hostapd

2. How to configure a gateway configuration[edit source]

For this example of configuration, the setup is:

  • wlan0: wireless interface connected to SSID_NETWORK with DHCP
  • eth0: ethernet interface with static IP which also have a DHCPserver on it
  • forward of packet are activated between the two network interfaces.

2.1. Configure wireless interface[edit source]

 cat /lib/systemd/network/wlan0.network
 [Match]
 Name=wlan0
  
 [Network]
 DHCP=ipv4
 IPForward=ipv4
IPForward
permit to forward all network packet from wireless network to other network.


Configure wireless interface for SSID_NETWORK network:

 mkdir -p /etc/wpa_supplicant/
 echo "ctrl_interface=/var/run/wpa_supplicant" > /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
 echo "eapol_version=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
 echo "ap_scan=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
 echo "fast_reauth=1" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
 echo "" >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
 wpa_passphrase SSID_NETWORK PASSWORD_NETWORK >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf
 or
 wpa_passphrase SSID_NETWORK  >> /etc/wpa_supplicant/wpa_supplicant-wlan0.conf

Where SSID_NETWORK PASSWORD_NETWORK correspond to the SSID and password of wireless network.

Enable the wireless configuration (to be take into account after reboot):

 systemctl enable wpa_supplicant@wlan0.service
         systemctl restart systemd-networkd.service
         systemctl restart wpa_supplicant@wlan0.service