deleted>Frq08942 mNo edit summary |
Registered User No edit summary |
||
(One intermediate revision by one other user not shown) | |||
Line 1: | Line 1: | ||
Some typical issues related to the '''GStreamer''' framework are listed below. Solutions or debugging methods are proposed for these issues. | Some typical issues related to the '''GStreamer''' framework are listed below. Solutions or debugging methods are proposed for these issues. | ||
Line 27: | Line 17: | ||
|| | || | ||
HDMI TV not connected, please connect it. | HDMI TV not connected, please connect it. | ||
|- | |||
| <pre>Could not load BMP file</pre> | |||
|| | |||
Make sure the loader of the bmp file format, libpixbufloader-bmp.so, is present in /usr/lib/gdk-pixbuf-2.0/2.10.0/. If not, remove /usr/lib/gdk-pixbuf-2.0/2.10.0/loaders.cache, copy libpixbufloader-bmp.so file from distrib build to /usr/lib/gdk-pixbuf-2.0/2.10.0/ then run "/usr/lib/gdk-pixbuf-2.0/gdk-pixbuf-query-loaders > /usr/lib/gdk-pixbuf-2.0/2.10.0/loaders.cache" to reload loaders. | |||
</onlyinclude> | </onlyinclude> | ||
|} | |} | ||
<noinclude> | |||
{{ArticleBasedOnModel | Troubleshooting grid article model}} | |||
{{PublicationRequestId | 10288 | 2019-01-15 | PhilipS}} | |||
[[Category:GStreamer]] | |||
[[Category:Troubleshooting grids]] | |||
</noinclude> |
Latest revision as of 11:44, 26 November 2019
Some typical issues related to the GStreamer framework are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try also looking in the articles in the Gstreamer or troubleshooting grids categories.
Symptom | Resolution |
---|---|
There may be a timestamping problem, or this computer is too slow. |
This message is typically displayed when the GStreamer A/V sync drops some frames. This may be due to a decoder that is too slow, badly timestamped buffers, or a badly formed container (.ts, .3gp, .mp4, .avi, ...). |
Could not create Wayland display |
HDMI TV not connected, please connect it. |
Could not load BMP file |
Make sure the loader of the bmp file format, libpixbufloader-bmp.so, is present in /usr/lib/gdk-pixbuf-2.0/2.10.0/. If not, remove /usr/lib/gdk-pixbuf-2.0/2.10.0/loaders.cache, copy libpixbufloader-bmp.so file from distrib build to /usr/lib/gdk-pixbuf-2.0/2.10.0/ then run "/usr/lib/gdk-pixbuf-2.0/gdk-pixbuf-query-loaders > /usr/lib/gdk-pixbuf-2.0/2.10.0/loaders.cache" to reload loaders. |