RTC device tree configuration

Revision as of 19:14, 20 November 2020 by Registered User
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

1. Article purpose[edit source]

This article explains how to configure the RTC internal peripheral when it is assigned to the Linux® OS. In this case, it is controlled by the RTC framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the RTC peripheral used by the STM32 RTC Linux driver.

2. DT bindings documentation[edit source]

The RTC is represented by the STM32 RTC device tree bindings[1]

3. DT configuration[edit source]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1. DT configuration (STM32 level)[edit source]

The RTC node is declared in the file stm32mp151.dtsi [2]. It describes the hardware register address, clocks and interrupts.

rtc: rtc@5c004000 {
	compatible = "st,stm32mp1-rtc";
	reg = <0x5c004000 0x400>;                               --> Register location and length
	clocks = <&rcc RTCAPB>, <&rcc RTC>;
	clock-names = "pclk", "rtc_ck";
	interrupts-extended = <&intc GIC_SPI 3 IRQ_TYPE_LEVEL_HIGH>,
			      <&exti 19 1>;
	status = "disabled";
};
Warning white.png Warning
This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.

3.2. DT configuration (board level)[edit source]

This part is used to enable the RTC used on a board, which is done by setting the status property to okay.

An "st,lsco" property is available to select and enable the RTC output on which RTC low-speed clock is output. The valid ouput values are defined in [3]. A pinctrl state named "default" can be defined to reserve a pin for the RTC output.

3.3. DT configuration examples[edit source]

#include <dt-bindings/rtc/rtc-stm32.h>
...
&rtc {
	st,lsco = <RTC_OUT2_RMP>;
	pinctrl-0 = <&rtc_out2_rmp_pins_a>;
	pinctrl-names = "default";
};

4. How to configure the DT using STM32CubeMX[edit source]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX might not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5. References[edit source]

Please refer to the following links for additional information: