How to manage OpenSTLinux project in STM32CubeIDE

Revision as of 11:06, 26 August 2020 by Registered User

This article explains how to import OpenSTLinux projects into STM32CubeIDE version 1.4.0 on Linux workstation.

1. Overview[edit source]

It is possible to import into an existing STM32MP15x Project some OpenSTLinux projects. This support is starting with OpenSTLinux version 2.0 a.k.a. 5.4-dunfell.

This is done thanks to Import an OpenSTLinux project... Cortex-A hierarchical project contextual menu.

OpenSTLinux Project Menu

2. OpenSTLinux Project Structure[edit source]

All the OpenSTLinux projects follow the same project structure approach with three main part:

  • Eclipse artifact, in order to ease project usage
  • build artifact, identifying clearly the project output
  • sources, as they appear in yocto environment
OpenSTLinux Project Structure

Device Trees generated by STM32CubeMX into DeviceTree/ directory of Cortex-A hierarchical project, are automatically included inside the corresponding OpenSTLinux project with:

  • source file links
  • dedicated Build target

3. Linux Project[edit source]

Several Build targets are proposed for linux project addressing Device Trees, module and kernel.

File:OSTL-SRC-Linux-Project-Structure.png
OpenSTLinux Linux Project Structure

Double click on Build target launches the corresponding compilation with associated Yocto SDK.

OpenSTLinux Linux Device Tree MX Build


4. U-Boot Project[edit source]

5. TF-A Project[edit source]

6. Optee Project[edit source]

Under construction.png Coming soon