X-LINUX-AI - image classification using TensorFlow Lite Python runtime

Revision as of 17:13, 23 June 2020 by Registered User (→‎Description)

This article explains how to experiment TensorFlow Lite[1] applications for image classification based on MobileNet v1 model using the TensorFlow Lite Python runtime.

Info white.png Information
Python applications are good for prototyping but are less efficient than C/C++ application

1. Description[edit source]

The image classification[2] neural network model allows identification of the subject represented by an image. It classifies an image into various classes.

Python TensorFlow Lite image classification application

The application enables OpenCV camera streaming (or test data picture) and the TensorFlow Lite[1] interpreter runing the NN inference based on the camera (or test data pictures) inputs.
It is a multi-process Python application that allow to run in parallel the camera preview (on the CPU core 0) and the neural network inference (using the CPU core 1).
The user interface is implemented using Python GTK.

The model used with this application is the MobileNet v1 downloaded from the Tensorflow Lite hosted models[3].

2. Installation[edit source]

2.1. Install from the OpenSTLinux AI package repository[edit source]

After having configured the AI OpenSTLinux package you can install the X-LINUX-AI components for this application:

 apt-get install tflite-cv-apps-image-classification-python

And restart the demo launcher:

 systemctl restart weston@root

2.2. Source code location[edit source]

The label_tfl_multiprocessing.py Python script is available:

  • in the Openembedded OpenSTLinux distribution with X-LINUX-AI expansion package:
<Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/image-classification/python/label_tfl_multiprocessing.py
  • on the target:
/usr/local/demo-ai/computer-vision/tflite-image-classification/python/label_tfl_multiprocessing.py
  • on GitHub:
https://github.com/STMicroelectronics/meta-st-stm32mpu-ai/tree/dunfell/recipes-samples/tflite-cv-apps/files/image-classification/python/label_tfl_multiprocessing.py

3. How to use it[edit source]

3.1. Launch application via the demo launcher[edit source]

Launch python tfl image classification.png

3.2. Or execute with command line[edit source]

The Python script label_tfl_multiprocessing.py application is located in the userfs partition:

/usr/local/demo-ai/computer-vision/tflite-image-classification/python/label_tfl_multiprocessing.py

It accepts the following input parameters:

usage: label_tfl_multiprocessing.py [-h] [-i IMAGE] [-v VIDEO_DEVICE] [--frame_width FRAME_WIDTH] [--frame_height FRAME_HEIGHT] [--framerate FRAMERATE]            
                                    [-m MODEL_FILE] [-l LABEL_FILE] [--input_mean INPUT_MEAN] [--input_std INPUT_STD]                                              
                                                                                                                                                                   
optional arguments:                                                                                                                                                
  -h, --help            show this help message and exit                                                                                                            
  -i IMAGE, --image IMAGE                                                                                                                                          
                        image directory with image to be classified                                                                                                
  -v VIDEO_DEVICE, --video_device VIDEO_DEVICE                                                                                                                     
                        video device (default /dev/video0)                                                                                                         
  --frame_width FRAME_WIDTH                                                                                                                                        
                        width of the camera frame (default is 320)                                                                                                 
  --frame_height FRAME_HEIGHT                                                                                                                                      
                        height of the camera frame (default is 240)                                                                                                
  --framerate FRAMERATE                                                                                                                                            
                        framerate of the camera (default is 15fps)                                                                                                 
  -m MODEL_FILE, --model_file MODEL_FILE                                                                                                                           
                        .tflite model to be executed                                                                                                               
  -l LABEL_FILE, --label_file LABEL_FILE                                                                                                                           
                        name of file containing labels                                                                                                             
  --input_mean INPUT_MEAN                                                                                                                                          
                        input mean                                                                                                                                 
  --input_std INPUT_STD                                                                                                                                            
                        input standard deviation

3.3. Testing with MobileNet V1[edit source]

The model used for test is the mobilenet_v1_0.5_128_quant.tflite downloaded from Tensorflow Lite hosted models[3]

To ease launching of the Python script, two shell scripts are available:

  • launch image classification based on camera frame inputs
 /usr/local/demo-ai/computer-vision/tflite-image-classification/python/launch_python_label_tfl_mobilenet.sh
  • launch image classification based on the pictures located in /usr/local/demo-ai/computer-vision/models/mobilenet/testdata directory:
 /usr/local/demo-ai/computer-vision/tflite-image-classification/python/launch_python_label_tfl_mobilenet_testdata.sh
Info white.png Information
Note that you need to populate the testdata directory with your own data sets.

The pictures are then randomly read from the testdata directory

4. References[edit source]