This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article provides the basic information required to start using the perfetto [1] Android™ tool.
1. Introduction[edit source]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
perfetto | Tracing tools | perfetto[1] is a performance instrumentation and tracing tool for Android™.
|
![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
2. Getting started with perfetto[edit source]
Perfetto instructions can be generated using the recording tool[2].
- Create record settings required
- Copy generated instructions
- Execute the copied instructions on a opened terminal with the device connected through USB, having ADB installed.
At the end of the trace execution, you can get back the trace:
adb pull /data/misc/perfetto-traces/trace
From this stage you can directly open the trace through the web viewer[3].
3. References[edit source]