How to exchange large data buffers with the coprocessor - principle

Revision as of 16:48, 5 November 2019 by Registered User

1. Introduction[edit source]

As explain In "How_to_exchange_buffers_with_the_Cortex-M_co-processor", the rpmsg protocol can not be enough efdficient to directly exchange large buffers between the Cortexes. In this case it is recommended to implement the indirect buffer exchange mode":

  • Create specific buffers to store the data to exchange,
  • use RPMsg to exchange reference to these buffers with the remote processor.

This article gives an example of mechanism that can be put in place to exchange indirect buffers between a main processor and a coprocessor.

2. Architecture overview[edit source]

This architecture example is relying on a the rpmsg_sdb linux driver.

Copro-sw-ipc-big-data.png

  • On Cortex-A:
  • The rpmsg_sdb driver implements on Linux side the service allocate and share buffers with the Cortex-M
  • the Linux Application directly access to the mmapped buffers.
  • On Cortex-M:
  • Application has to implement the "rpmsg-sdb-channel" rpmsg service to manage the buffer information.
  • a DMA can be used to transfer data to/from DDR.

For example, refer to How_to_exchange_big_data_between_Cortex-M4_and_Cortex-A7 article.

3. rpmsg_sdb driver[edit source]

The RPMsg shared data buffer driver example in in charge of:

  • allocating large buffers in DDR memory and mmap them for an application usage.
  • implementing the RPMsg service to share buffer with the remote processor.
  • send event to Linux Application when buffers are available ( on RPMsg related message reception)
Info white.png Information
This drivers is only provided as example, Only the transfer from Cortex-M to cortex-A is implemented in the rpmsg_sdb driver

3.1. Configuration[edit source]

3.1.1. Kernel configuration[edit source]

No kernel configuration is needed. The rpmsg_sdb Linux driver is proposed as module and can be installed thanks to the associated Yocto recipe.

3.1.2. Device tree[edit source]

No device tree device tree declaration is needed. The rpmsg_sdb driver is registered as a rpmsg driver. it is probed when the remote processor creates the "rpmsg-sdb-channel" service

3.2. How to use[edit source]

3.2.1. User space interface[edit source]

The rpmsg_sdb driver exposes a "/dev/rpmsg_sdb" sysfs that offers an interface to allocate and manage the shared buffers.

  • open/close: get/release file descriptor.
    fd= open('/dev/rpmsg_sdb');
    close(fd);
  • mmap: allocate and map memories
    buff0_id = mmap(size,fd);
    buff1_id = mmap(size,fd);
  • ioctrl
  • RPMSG_SDB_IOCTL_SET_EFD
register event for a buffer
    ioctrl(fd, RPMSG_SDB_IOCTL_SET_EFD, buff0_id, eventfd);
  • RPMSG_SDB_IOCTL_GET_DATA_SIZE
get the size of a buffer
    ioctrl(fd, RPMSG_SDB_IOCTL_GET_DATA_SIZE, buff0_id, eventfd);

3.2.2. RPMsg messaging[edit source]

The RPMsg protocol is used for the communication with the Cortex-M:

  • Information on buffer allocated and mmaped is sent to the Cortex-M.
The message is structured in a string with following format: "BxAyyyyyyyyLzzzzzzzz"
  • x: buffer index,
  • yyyyyyyy: address of the buffer in DDR ( 32 bits format),
  • zzzzzzzz: length of the buffer (32 bits format)
  • Buffer filled event received from the Cortex-M:
When the Cortex-M4 has filled a buffer it can inform the Linux Application by sending a RPMsg with following string Format : "BxLzzzzzzzz"'.
  • x: buffer index,
  • zzzzzzzz: length of the buffer (32 bits format)
On this message reception the rpmsg_sdb driver send an event to application ( if an event is associated to the buffer).
No categories assignedEdit