How to customize kernel for Android

Revision as of 09:37, 18 October 2019 by Registered User


1. Prerequisites[edit source]

The environment must be installed using the Distribution Package adapted to your microprocessor device. See the list of Android Distribution Package.

Get the kernel sources as explained in How to build kernel for Android.

To be able to execute the following instructions, go to your distribution root directory and initialize your environment as follows:

 source build/envsetup.sh
 bspsetup
 lunch aosp_<BoardId>-userdebug
Info white.png Information
The bspsetup command needs to be run only one time for the distribution

2. Updating the kernel configuration[edit source]

Info white.png Information

The kernel configuration file used is merged between the following files (this operation is performed at the beginning of the kernel build process):

  • The Android configuration files named android-base.config and android-recommended.config files available in the device/stm/<STM32Series>-kernel/source/kconfig/<kernel version>/ directory.
  • The android-soc.config file available in the device/stm/<STM32Series>-kernel/source/kconfig/<kernel version>/ directory.

By using menuconfig, you can adapt the configuration file to your needs. Some guidelines are given below.

2.1. Saving the current configuration[edit source]

Before changing the kernel configuration, it is recommended to build the kernel using the current configuration:

 build_kernel

A default config file named defconfig.default is generated in out-bsp/<STM32Series>/KERNEL_OBJ/ directory.

2.2. Creating a new kernel configuration[edit source]

Start menuconfig:

 build_kernel menuconfig

You can load a .config file and modify any entry using this interface. Please read on the top of the windows the instructions to navigate.

Do not forget to click save.

This generates a .config file located in out-bsp/<STM32Series>/KERNEL_OBJ/, as well as a defconfig file at the same location.

2.3. Testing the new kernel configuration[edit source]

To test the new configuration, rebuild the kernel, and then update the prebuilts and flash, as explained in in How to build kernel for Android.

2.4. Applying the newly generated kernel configuration[edit source]

To make your change permanent, first compare the new defconfig file with the defconfig.default file generated at first build.

You can use a graphical tool such as meld.

 meld out-bsp/<STM32Series>/KERNEL_OBJ/defconfig out-bsp/<STM32Series>/KERNEL_OBJ/defconfig.default


Then report the changes into the android-soc.config file located in device/stm/<STM32Series>-kernel/source/kconfig/<kernel version>/.

Eventually force the regeneration of the .config:

 build_kernel defaultconfig

Note: the defconfig.default is then updated.

To test your configuration, rebuild the kernel and update the prebuilts and flash, as explain in How to build kernel for Android.

3. Changing the kernel command line[edit source]

You can customize the kernel command line call at boot time. The arguments are defined in the BoardConfig.mk file located in device/stm/<STM32Series>/<BoardId>/.

Adapt the value of the BOARD_KERNEL_CMDLINE variable to your needs.

Rebuild the bootimage to apply the changes:

 make bootimage-nodeps

Then flash the boot partition:

Info white.png Information
To control the command line after compilation you can execute:
 ./system/core/mkbootimg/unpack_bootimg --boot_img out/target/product/<BoardId>/boot.img

Check the "command line args" value from the output: it must match your changes.

4. Changing the Device Tree[edit source]

The kernel device tree used is set in the dt.mk file available in the device/stm/<STM32Series>/build/tasks/ directory. For more information refer to the Device tree and How to create your board device tree pages.

The device trees are located inside the Linux® kernel source code previously loaded. A Device Tree can be modified directly in device/stm/<STM32Series>-kernel/linux-<STM32Series>/arch/arm/boot/dts.

Once the Device Tree has been modified, rebuild the device tree:

 build_kernel -i dtb

 make -j

Then flash again the DT partition: