1. Article purpose[edit source]
This article is intended for Developer Package users (see Which Package better suits your needs for more information).
This article explains how to use the CoproService which is a SystemService embedded in the Android framework, allowing to use a serial connection to communicate with the Cortex M4 MPU embedded in a compatible hardware board.
See STM32MPU Embedded Software for Android architecture overview to get more information on compatible hardware boards.
2. Prerequisites[edit source]
The used environment stems from the installed Developer Package adapted to your selected microprocessor device. See the list of Android distribution Packages here.
The firmware built for the Cortex M4 has to use RemoteProc and RPMSG, and has to instantiate a /dev/ttyRPMSG
unit during its initialization.
3. CoproService[edit source]
CoproService is composed of 2 parts: Firmware management and TTY management.
3.1. Firmware management[edit source]
The Cortex M4 can be used to offload real time algorithms (such as MotorControl), support connectivity mediums (like LORA), etc.
Users will develop their Firmwares thanks to the CubeMX and SW4STM32 tools.
The Firmware will be embedded in the Android vendor partition in the /vendor/firmware/copro/
directory.
The CoproService will look at the contents of /vendor/firmware/copro/
to get the list of available firmwares. It will then load the requested firmware at the user's/application's request.
3.2. TTY management[edit source]
When the firmware is loaded and running, a /dev/ttyRPMSG0
driver is available to communicate with the Cortex M4.
It is up to users to define and write their own protocol on top of ttyRPMSG0
.
Application will then be able to:
- open
ttyRPMSG0
- write to
ttyRPMSG0
- read from
ttyRPMSG0
- close
ttyRPMSG0
4. API[edit source]
4.1. CoproManager API[edit source]
The CoproManager API gives access to the Firmware management.
CoproManager getInstance()
: Get the instance of the availableCoproManager
to start using it.FirmwareInfo[] getFirmwareList()
: Return the list of available firmwares present in/vendor/firmware/copro/
FirmwareInfo getFirmwareByName(String name)
: Looks up a firmware by its name in the/vendor/firmware/copro/
folder and returns all useful information about it, overwise returnsnull
.boolean isFirmwareRunning(int id)
: Returnstrue
if the Firmware of identifierid
is running, otherwise returnsfalse
.void startFirmware(int id)
: Starts the Firmware defined by its identifierid
.void stopFirmware()
: Stop any running FirmwareICoproSerialPort getSerialPort()
: Get access toCoproSerialPort
to interact with the Firmware. See below for more info.
4.2. FirmwareInfo API[edit source]
The FirmwareInfo API gives information about Firmwares.
int getId()
: get the ID given by the CoproService to this FirmwareString getName()
: get the file name of this Firmwareboolean getState()
: returns the state of the Firmware at the moment of the call: running (true
) or stopped (false
).
4.3. CoproSerialPort API[edit source]
The CoproSerialPort API gives access to the /dev/ttyRPMSG0
driver available when a Firmware is running. It allows the application to open and close the interface and also to send and receive data.
void open(int mode)
: opens a file descriptor to/dev/ttyRPMSG0
with the given mode : 0 for normal mode, 1 for raw modevoid close()
: closes the file descriptor to/dev/ttyRPMSG0
String read()
: reads available bytes if the file descriptor is open, overwise an empty string is returned.void write(String command)
: write the given "command" to the file descriptor.
5. Developping a Copro application[edit source]
In order to build the application, make sure you are using the appropriate Android SDK including CoproService How to build and install an SDK.
In Android Studio create a new application.
Then, do not forget to select the right API level in the application Manifest, in order to be sure that CoproService is available.
To use the CoproService you need to get the instance to the CoproManager, then you will be able to use the CoproManager API defined above:
CoproManager mCoproManager = CoproManager.getInstance();
To be able to communicate with the running Firmware you need to get a CoproSerialPort from CoproManager, then you will be available to use the CoproSerialPort API defined above :
ICoproSerialPort mCoproSerialPort = mCoproManager.getSerialPort();
The serial communication is possible only if a Firmware is running. Make sure to close the serial communication when you stop a firmware and open it when you start one.