NVMEM overview


Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


SUMMARY

This article introduces how NVMEM Linux® framework manages BSEC OTP data and how to read/write from/to it.

1. Framework purpose[edit source]

The NVMEM Linux® framework provides a generic interface for the device non-volatile memory data such as:

  • OTP (one-time programmable) fuses
  • EEPROM

It offers kernel space and user space interfaces to read and/or write data such as analog calibration data or MAC address.

2. System overview[edit source]

NVMEM sysfs interfaceNVMEM consumers interfaceBSEC internal peripheral
NVMEM system overview

Template:WarningImageMapOverlay

2.1. Component description[edit source]

  • NVMEM user (user space)

The user can use the NVMEM sysfs interface, from a user terminal or a custom application, to read/write data from/to NVMEM device(s) from user space.

  • NVMEM user (kernel space)

User drivers can use the NVMEM API to read/write data from/to NVMEM device(s) from kernel space (such as the analog calibration data used by an ADC driver).

  • NVMEM framework (kernel space)

The NVMEM core provides sysfs interface and NVMEM API. They can be used to implement NVMEM user and NVMEM controller drivers.

  • NVMEM drivers (kernel space)

Provider drivers such as BSEC Linux® driver that exposes OTP data to the core.

  • NVMEM hardware

NVMEM controller(s) such as the BSEC internal peripheral[1]

2.2. API description[edit source]

The NVMEM kernel documentation[2] describes:

  • Kernel space API for NVMEM providers and NVMEM consumers.
  • Userspace binary interface (sysfs).

See also sysfs-bus-nvmem[3] ABI documentation.

3. Configuration[edit source]

3.1. Kernel configuration[edit source]

Activate NVMEM framework in the kernel configuration through the Linux® menuconfig tool, Menuconfig or how to configure kernel (CONFIG_NVMEM=y):

Device Drivers  --->
   [*] NVMEM Support  --->

3.2. Device tree configuration[edit source]

The NVMEM data device tree bindings[4] describe:

  • The location of non-volatile memory data
  • The NVMEM data providers
  • The NVMEM data consumers

4. How to use the framework[edit source]

4.1. How to use NVMEM with sysfs interface[edit source]

The available NVMEM devices can be listed in sysfs:

 ls /sys/bus/nvmem/devices/                                            # Example to list nvmem devices
stm32-romem0

The data content of an NVMEM device can be dumped to a binary file, and then displayed.

For the Basic boot chain (using U-Boot SPL), it is impossible to access any upper NVMEM information because SMC feature is not available (CONFIG_HAVE_ARM_SMCCC).

 dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file bs=4 count=32                  # Example to read lower nvmem data content
 hexdump -C -v /tmp/file                  # Example to display nvmem data content

For the Trusted boot chain (using TF-A), SMC feature is available. It is then possible to access to some upper NVMEM information, only if access is authorized by the device tree configuration. This is the case of the MAC address, presented below.

 dd if=/sys/bus/nvmem/devices/stm32-romem0/nvmem of=/tmp/file skip=57 bs=4 count=2 status=none                  # Example to read MAC address
 hexdump -C -v /tmp/file                  # Example to display MAC address

Note that a specific chapter of the reference manual is dedicated to OTP mapping, in which information is detailed.

Warning white.png Warning
The below examples show how to write data to an NVMEM device. This may cause unrecoverable damage to the STM32 device (for example when writing to an OTP area)

Whatever the boot chain, the full lower NVMEM data content can be written as follows (if we suppose it has been previously read as described above, and updated directly in /tmp/file):

 dd if=/tmp/file of=/sys/bus/nvmem/devices/stm32-romem0/nvmem bs=4 count=32                  # Example to write lower nvmem data content

Only on Trusted boot chain, and under the condition the device tree authorizes it, an upper NVEM information can be written.
Example of 32-bit data word writing (filling it with ones) in OTP n°95:

 dd if=/dev/zero count=1 bs=4 | tr '\000' '\377' > file                # Create a 4 bytes length file filled with ones, e.g. 0xffffffff)
 dd if=file bs=4 seek=95 of=/sys/bus/nvmem/devices/stm32-romem0/nvmem  # Write it (32-bits, e.g. 4bytes) to OTP data 95

Note that when using this SYSFS interface, it may be necessary to reboot board when new OTP value is written. Actually, it is not sure the OTP value can be read directly after a write because OTP value is read in shadow area not directly in OTP area.

5. How to trace and debug the framework[edit source]

5.1. How to trace[edit source]

Ftrace can be used to trace the NVMEM framework:

 cd /sys/kernel/debug/tracing
 cat available_filter_functions | grep nvmem                           # Show available filter functions
rtc_nvmem_register
rtc_nvmem_unregister
nvmem_reg_read
bin_attr_nvmem_read
...

Enable the kernel function tracer, then start using nvmem and display the result:

 echo function > current_tracer
 echo "*nvmem*" > set_ftrace_filter                                    # Trace all nvmem filter functions
 echo 1 > tracing_on                                                   # start ftrace
 hexdump -C -v /sys/bus/nvmem/devices/stm32-romem0/nvmem               # dump nvmem
00000000  17 00 00 00 01 80 00 00  00 00 00 00 00 00 00 00  |................|
...
 echo 0 > tracing_on                                                   # stop ftrace
 cat trace
# tracer: function
#
#                              _-----=> irqs-off
#                             / _----=> need-resched
#                            | / _---=> hardirq/softirq
#                            || / _--=> preempt-depth
#                            ||| /     delay
#           TASK-PID   CPU#  ||||    TIMESTAMP  FUNCTION
#              | |       |   ||||       |         |
         hexdump-478   [000] ....   423.502278: bin_attr_nvmem_read <-sysfs_kf_bin_read
         hexdump-478   [000] ....   423.502290: nvmem_reg_read <-bin_attr_nvmem_read
         hexdump-478   [000] ....   423.515804: bin_attr_nvmem_read <-sysfs_kf_bin_read

6. References[edit source]