STM32MP15 device tree

Revision as of 18:00, 29 June 2020 by Registered User (→‎Introduction)

1. Purpose and scope[edit source]

This article shows the structure of the device tree files as it is implemented in STM32MP15 for the following software components: Linux® kernel, U-Boot, TF-A and OP-TEE.

The purpose of this article is not to explain the device tree concept and the device tree configuration supported by STM32MP15. A good knowledge of the concept is a prerequisite before reading this article. The articles regarding the configuration can be read afterwards.

2. Device tree structure for Linux, U-Boot, TF-A and OP-TEE[edit source]

2.1. Introduction[edit source]


The device tree files are used during boot time by the FSBL (TF-A), the secure OS (OP-TEE), the SSBL (U-Boot) and eventually by the Linux kernel.

These files are stored in different repositories, but source code reuse is maximized from one repository to another:

  • The initial device tree files supporting STM32MP15 are created in the Linux kernel.
  • In U-Boot, Linux files are copied and overloaded with U-Boot properties (including DDR configuration).
    • The source code path is arch/arm/dts/stm32mp15* .
    • The U-Boot add-ons file, "<dts-file-name>-u-boot.dtsi", is automatically included at the end of "<dts-file-name>.dts" during device tree compilation (this is a generic U-Boot Makefile behavior).
  • In TF-A, Linux files are partly copied (for device tree blob size optimization) and completed with the security configuration (firewalling), and the DDR configuration is also added (same files as U-Boot).
  • In OP-TEE, TF-A files are reused, except the DDR configuration ones.

The figure below shows the device tree creation flow for Linux, U-Boot, TF-A and OP-TEE:

Device tree for Linux U-Boot TF-A OP-TEE.png

Color legend:

  •  Linux  in dark blue
  •  U-Boot  add-ons in green
  •  TF-A  add-ons in pink
  •  STM32CubeMX generated parts  in light blue

The above color codes are used for all the figures included in this article.


2.2. Upstreamed device tree[edit source]

2.2.1. Overview[edit source]

As explained in the STM32 MPU Embedded Software Open Source Software (OSS) philosophy, STMicroelectronics maximizes the usage of open source software and the upstreaming to the communities.

So, the device tree files supporting the evaluation board and the Discovery kit are upstreamed to their official respective repositories. But waiting for the upstream process completion, STMicroelectronics latest contributions are available in advance on github in Linux , U-Boot , TF-A and OP-TEE repositories.

Info white.png Information
The figures shown below are reflecting the current implementation on github and they may be somehow in advance compare to the upstreamed version for all parts that are still under review.
Info white.png Information
For the sake of simplicity, the figures below only show the dtsi & dts files structure, without showing the h files that are also included.
Info white.png Information
The dtb files, resulting from the compilation with the dtc compiler, may be named differently when the compilation is launched with the Distribution Package.

2.2.2. Linux[edit source]

Device tree Linux upstreamed.png
Device tree legend.png


2.2.3. U-Boot[edit source]

Device tree U-Boot upstreamed.png
Device tree legend.png


Info white.png Information
'<board>-u-boot.dtsi' file inclusion at the end of '<board>.dts' file is not explicit (#include ...) but realized via an U-Boot generic mechanism (see README )

2.2.4. TF-A[edit source]

Device tree TF-A upstreamed.png
Device tree legend.png


Note: The hashed areas on Linux device tree files represent the fact that these files are partly copied in TF-A.


2.2.5. OP-TEE[edit source]

Device tree OP-TEE upstreamed.png
Device tree legend.png


Note: The hashed areas on Linux device tree files represent the fact that these files are partly copied in OP-TEE.


2.3. STM32CubeMX generated device tree[edit source]

2.3.1. Overview[edit source]

STM32CubeMX can be used to generate the device tree files for a given project. The tool generates the files  highlighted in light blue  in the following diagrams, including the upstreamed files shown in the previous chapter.

The device tree files generated by STM32CubeMX can be built with the Developer Package or Distribution Package:

2.3.2. Linux[edit source]

Device tree Linux STM32CubeMX.png



2.3.3. U-Boot[edit source]

Device tree U-Boot STM32CubeMX.png


2.3.4. TF-A[edit source]

Device tree TF-A STM32CubeMX.png


2.3.5. OP-TEE[edit source]

STM32CubeMX does not generate a dedicated file for OP-TEE but TF-A generated files can be reused, as seen earlier in this article. In order to minimize OP-TEE device tree file, it is recommended to remove the inclusion of the DDR configuration files, that are useless for OP-TEE.