1. Article purpose[edit source]
This article explains how to configure the QUADSPI internal peripheral and FMC internal peripheral connected to a flash device when it is assigned to the TF-A BL2. In that case, it is controlled by new TF-A frameworks:
- SPI NOR
- SPI NAND
- SPI MEM
- FMC NAND
These frameworks represents the memory access organisation.
These frameworks use two different configurations:
If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.
2. Framework overview[edit source]
2.1. Components description[edit source]
- IO_Storage
The IO storage provides an abstraction layer to access storage devices.
- Boot device configuration
The Boot device configuration is a platform specific ad-dons to specify memory specific settings.
- MTD core
The MTD core provides an abstraction layer for raw Flash memories.
- Raw NAND subsystem
The Raw NAND protocol is used in the MTD subsystem for interfacing NAND Flash memories.
- SPI-MEM subsystem
The SPI-MEM protocol is used in the MTD subsystem for interfacing all kinds of SPI memories (NORs, NANDs)
- SPI-NAND subsystem
The SPI-NAND protocol is used in the MTD subsystem for interfacing SPI NAND Flash memories.
- SPI-NOR subsystem
The SPI-NOR protocol is used in the MTD subsystem for interfacing SPI NOR Flash memories.
- FMC driver / FMC (Hardware)
Please refer to the FMC internal peripheral.
- QUADSPI driver / QUADSPI (Hardware)
Please refer to the QUADSPI internal peripheral.
3. DT configuration[edit source]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.
Pinctrl device tree configuration (and optionally to Pinctrl overview) must be added in #DT configuration (board level).
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
4. Raw NAND flash memory[edit source]
4.1. Raw NAND DT configuration[edit source]
For the DT bindings, refers to FMC_device_tree_configuration.
For the DT configuration (STM32 level), refers to FMC DT Configuration at STM32 level.
For the DT configuration (board level), refers to FMC DT Configuration at board level.
4.2. Raw NAND device configuration[edit source]
Raw NAND access will use the MTD Core and raw NAND framework. Some additional parameters are required by the raw NAND framework to address the memory:
- Page size
- Block size
- Blocks number in device
- NAND width (8 or 16 bits)
- ECC : Supported algorithm (BCH8/BCH4/Hamming are available). The default ECC framework configuration is no error correction.
Some memories are ONFI[1] compliant. In that case, required parameters can be directly read from the parameter description table.
For the others, user must properly fill out OTP configuration.
4.2.1. Raw NAND examples[edit source]
- 8bit NAND with 4KB paged / 256KB erase size / 1024MB size, ECC BCH8
OTP Word 9 : 0xA0818000
Param in OTP | Page size | Block size | Block numbers (N * 256) | Width | ECC | |||||||||||||||||||||||||
1 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
- Raw Nand ONFI with ECC override (Default from parameter table is BCH8, force to BCH4).
OTP Word 9 : 0x8000
Param in OTP | Page size | Block size | Block numbers (N * 256) | Width | ECC | |||||||||||||||||||||||||
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
- 16bit NAND with 2KB paged / 512KB erase size / 2048MB size, with On die ECC
OTP Word 9 : 0x91060000
Param in OTP | Page size | Block size | Block numbers (N * 256) | Width | ECC | |||||||||||||||||||||||||
1 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
5. SPI NAND flash memory[edit source]
5.1. SPI NAND DT configuration[edit source]
For the DT bindings, refers to the QUADSPI_device_tree_configuration.
For the DT configuration (STM32 level), refers to QUADSPI DT Configuration at STM32 level.
For the DT configuration (board level), refers to QUADSPI DT Configuration at board level.
5.2. SPI NAND device configuration[edit source]
SPI NAND and SPI MEM frameworks are used to address such memories.
- SPI NAND framework required additional parameters:
- Page size
- Block size
- Blocks number in device
- Plane number
These parameters must be properly filled out by user in OTP configuration.
- SPI MEM framework is used to send commands.
By default, the generic read command used is the legacy command:
0x03 with 1 line command, 1 line address, 1 data bus width (1_1_1).
It is possible to override this read command to improve performance access to the memory using platform configuration.
5.2.1. SPI NAND example[edit source]
- SPI NAND with 2KB paged / 256KB erase size / 1024MB size, 2 Planes
OTP Word 9 : 0x88804000
Param in OTP | Page size | Block size | Block numbers (N * 256) | Not Used | Not Used | 2 Planes | ||||||||||||||||||||||||
1 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
- Update read command to use command 0x6B (1_1_4) define in platform file[2]
device->spi_read_cache_op.cmd.opcode = SPI_NAND_OP_READ_FROM_CACHE_4X; device->spi_read_cache_op.cmd.buswidth = SPI_MEM_BUSWIDTH_1_LINE; device->spi_read_cache_op.addr.nbytes = 2U; device->spi_read_cache_op.addr.buswidth = SPI_MEM_BUSWIDTH_1_LINE; device->spi_read_cache_op.dummy.nbytes = 1U; device->spi_read_cache_op.dummy.buswidth = SPI_MEM_BUSWIDTH_1_LINE; device->spi_read_cache_op.data.buswidth = SPI_MEM_BUSWIDTH_4_LINE; device->spi_read_cache_op.data.dir = SPI_MEM_DATA_IN;
6. SPI NOR flash memory[edit source]
6.1. SPI NOR DT configuration[edit source]
For the DT bindings, refers to the QUADSPI_device_tree_configuration.
For the DT configuration (STM32 level), refers to QUADSPI DT Configuration at STM32 level.
For the DT configuration (board level), refers to QUADSPI DT Configuration at board level.
6.2. SPI NOR device configuration[edit source]
SPI NOR and SPI MEM frameworks are used to address such memories.
- SPI NOR framework required additional parameters:
- Device size
This parameters need to be defined in the platform configuration file<ref_name="boot_device">.
- SPI MEM framework is used to send commands.
By default, the generic read command used is the legacy command:
0x03 with 1 line command, 1 line address, 1 data bus width (1_1_1).
It is possible to override this read command to improve performance access to the memory using platform configuration.
6.2.1. SPI NOR example[edit source]
- SPI NOR 64MB size
device->size = SZ_64M; --> Device size
- Update read command to use command 0x6B (1_1_4) define in platform file[2]
device->read_op.cmd.opcode = SPI_NOR_OP_READ_1_1_4; device->read_op.cmd.buswidth = SPI_MEM_BUSWIDTH_1_LINE; device->read_op.addr.nbytes = 3U; device->read_op.addr.buswidth = SPI_MEM_BUSWIDTH_1_LINE; device->read_op.dummy.nbytes = 1U; device->read_op.dummy.buswidth = SPI_MEM_BUSWIDTH_1_LINE; device->read_op.data.buswidth = SPI_MEM_BUSWIDTH_4_LINE; device->read_op.data.dir = SPI_MEM_DATA_IN;
7. How to configure the DT using STM32CubeMX[edit source]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.
8. References[edit source]
Please refer to the following links for additional information: