STM32MP15 RAM mapping

Revision as of 12:32, 27 November 2019 by Registered User (→‎How to do that in pratice)


1. Overview[edit source]

This article shows the default memory mapping defined by STMicroelectronics in STM32MPU Embedded Software. It uses a subset of all memory regions that are exposed at hardware level: customers may use other memory regions or aliases that are not shown here but are described in the STM32MP15 reference manuals.

2. Arm core characteristics[edit source]

Integration of Arm cores sets some constraints on the device memory mapping: the main ones are listed in this article.

2.1. Reset address[edit source]

Arm® Cortex® cores start running from address 0x00000000 on reset, which is why this address respectively points to:

  • The ROM code on the Cortex-A7 side. This read-only memory embeds the boot code that is executed when the platform boots (and executes the boot chain) or wakes up from low power STANDBY mode.
  • The Retention RAM on the Cortex-M4 side. This needs to be loaded by the Cortex-A7 before releasing the Cortex-M4 reset (in the RCC) and getting it running. This is done by Linux coprocessor management, by default.

Note: since the Cortex-A7 has its ROM code mapped at address 0x00000000, it uses a hardware alias to access the retention RAM at address 0x38000000

2.2. Cortex-M4 multiple ports[edit source]

The Cortex-M4 is connected to the interconnect (ML-AHB) via three ports, listed below and shown in the following figure:

  • I-bus is used to fetch code instructions in the 0x00000000--0x1FFFFFFF address range
  • D-bus is used to read/write data in the 0x00000000--0x1FFFFFFF address range
  • S-bus is used for all accesses in the 0x20000000--0xFFFFFFFF address range; all STM32MP15 internal peripherals registers are mapped in this range.

Cortex-M4 ports.png


Balancing the Cortex-M4 firmware accesses among those ports allows tuning of the system performance, which is why the MCU SRAM is defined in the first address range (from 0x10000000), but is also visible in the second range (from 0x30000000) in the STM32MP15 reference manuals.

Nevertheless, it is important to notice that the Cortex-M4 embedded in the STM32MP15 only allows hardware breakpoints to be set on the address range covered by the I-bus. Thus any code accessed via the S-bus has to be debugged through software breakpoints.

3. Memory mapping[edit source]

3.1. Overall memory mapping[edit source]

The memory mapping below is a subset of all regions that are exposed at hardware level: it shows the default configuration used in OpenSTLinux but the customer may choose a different mapping to take advantage of other address ranges defined in STM32MP15 reference manuals.


DDRBackup registersBKPSRAMCAN SRAMRETRAMRETRAMSYSRAMMCU SRAMMCU SRAMROM
STM32MP15 memory mapping



3.2. Zoom in the Cortex-A7/Cortex-M4 shared memory[edit source]

The figure below is a zoom of the RAM areas that are shared between the Cortex-A7 non-secure and the Cortex-M4. This mapping is STMicroelectronics' default implementation that can be freely adapted by customers to fit to other needs.

Shared RAM memory mapping.png


3.3. Possible customization of internal RAM[edit source]

As described in https://wiki.st.com/stm32mpu/wiki/MCU_SRAM_internal_memory, ST has defined a memory mapping to be able to enable all the possible use cases in parallel but this can be changed depending on customer use cases.

3.3.1. Overview[edit source]

  • RETRAM is used for low power (code + data) and vector table. If not used for low power all this section can be used for any purpose (except the vector table).
  • SRAM1 (Code) and SRAM2 (Data) sizes can be tuned depending on user needs to better use physical area of 256KB.
  • SRAM3 (IPC Buffers) can be used for other purpose if IPC is not used
  • SRAM4 (dma) can be used for other purpose if dma1 and dma2 is not used in chained mode (only used in linux side)

3.3.2. How to do that in pratice[edit source]

  • RETRAM
- Linux: (mapped @:0x38000000)
	retram: retram@0x38000000 {
	compatible = "shared-dma-pool";
	reg = <0x38000000 0x10000>;
	no-map;
	};
- M4 ressource (mapped @:0x00000000)
&m4_rproc {
	memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>,
			<&vdev0vring1>, <&vdev0buffer>;
	ranges =  <0x00000000 0x38000000 0x10000>,
			 <0x30000000 0x30000000 0x60000>,
			 <0x10000000 0x10000000 0x60000>;
  • SRAM4 can be freed for M4 code by removing DTS declarations in Linux (64KB starting at 0x10050000):
	sram: sram@10050000 {
		compatible = "mmio-sram";
		reg = <0x10050000 0x10000>;
		#address-cells = <1>;
		#size-cells = <1>;
		ranges = <0 0x10050000 0x10000>;

		dma_pool: dma_pool@0 {
			reg = <0x0 0x10000>;
			pool;
		};
	};
&dma1 {
	sram = <&dma_pool>;
};

&dma2 {
	sram = <&dma_pool>;
};
  • SRAM3 (64KB starting at 0x10040000):
- Linux:
		vdev0vring0: vdev0vring0@10040000 {
			compatible = "shared-dma-pool";
			reg = <0x10040000 0x2000>;
			no-map;
		};

		vdev0vring1: vdev0vring1@10042000 {
			compatible = "shared-dma-pool";
			reg = <0x10042000 0x2000>;
			no-map;
		};

		vdev0buffer: vdev0buffer@10044000 {
			compatible = "shared-dma-pool";
			reg = <0x10044000 0x4000>;
			no-map;
		};
- M4 Cube:

Must be aligned with cube linker script definition (.ld):

MEMORY
{
    m_ipc_shm    (RW)  : ORIGIN = 0x10040000, LENGTH = 0x00008000
}
  • SRAM2 & 1 (256KB starting at 0x10000000):
- Linux (only one section declared from linux (code + data)):
	mcuram2: mcuram2@0x10000000 {
		compatible = "shared-dma-pool";
		reg = <0x10000000 0x40000>;
		no-map;
	};
- M4 ressource (mapped @:0x10000000)
&m4_rproc {
	memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&vdev0vring0>,
			<&vdev0vring1>, <&vdev0buffer>;

	ranges = <0x00000000 0x38000000 0x10000>,
			 <0x30000000 0x30000000 0x60000>,
			 <0x10000000 0x10000000 0x60000>;
- M4 Cube:

Must be aligned with cube linker script definition (.ld):

MEMORY
{
    m_text       (RX)  : ORIGIN = 0x10000000, LENGTH = 0x00020000
    m_data       (RW)  : ORIGIN = 0x10020000, LENGTH = 0x00020000
}