How to exchange large data buffers with the coprocessor - principle

Revision as of 13:01, 5 November 2019 by Registered User (Created page with "== Introduction == As explain In "How_to_exchange_buffers_with_the_Cortex-M_co-processor", the rpmsg protocol can not be adapted to exchange buffers between the cortexes....")
(diff) ← Older revision | Latest revision (diff) | Newer revision → (diff)

1. Introduction[edit source]

As explain In "How_to_exchange_buffers_with_the_Cortex-M_co-processor", the rpmsg protocol can not be adapted to exchange buffers between the cortexes. In this case it is recommended to implement the indirect buffer exchange mode":

  • create extra buffers to store the data,
  • use rpmsg to transmit reference to these buffers to the remote processor.

This article gives an example of mechanism that shall be put in place to exchange indirect buffers between a main processor and a coprocessor.

2. architecture overview[edit source]

This example is relying on a the rpmsg_sdb linux driver.

Copro-sw-ipc-big-data.png

  • On Cortex-A: The rpmsg_sdb driver implements on Linux side the service allocate and share buffers with the Cortex-M
  • On Cortex-M: Application as to implement the "rpmsg-sdb-channel" rpmsg service to exchange the buffer information. For example, refer to How_to_exchange_big_data_between_Cortex-M4_and_Cortex-A7 article.

3. rpmsg_sdb driver[edit source]

The rpmsg shared data buffer driver example implements mechanisms to:

  • allocate large buffers in DDR memory
  • implement RPMsg service to share buffer with the remote processor.
  • send event to Linux Application when buffers are available
Info white.png Information
This drivers is only provided as example, Only the transfer from Cortex-M to cortex-A is implemented in the rpmsg_sdb driver

3.1. Configuration[edit source]

3.1.1. Kernel configuration[edit source]

No kernel configuration is needed. The rpmsg_sdb Linux driver is proposed as module and can be installed thanks to the associated Yocto recipe.

3.1.2. Device tree[edit source]

No device tree device tree declaration is needed. The rpmsg_sdb driver is registered as a rpmsg driver. it is probed when the remote processor creates the "rpmsg-sdb-channel" service

3.2. How to use[edit source]

3.2.1. User space interface[edit source]

The rpmsg_sdb driver exposes a "/dev/rpmsg_sdb"sysfs that offers interface to allocate and manage the shared buffers.

  • open/close: gete/release file descriptor.

fd= open('/dev/rpmsg_sdb'); close(fd);

  • mmap: allocate and map memoryioctrl

buff0_id = mmap(size,fd); buff1_id = mmap(size,fd);

  • ioctrl
  • RPMSG_SDB_IOCTL_SET_EFD
register event for a buffer
ioctrl(fd, buff0_id, eventfd);
  • RPMSG_SDB_IOCTL_GET_DATA_SIZE

3.2.2. RPMsg messaging[edit source]

No categories assignedEdit