This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Article Purpose[edit source]
The purpose of this article is to explain how to integrate the NFC05A1 expansion board with STM32MP157C-DK2, Software will run on Linux on Cortex®-A7. NFC05A1 board is a NFC card reader expansion board based on ST25R3911B for STM32 and STM8 Nucleos.
2. Prerequisites[edit source]
All the dependencies as per the LINK:Getting_started/STM32MP1_boards/STM32MP157C-DK2 should be installed
2.1. Hardware Prerequisites[edit source]
- STM32MP157C-DK2 Discovery Kit
- X-NUCLEO-NFC05A1
- 8 GB micro SD card to boot the STM32MP157C-DK2
- SD card reader OR LAN connectivity
For more information about the STM32 discovery board and how to start it up, jump to this section Getting_started/STM32MP1_boards/STM32MP157C-DK2
- NFC05A1 expansion board
2.2. Software prerequisites[edit source]
- Linux PC with Ubuntu 16.04 LTS installed
- The STM32MP157C-DK2 board must be downloaded with appropriate software in order to support NFC05A1 expansion board. For proceeding, follow the step-by-step instructions provided at STM32MP157C-DK2 Let's start.
3. Hardware setup - connections explained[edit source]
The X-NUCLEO-NFC005A1 is docked on to the Arduino connector present on the bottom side of the STM32MP157C-DK2 board as shown in below figure -
[upload Pic ]
4. Software setup- configuration steps[edit source]
Please follow below steps to first flash the Starter Package onto the SD Card and then customize the platform to run application for X_NUCLEO NFC05A1.
Please follow intsructions in the link : STM32MP157C-DK2 Let's start. to flash the Starter Package onti SD Card.
In order to set up the development platform, please follow below mentioned steps –
- Download the Developer-Package in the default folder structure on an Ubuntu 16.04 machine.
- copy the patch file to the location where all patch files are placed. If youo follow the defaut folder structure, then the location should be :