This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Contents[edit source]
- 1. Article Purpose
- 2. Prerequisites
- 2.1 Hardware prerequisites
- 2.2 Software prerequisites
- 3 Hardware setup - connections explained
- 4 Software setup - customization to support X-NUCLEO-NFC05A1 expansion board
- 4.1 Kernel configuration
- 4.2 Kernel device tree configuration
- 4.2.1 Hardware / software interface
- 4.2.2 Kernel device tree configuration
- 4.3 Activate the new configuration in the STM32MP157C-DK2 board
- 4.4 Verify the new configuration on board
2. Article Purpose[edit source]
The purpose of this article is to explain how to integrate the NFC05A1 expansion board with STM32MP157C-DK2, Software will run on Linux on Cortex®-A7. NFC05A1 board is a NFC card reader expansion board based on ST25R3911B for STM32 and STM8 Nucleos.
3. Prerequisites[edit source]
All the dependencies as per the LINK:Getting_started/STM32MP1_boards/STM32MP157C-DK2 should be installed
3.1. Hardware Prerequisites[edit source]
- STM32MP157C-DK2 Discovery Kit
- X-NUCLEO-NFC05A1
- 8 GB micro SD card to boot the STM32MP157C-DK2
- SD card reader OR LAN connectivity
For more information about the STM32 discovery board and how to start it up, jump to this section Getting_started/STM32MP1_boards/STM32MP157C-DK2
- NFC05A1 expansion board
3.2. Software prerequisites[edit source]
- Linux PC with Ubuntu 16.04 LTS installed
- The STM32MP157C-DK2 board must be downloaded with appropriate software in order to support NFC05A1 expansion board. For proceeding, follow the step-by-step instructions provided at STM32MP157C-DK2 Let's start.
4. Hardware setup - connections explained[edit source]