In U-Boot, the U-Boot SPL can provide a debug console for the DDR configuration.
It is the embedded part used by the STM32CubeMX DDR tuning tools.
1. DDR interactive mode[edit source]
This mode is defined under the compilation flag CONFIG_STM32MP1_DDR_INTERACTIVE.
When this configuration flag is activated, to enter in interactive mode, you have 2 solutions:
- load SPL and key press the character 'd' (as DDR) in the console.
Polling is done only during 200ms in boot sequence.
So it is difficult manually and you should maintain the key "d" pressed during the SPL startup until the DDR> prompt - compile to force DDR_INTERACTIVE mode by adding DDR_INTERACTIVE=1 in make option
then SPL automatically enters in DDR mode:
DEVICE_TREE=<device tree name> DDR_INTERACTIVE=1 make
when the DDR tool console is available you have the display after the SPL information banner:
0:DDR_RESET DDR>
The interactive mode uses the same UART that SPL console, by default the STMicroelectronics boards use UART4 with Bps=115200 Bit=8 Parity=None Stop=1
1.1. DDR steps[edit source]
The DDR interactive mode uses some 5 steps to initialize the DDR controller and the PHY (including the "Mode Register" 0-3 sent to DDR during initialization) with parameters found in the device tree:
step | name | Description | DDR CTL state |
DDR PHY state |
DDR CTL registers |
DDR PHY registers |
---|---|---|---|---|---|---|
0 | DDR_RESET | Initial state Clock initialized 'param' initialized with Device Tree |
Reset | Reset | Reset Values | Reset Values |
1 | DDR_CTRL_INIT_DONE | Controller init done | Clocked | Reset | Init done with 'param.ctl' CTL register can be updated (command edit) |
Reset Values |
2 | DDR PHY_INIT_DONE | DDR PHY init done | Runnig Waiting PHY |
Clocked | - | Init done with 'param.phy' PHY register can be updated (command edit) |
3 | DDR_READY | DDR ready and ports are open test can be executed |
Running | Running | - | - |
4 | RUN | Continue execution (U-Boot load) | Running | Running | - | - |
1.2. commands available[edit source]
with :
- <type> = ctl, phy (for all DDR controller or PHY registers)
or one category: static, timing, map, perf, cal, dyn - <reg> = name of the register (dx0dqstr for example)
You can execute the commands:
- help: displays help
- info: manages the DDR information (step, name, size and speed)
- info: displays the DDR information
- info <param> <val>: changes the <param> with <value> (<param> = "step", "name", "size" or "speed")
- freq: manages the DDR PHY frequency
- freq: displays the DDR frequency
- freq <frequency>: changes the frequency (in kHz), allowed only in step 0
DDR>freq DDRPHY = 40000 kHz DDR> freq 523000 DDRPHY = 522999 kHz
- param: manages the input parameters (read from the device tree)
- param [type|reg]: prints input parameters
- param <reg> <val>: edits parameters in step 0
- print [type|reg]: dump register
- edit: modifies register in the DDR controller and DDR PHY
need to be done at the correct step, AFTER the initialization from the input parameters (values from device tree )
- step 1 => CTRL register update allowed
- step 2 => PHY register update allowed
- step 3 => DDR ready (only for dynamic register for controller and PHY)
- edit [type|reg]: modifies value register in DDR controller or PHY
- step: manages the step
- step: lists the available steps
- step [n]: goes to the step <n>
you can reset and restart init sequence with "step 0"
0:DDR_RESET 1:DDR_CTRL_INIT_DONE 2:DDR PHY_INIT_DONE 3:DDR_READY 4:RUN
- next: goes to the next step
- go: continues the U-Boot SPL execution (load u-boot, same than "step 4")
- reset: reboots the machine
- test: test management : see next chapter
- tuning: executes the tuning command, today only one sub command
- tuning <n>: executing tuning procedure <n>
- tuning help: displays the help message, lists available tuning procedures
0:Read DQS gating:software read DQS Gating 1:Bit de-skew: 2:Eye Training:or DQS training 3:Display registers: 4:Bist config:[nbErr] [seed]
The command "param" is simple to test modified settings as it modifies the input parameters ( 'param' read from device tree). It is recommanded to execute this command at step 0 and the modified values will be applied at the correct #DDR steps.
The command "print" and "edit" directly access to the CTRL and PHY registers, so the values can be overidden by the input parameters when the driver execute the intialization steps. These command are used to finely debug the DDR initialization.
1.3. Examples[edit source]
DDR>info step = 3 : DDR_READY name = DDR3-1066/888 bin G 2x4Gb 533MHz v1.40 size = 0x40000000 speed = 533000 kHz
DDR>param cal
==phy.cal==
dx0dllcr= 0x40000000
dx0dqtr= 0xffffffff
dx0dqstr= 0x3db02000
dx1dllcr= 0x40000000
dx1dqtr= 0xffffffff
dx1dqstr= 0x3db02000
dx2dllcr= 0x40000000
dx2dqtr= 0xffffffff
dx2dqstr= 0x3db02000
dx3dllcr= 0x40000000
dx3dqtr= 0xffffffff
dx3dqstr= 0x3db02000
DDR>print dx0dqstr
dx0dqstr= 0x3db03001
DDR>print mstr
mstr= 0x00040401
1.4. DDR test[edit source]
To execute the DDR test you need to be in the step 'DDR ready' (= step 3).
To have the list of the test, execute the command 'test' without parameter:
DDR>step 3
DDR>test
test:25
0:All:
1:Simple DataBus:[addr]
2:DataBusWalking0:[loop] [addr]
3:DataBusWalking1:[loop] [addr]
4:AddressBus:[size] [addr]
5:MemDevice:[size] [addr]
6:SimultaneousSwitchingOutput:[size] [addr]
7:Noise:[pattern] [addr]
8:NoiseBurst:[size] [pattern] [addr]
9:Random:[size] [loop] [addr]
10:FrequencySelectivePattern :[size]
11:BlockSequential:[size]
12:Checkerboard:[size]
13:BitSpread:[size]
14:BitFlip:[size]
15:WalkingOnes:[size]
16:WalkingZeroes:[size]
17:infinite read:[addr]
18:infinite write:[addr]
Each test can be executed individually, identified by its number:
DDR>test 1
execute 1:Simple DataBus
Result: Pass [address 0xc0000000]
All tests can be executed with test 0:
DDR>test 0
execute 0:All
execute 1:Simple DataBus
result 1:Simple DataBus = Passed
execute 2:DataBusWalking0
running 100 loops at 0xc0000000
result 2:DataBusWalking0 = Passed
execute 3:DataBusWalking1
running 100 loops at 0xc0000000
result 3:DataBusWalking1 = Passed
....
check buffer.
pattern = 00000001.
check buffer.
result 15:WalkingOnes = Passed
Result: Pass [0/16 test failed]
2. Source code organization[edit source]
- driver = drivers/ram/stm32mp1/
- ddr initialization : stm32mp1_ddr.c
- test : stm32mp1_tests.c
- tuning code: stm32mp1_tuning.c
- device tree files for DDR setting: arch/arm/dts/stm32mp15-*dtsi , for example:
These files provide a list of define:
#define DDR_<NAME> <VALUE>
and include stm32mp15-ddr.dtsi to provide each register values for the DDR controller and PHY.
These DDR files are included in the needed board files stm32mp157c_<board>-uboot.dts to build the device tree with the needed DDR configuration nodes.
3. Load SPL in embedded RAM[edit source]
To execute SPL in the DDR interactive mode and to tune the DDR settings, SPL needs to be loaded in embedded RAM:
- manually (to be repeated after each reset):
- automatically by ROM code after each reset:
3.1. with STM32CubeProgrammer[edit source]
You can use the CLI command to directly load SPL in the embedded RAM for peripheral boot on USB or UART.
In this case the load with STM32Programmer needs to be repeated after each reset.
In the next example, we use Linux cli but you can use also ST32CubeProgrammer for Windows (.bat file) with same parameter.
3.1.1. USB[edit source]
- Compile SPL with DDR_INTERACTIVE=1
- Select USB_Boot on the board
(for example STM32MP157C-EV1_-_hardware_description#Boot_related_switches). - Connect USB to USB HS, reset the board and execute the STM32CubeProgrammer CLI command :
STM32_Programmer.sh -c port=usb1 -w spl/u-boot-spl.stm32 0x01 --start 0x01
3.1.2. UART[edit source]
- Compile SPL with DDR_INTERACTIVE=1
- Select UART_Boot on the board
(for example STM32MP157C-EV1_-_hardware_description#Boot_related_switches). - Connect board UART to the PC, reset the board and the STM32CubeProgrammer CLI command (with the correct tty interface : ttyS0 / ttyUSB0):
STM32_Programmer.sh -c port=/dev/ttyS0 br=115200 -w spl/u-boot-spl.stm32 0x01 --start 0x01
3.2. with GDB[edit source]
- Compile SPL with DDR_INTERACTIVE=1
- Select "Engineering boot" = "Forced USB boot for flashing" on the board
(for example STM32MP157C-EV1_-_hardware_description#Boot_related_switches). - After GDB connection, reset and attach to the target, execute the commands:
(gdb) file u-boot-spl.elf (gdb) load (gdb) set $dtb = __bss_end (gdb) restore spl/u-boot-spl.dtb binary $dtb
Warning: SPL DTB is not included in the ELF file by default, you need to load it manually with GDB at the correct location.
3.3. Boot from SD Card[edit source]
You can directly update SPL on the SD card used and let Boot ROM code to load the binary for the next boot form SD Card.
In this case you activate the DDR mode by pressing the 'd' key continously (DDR_INTERACTIVE=1 is not mandatory).
3.3.1. writing SPL in SDMMC on Linux PC[edit source]
See How_to_update_U-Boot_on_an_SD_card to update partition 1 and 2 with partition <n> = /dev/mmcblk0p<n> or /dev/sdb<n> :
dd if=u-boot-spl.stm32 of=<dev>1 conv=fdatasync dd if=u-boot-spl.stm32 of=<dev>2 conv=fdatasync
3.3.2. writing SPL in SDMMC with STM32CubeProgrammer[edit source]
Warning: to use STM32CubeProgrammer, the DDR needs to work to allow U-Boot execution.
So it can be only using for the stress test / tuning.
To boot from SDCARD, we need to write in 2 partitions the generated files:
- 1: spl/u-boot-spl.stm32
- 4: u-boot.img
on Linux, the command is:
STM32_Programmer.sh -c port=usb1 -w FlashLayout.tsv
with FlashLayout.tsv following STM32CubeProgrammer_flashlayout format, for example:
#Option Id Name Type Device Offset Binary P 0x01 fsbl1 Binary SDMMC1 0x00004400 spl/u-boot-spl.stm32 PE 0x02 fsbl2 Binary SDMMC1 0x00044400 none P 0x03 ssbl Binary SDMMC1 0x00084400 u-boot.img.bin
You can use also programmer for Windows (.bat file) with same parameter.