Template:ArticleMainWriter Template:ArticleApprovedVersion
This page explains how to boot the Linux kernel from U-Boot through a TFTP server (trivial file transfer protocol[1]) installed on a host PC, based on the U-Boot command pxe.
1. Documentation[edit source]
The documentation is available in the U-Boot source:
2. tftp server installation on host PC[edit source]
See: https://importgeek.wordpress.com/2013/09/04/install-configure-and-test-tftp-server-in-ubuntu/
3. tftp server configuration[edit source]
U-Boot follows pxelinux's rules[2] to download from the tftp server a #PXE configuration file located in the #pxelinux.cfg directory.
See details in http://syslinux.zytor.com/wiki/index.php/PXELINUX
3.1. PXE configuration file[edit source]
Each PXE configuration file has same format as the extlinux.conf file generated by yocto distribution.
To fully boot on a network (kernel and rootfs), you can define the ramfs option.
For example for an ev1 board:
menu title Select the boot mode DEFAULT ramfs LABEL ramfs KERNEL uImage FDT stm32mp157c-ev1.dtb INITRD uInitrd APPEND rootwait rw earlyprintk console=ttyS3,115200
Another solution for network boot is to use rootfs as nfs with modified Linux bootargs (APPEND: rootfstype=nfs nfsroot=... see kernel bootargs).
You be can also use rootfs on a device (e•MMC, SDCard, NAND, and so on) by adding other labels and TIMEOUT (selection needs user action on the U-Boot console).
menu title Select the boot mode
DEFAULT ramfs
TIMEOUT 20
LABEL ramfs
KERNEL uImage
FDT stm32mp157c-ev1.dtb
INITRD uInitrd
APPEND rootwait rw earlyprintk console=ttySTM0,115200
LABEL sdcard
KERNEL uImage
FDT stm32mp157c-ev1.dtb
APPEND root=/dev/mmcblk0p6 rootwait rw earlyprintk console=ttySTM0,115200
LABEL eMMC
KERNEL uImage
FDT stm32mp157c-ev1.dtb
APPEND root=/dev/mmcblk1p6 rootwait rw earlyprintk console=ttySTM0,115200
3.2. pxelinux.cfg directory[edit source]
Because more than one board may be booted from the same server, the PXE configuration file name depends on U-boot parameters (hardware address/IP address).
U-Boot looks in the pxelinux.cfg directory for a PXE configuration file name in this order:
- UUID comes from "pxeuuid" variable [3]
- hardware type and address: Ethernet (ARP[4] type "1") with MAC address[5] (ethaddr env variable)
- IP address of the board and each subnet mask
- at the end, the file named "default-$CONFIG_SYS_ARCH-$CONFIG_SYS_SOC"
You need to provide at least one file on the server for your board.
Each file of the pxelinux.cfg directory can share the the same content (or can be a symbolic link to a default one).
For example, for an stm32mp1 target, when:
- UUID is not defined
- ethaddr=00:80:e1:01:2d:6f
- IP =10.48.0.141 (hexa coding=0A30008D)
- ARCH=arm and SOC=stm32mp
U-Boot searches the configuration file is this order:
- "01-00-80-e1-01-2d-6f"
- 0A30008D then subnet 0A30008, 0A3000, 0A300 ...
- default-arm-stm32mp
With ethaddr=00:80:e1:01:2d:6f, the tftp directory (for example /tftpboot) may look like:
├── pxelinux.cfg │ ├── 01-00-80-e1-01-2d-6f ├── stm32mp157c-ev1.dtb ├── uImage ├── uInitrd
An other example with
- different boards (identified by a MAC address)
each pxe file selects a different device tree (ed1, ev1, dk1, dk2) or kernel file - fallback with the IP address submask (symbolic link to default-arm-stm32mp)
- default-arm-stm32mp (final fallbackup file)
├── pxelinux.cfg │ ├── 01-00-80-e1-01-2d-6f │ ├── 01-00-80-e1-42-42-8c │ ├── 01-00-80-e1-42-42-cd │ ├── 01-00-80-e1-42-46-76 │ ├── 0A300 -> default-arm-stm32mp │ ├── 0A30001 -> default-arm-stm32mp │ ├── 0A30004 -> default-arm-stm32mp │ ├── 0A30008 -> default-arm-stm32mp │ └── default-arm-stm32mp ├── stm32mp157c-ed1.dtb ├── stm32mp157c-ev1.dtb ├── stm32mp157a-dk1.dtb ├── stm32mp157c-dk2.dtb ├── uImage ├── uInitrd
4. Board command in U-boot console[edit source]
You can execute the DISTRO bootcmd for PXE:
env set serverip <you PC address> run bootcmd_pxe