This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Article purpose[edit source]
This article will help you to create a first TF-A device tree with STM32CubeMX, to bring up your board.
2. TF-A setup to get the serial log and USB boot[edit source]
- In STM32CubeMX:
- Create a new project from the MCU selector
- Select the STM32MP1 part number that is mounted on your board
- In Pinout & Configuration:
- RCC: enable the HSE according to your board setup. The HSE is needed for various PLL (USB, DDR).
- UARTx: setup the serial console.
- Assign UARTx to the "Cortex-A7 non-secure" and the "Boot loader" contexts
- Select the "Asynchronous" mode
- In the pinout view, change the RX and TX lines (if STM32CubeMX default proposal is not good)