U-Boot overview

Revision as of 10:13, 6 August 2019 by Registered User (→‎U-Boot command line interface (CLI))

1. Das U-Boot[edit source]

Das U-Boot (universal bootloader or U-Boot) is an open-source bootloader that can be used on ST boards to initialize the platform and load the Linux® kernel.

  git clone https://gitlab.denx.de/u-boot/u-boot.git

Read the README file before starting using U-Boot. It covers the following topics:

  • source file tree structure
  • description of CONFIG defines
  • instructions for building U-Boot
  • brief description of the Hush shell
  • list of common environment variables

2. U-Boot overview[edit source]

Zoom out to STM32MPU Embedded Software

The same U-Boot source can generate two pieces of firmware used in SPL and U-Boot STM32 MPU boot chain:

  • Trusted boot chain: TF-A as FSBL and U-Boot as SSBL
  • Basic boot chain: SPL as FSBL and U-Boot as SSBL


Warning white.png Warning
The basic boot chain cannot be used for product development (see Boot chains overview for details).

It is provided only as an example of the simplest SSBL and to support upstream U-Boot development. However, several known limitations have been identified when SPL is used in conjunction with the minimal secure monitor provided within U-Boot for basic boot chain. They apply to:

  • power
  • secure access to registers
  • limited features (STM32CubeProgrammer / boot from NAND Flash memory).

No fix is planned for these limitations.

2.1. SPL: FSBL for basic boot[edit source]

The U-Boot SPL or SPL is the first stage bootloader (FSBL) for the basic boot chain.
It is a small binary (bootstrap utility) generated from the U-Boot source and stored in the internal limited-size embedded RAM. SPL main features are the following:

  • It is loaded by the ROM code.
  • It performs the initial CPU and board configuration (clocks and DDR memory).
  • It loads the SSBL (U-Boot) into the DDR memory.

2.2. U-Boot: SSBL[edit source]

U-Boot is the default second-stage bootloader (SSBL) for STM32 MPU platforms. It is used both for trusted and basic boot chains. SSBL main features are the following:

  • It is configurable and expendable.
  • It features a simple command line interface (CLI), allowing users to interact over a serial port console.
  • It provides scripting capabilities
  • It loads the kernel into RAM and gives control to the kernel
  • It manages several internal and external devices such as NAND and NOR Flash memories, Ethernet and USB.
  • It supports the following features and commands:
    • File systems: FAT, UBI/UBIFS, JFFS
    • IP stack: FTP
    • Display: LCD, HDMI, BMP for splashcreen
    • USB: host (mass storage) or device (DFU stack)

2.3. SPL phases[edit source]

SPL executes the following main phases in SYSRAM:

  • board_init_f(): driver initialization including DDR initialization (mininimal stack and heap: CONFIG_SPL_STACK_R_MALLOC_SIMPLE_LEN)
  • configuration of heap in DDR memory (CONFIG_SPL_SYS_MALLOC_F_LEN)
  • board_init_r(): initialization of the other drivers activated in the SPL device tree
  • loading and execution of U-Boot (or Kernel in Falcon mode[1]: README.falcon ).

2.4. U-Boot phases[edit source]

U-Boot executes the following main phases in DDR memory:

  • Pre-relocation initialization (common/board_f.c): minimal initialization (such as CPU, clock, reset, DDR and console) running at the CONFIG_SYS_TEXT_BASE load address.
  • Relocation: copy of the code to the end of DDR memory.
  • Post-relocation initialization:(common/board_r.c): initialization of all the drivers.
  • Command execution through autoboot (CONFIG_AUTOBOOT) or console shell
    • Execution of the boot command (bootcmd=CONFIG_BOOTCOMMAND by default):
      for example, execution of the command 'bootm' to:
      • load and check images (such as kernel, device tree and ramdisk)
      • fixup the kernel device tree
      • install the secure monitor (optional) or
      • pass the control to the Linux kernel (or to another target application)

3. U-Boot configuration[edit source]

The U-Boot binary configuration is based on

  • Kbuild infrastructure (as in Linux Kernel, you can use "make menuconfig" in U-Boot)
    The configurations are based on:
  • other compilation flags defined in include/configs/stm32mp*.h (these flags are progressively migrated to Kconfig)
    The file name is configured through CONFIG_SYS_CONFIG_NAME.
    For stm32mp157, the include/configs/stm32mp1.h file is used.
  • DeviceTree = U-Boot and SPL binaries include a device tree blob that is parsed at runtime

All the configuration flags (prefixed by CONFIG_) are described in the source code, either in the README file or in the documentation directory .
For example, CONFIG_SPL activates the SPL compilation.
Hence to compile U-Boot, select the <target> and the device tree for the board in order to choose a predefined configuration.
Refer to #U-Boot_build for examples.

3.1. Kbuild[edit source]

Like the kernel, he U-Boot build system is based on configuration symbols (defined in Kconfig files). The selected values are stored in a .config file in the build directory, with the same makefile target. .
Proceed as follows:

  • Select a pre-defined configuration (defconfig file in configs directory ) and generate the first .config:
  make <config>_defconfig.
  • Change the U-Boot compile configuration (modify .config) by using one of the following five make commands:
  make menuconfig --> menu based program
  make config  --> line-oriented configuration
  make xconfig --> QT program[2]
  make gconfig --> GTK program
  make nconfig --> ncurse menu based program

You can then compile U-Boot with the updated .config.

Warning: the modification is performed locally in the build directory. It will be lost after a "make distclean".

Save your configuration to be able to use it as a defconfig file:

   make savedefconfig

This target saves the current config as a defconfig file in the build directory. It can then be compared with the predefined configuration (configs/stm32mp*defconfig).

The other makefile targets are the following:

  make help
 ....
 Configuration targets:
   config	  - Updates the current config file using a line-oriented program
   nconfig         - Updates the current config file using a ncurses menu-based program
   menuconfig	  - Updates the current config file using a menu-based program
   xconfig	  - Updates the current config file using a Qt-based front-end
   gconfig	  - Updates the current config file using a GTK+-based front-end
   oldconfig	  - Updates the current config file starting from a provided .config file 
   localmodconfig  - Updates the current config file by disabling non-loaded modules
   localyesconfig  - Updates the current config file by converting local modules to core modules  
   defconfig	  - Creates new config file from default ARCH-supplied defconfig file
   savedefconfig   - Saves the current config file as ./defconfig (minimal configuration)
   allnoconfig	  - Creates a new config file where all options are set to NO
   allyesconfig	  - Creates a new config file where all options are set to YES
   allmodconfig	 - Creates a new config file where the modules are selected when possible
   alldefconfig    - Creates a new config file where all symbols are set to their default value
   randconfig	  - Creates a new config file where all options are set randomly
   listnewconfig   - Lists new options
   olddefconfig	  - Same as oldconfig but sets new symbols to their default value without prompting the user

3.2. Device tree[edit source]

Refer to doc/README.fdt-control .

The board device tree has the same binding as the kernel. It is integrated within the SPL and U-Boot binaries:

  • By default, it is appended at the end of the code (CONFIG_OF_SEPARATE).
  • It is embedded in the U-Boot binary (CONFIG_OF_EMBED). This is useful for debugging since it enables easy .elf file loading.

A default device tree is available in the defconfig file (by setting CONFIG_DEFAULT_DEVICE_TREE).

You can select another supported device tree using the DEVICE_TREE make flag.
For stm32mp32 boards, the corresponding file is: arch/arm/dts/stm32mp*.dts .

   make DEVICE_TREE=<dts-file-name>

or provide a precompiled device tree blob (using EXT_DTB option):

   make EXT_DTB=boot/<dts-file-name>.dtb

The SPL device tree is also generated from this device tree. However to reduce its size, the U-Boot makefile uses the fdtgrep tool to parse the full U-Boot DTB and identify all the drivers required by SPL.

To do this, U-Boot uses specific device-tree flags to define if the associated driver is initialized prior to U-Boot relocation and/or if the associated node is present in SPL :

  • u-boot,dm-pre-reloc => present in SPL, initialized before relocation in U-Boot
  • u-boot,dm-pre-proper => initialized before relocation in U-Boot
  • u-boot,dm-spl => present in SPL

In the device tree used by U-Boot, these flags need to be added in each node used in SPL or in U-Boot before relocation and for each used handle (clock, reset, pincontrol).

4. U-Boot command line interface (CLI)[edit source]

Refer to U-Boot Command Line Interface.

If CONFIG_AUTOBOOT is activated, you have CONFIG_BOOTDELAY seconds (2s by default) to enter the console by pressing any key, after the line below is displayed and bootcmd is executed (CONFIG_BOOTCOMMAND):

 Hit any key to stop autoboot:  2

4.1. Commands[edit source]

The commands are defined in cmd/*.c . They are activated through the corresponding CONFIG_CMD_* configuration flag.

Use the help command in the U-Boot shell to list the commands available on your device:

  help

Below the list of all commands extracted from U-Boot Manual (not-exhaustive):

  • Information Commands
    • bdinfo - prints Board Info structure
    • coninfo - prints console devices and information
    • flinfo - prints Flash memory information
    • iminfo - prints header information for application image
    • help - prints online help
  • Memory Commands
    • base - prints or sets the address offset
    • crc32 - checksum calculation
    • cmp - memory compare
    • cp - memory copy
    • md - memory display
    • mm - memory modify (auto-incrementing)
    • mtest - simple RAM test
    • mw - memory write (fill)
    • nm - memory modify (constant address)
    • loop - infinite loop on address range
  • Flash Memory Commands
    • cp - memory copy
    • flinfo - prints Flash memory information
    • erase - erases Flash memory
    • protect - enables or disables Flash memory write protection
    • mtdparts - defines a Linux compatible MTD partition scheme
  • Execution Control Commands
    • source - runs a script from memory
    • bootm - boots application image from memory
    • go - starts application at address 'addr'
  • Download Commands
    • bootp - boots image via network using BOOTP/TFTP protocol
    • dhcp - invokes DHCP client to obtain IP/boot params
    • loadb - loasd binary file over serial line (kermit mode)
    • loads - loads S-Record file over serial line
    • rarpboot- boots image via network using RARP/TFTP protocol
    • tftpboot- boots image via network using TFTP protocol
  • Environment Variables Commands
    • printenv- prints environment variables
    • saveenv - saves environment variables to persistent storage
    • setenv - sets environment variables
    • run - runs commands in an environment variable
    • bootd - boots default, i.e., run 'bootcmd'
  • Flattened Device Tree support
    • fdt addr - selects the FDT to work on
    • fdt list - prints one level
    • fdt print - recursive printing
    • fdt mknode - creates new nodes
    • fdt set - sets node properties
    • fdt rm - removes nodes or properties
    • fdt move - moves FDT blob to new address
    • fdt chosen - fixup dynamic information
  • Special Commands
    • i2c - I2C sub-system
  • Storage devices
  • Miscellaneous Commands
    • echo - echoes args to console
    • reset - Performs a CPU reset
    • sleep - delays the execution for a predefined time
    • version - prints the monitor version

To add a new command, refer to doc/README.commands .

4.2. U-Boot environment variables[edit source]

The U-Boot behavior is configured through environment variables.

Refer to Manual and README / Environment Variables.

On the first boot, U-Boot uses a default environment embedded in the U-Boot binary. You can modify it by changing the content of CONFIG_EXTRA_ENV_SETTINGS in your configuration file (for example ./include/configs/stm32mp1.h) (see README / - Default Environment).

This environment can be modified and saved in the boot device. When it is present, it is loaded during U-Boot initialization:

  • for eMMC/SDCARD boot (CONFIG_ENV_IS_IN_EXT4), in the bootable ext4 partition "bootfs" in
    in file CONFIG_ENV_EXT4_FILE="uboot.env".
  • for NAND boot (CONFIG_ENV_IS_IN_UBI), in the two UBI volumes "config" (CONFIG_ENV_UBI_VOLUME) and "config_r" (CONFIG_ENV_UBI_VOLUME_REDUND).
  • for NOR boot (CONFIG_ENV_IS_IN_SPI_FLASH), in the u-boot_env mtd parttion (at offset CONFIG_ENV_OFFSET).

4.2.1. env command[edit source]

The "env" command allows displaying, modifying and saving the environment in U-Boot console.

  help env
 env - environment handling commands
 
 Usage:
 env default [-f] -a - [forcibly] resets the default environment
 env default [-f] var [...] - [forcibly] resets the variable(s) to their default values
 env delete [-f] var [...] - [forcibly] deletes variable(s)
 env edit name - edits an environment variable
 env exists name - tests the existence of variable
 env print [-a | name ...] - prints the environment
 env print -e [name ...] - prints the UEFI environment
 env run var [...] - runs commands in an environment variable
 env save - saves the environment
 env set -e name [arg ...] - sets UEFI variable or unset it if 'arg' is not specified
 env set [-f] name [arg ...]

Example: proceed as follows to restore the default environment and save it. This is useful after a U-Boot upgrade:

  env default -a
  env save

4.2.2. bootcmd[edit source]

"bootcmd" is the autoboot command. It defines the command executed when U-Boot starts (CONFIG_BOOTCOMMAND).

For stm32mp, CONFIG_BOOTCOMMAND="run bootcmd_stm32mp":

  env print bootcmd    
  bootcmd=run bootcmd_stm32mp

"bootcmd_stm32mp" is a script that selects the command to be executed for each boot device (see ./include/configs/stm32mp1.h), based on generic distro scripts:

  • for serial/usb: execute the stm32prog command.
  • for mmc boot (eMMC, SD card), boot only on the same device (bootcmd_mmc...).
  • for nand boot, boot with on ubifs partition on nand (bootcmd_ubi0).
  • for nor boot, use the default order eMMC (SDMMC 1)/ NAND / SDCARD (SDMMC 0) / SDMMC2 (the default bootcmd: distro_bootcmd).
  env print bootcmd_stm32mp

You can then change this configuration:

  • either permanently in your board file (default environment by CONFIG_EXTRA_ENV_SETTINGS or change CONFIG_BOOTCOMMAND value) or
  • temporally in saved environment:
  env set bootcmd run bootcmd_mmc0 
  env save

Note: To reset the environment to its default value:

  env default bootcmd
  env save

4.3. Generic Distro configuration[edit source]

see doc/README.distro

This feature is activated for ST boards (CONFIG_DISTRO_DEFAULTS):

  • one boot command (bootmcd_xxx) exists for each bootable device.
  • U-Boot is independent of the Linux distribution used.
  • bootcmd is defined in ./include/config_distro_bootcmd.h

With DISTRO the default command executed: include/config_distro_bootcmd.h

 bootcmd=run distro_bootcmd

This script will try any device found in the variable 'boot_targets' and execute the associated bootcmd.

Example for device mmc0, mmc1, mmc2, pxe and ubifs:

 bootcmd_mmc0=setenv devnum 0; run mmc_boot
 bootcmd_mmc1=setenv devnum 1; run mmc_boot
 bootcmd_mmc2=setenv devnum 2; run mmc_boot
 bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
 bootcmd_ubifs0=setenv devnum 0; run ubifs_boot

U-Boot searchs for a configuration file extlinux.conf in a bootable device, this file defines the kernel configuration to use:

  • bootargs
  • kernel + device tree + ramdisk files (optional)
  • FIT image

4.4. U-Boot scripting capabilities[edit source]

"Script files" are command sequences that will be executed by U-Boot's command interpreter; this feature is especially useful when you configure U-Boot to use a real shell (hush) as command interpreter.

See U-Boot script manual for example.

5. U-Boot build[edit source]

5.1. Prerequisites[edit source]

You need:

  git clone https://github.com/STMicroelectronics/u-boot
  • from the Mainline U-Boot in official GIT repository [4]
  git clone https://gitlab.denx.de/u-boot/u-boot.git

5.1.1. ARM cross compiler[edit source]

You need to have a cross compiler [5] installed on your Host (X86_64, i686, ...) for the targeted Device architecture = ARM, the environment variables ($PATH and $CROSS_COMPILE) need to be configured in your shell.

You can use gcc for ARM, available in:

  1. the SDK toolchain
    See Cross-compile with OpenSTLinux SDK, PATH and CROSS_COMPILE are automatically updated.
  2. an existing package (for example, on Ubuntu/Debian: ( sudo apt-get install gcc-arm-linux-gnueabihf)
  3. an existing toolchain:

for example: gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi.tar.xz
from https://releases.linaro.org/components/toolchain/binaries/7.2-2017.11/arm-linux-gnueabi/
unzip the toolchain in $HOME and update your environment with:

  export PATH=$HOME/gcc-linaro-7.2.1-2017.11-x86_64_arm-linux-gnueabi/bin:$PATH
  export CROSS_COMPILE=arm-linux-gnueabi-

5.2. Compilation[edit source]

In the U-Boot source directory, you need to select the <target> and the <device tree> for your configuration and then execute the "make all" command.

  make <target>_defconfig
  make DEVICE_TREE=<device-tree> all

KBUILD_OUTPUT can be used optionally to change the output directory if you want to compile several targets or don't compile in the source directory, for example:

  export KBUILD_OUTPUT=../build/basic

DEVICE_TREE can be also exported to your environment when you support only one board, for example:

  export DEVICE_TREE=stm32mp157c-ev1

For all the stm32mp15 family, we manage 3 configurations:

  • stm32mp15_trusted_defconfig: trusted boot chain, U-Boot (without SPL) is unsecure and uses Secure monitor from TF-A
  • stm32mp15_optee_defconfig: trusted boot chain, U-Boot (without SPL) is unsecure and uses Secure monitor from SecureOS = OP-TEE
  • stm32mp15_basic_defconfig: basic boot chain, with an SPL as FSBL, U-BOOT is secure and installs monitor with PSCI

The board diversity is only managed with the device tree.

Examples from STM32MP15 U-Boot:

  export KBUILD_OUTPUT=../build/trusted
  make stm32mp15_trusted_defconfig
  make DEVICE_TREE=stm32mp157c-<board> all
  export KBUILD_OUTPUT=../build/optee
  export DEVICE_TREE=stm32mp157c-<board>
  make stm32mp15_optee_defconfig
  make all
  make stm32mp15_basic_defconfig
  make DEVICE_TREE=stm32mp157c-<board>  all

Use help to list other targets:

  make help

5.3. Output files[edit source]

The resulting U-Boot files are present in your build directory (U-Boot or KBUILD_OUTPUT).

Two binary format is used for stm32mp product:

  • STM32 image format (*.stm32), managed by mkimage U-Boot tools and Signing_tool ; it is requested by ROM code and by TF-A; see STM32 header for details.
  • uImage (*.img) format, file with U-Boot header, managed by SPL and U-Boot (for kernel load)

The U-Boot generated files for

  • Trusted boot chain (TF-A is used as FSBL, with or without OP-TEE)
    • u-boot.stm32 : U-Boot binary with STM32 image header, loaded by TF-A
  • Basic boot chain (SPL is used as FSBL)
    • u-boot-spl.stm32 : SPL binary with STM32 image header, loaded by ROM code
    • u-boot.img : U-Boot binary with uImage header, loaded by SPL

The files used to debug with gdb are

  • u-boot : elf file for U-Boot
  • spl/u-boot-spl : elf file for SPL

6. References[edit source]