STM32CubeProgrammer release note

Revision as of 11:17, 20 February 2019 by Registered User (→‎STM32CubeProgrammer - Version 2.0.0)

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


STM32CubeProgrammer.png

STM32CubeProgrammer is the official STMicroelectronics tool to download firmware into STMicroelectronics boards.

1. STM32CubeProgrammer - Version 2.0.0[edit source]

STM32CubeProgrammer for LinuxTemplate:Sup host PC STM32CubeProgrammer for WindowsTemplate:Sup host PC
Download

Version 2.0.0

  • To access the following link and follow instructions to download the package, you will need a myST account

SetupSTM32CubeProgrammer

  • Download the archive file in a temporary directory of your host PC
  • Uncompress the archive file to get the STM32CubeProgrammer installers:
 unzip SetupSTM32CubeProgrammer.zip
Installation
  • Execute the Linux installer, which guides you through the installation process. If you follow the proposition to organize the tools' directory, indicate "STM32MPU-Tools/STM32CubeProgrammer-2.0.0" as the installation directory, when it's requested by the installer
 ./SetupSTM32CubeProgrammer-2.0.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, with the following command:
 export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already in PATH. Example, if "/home/bin" is in the PATH environment varialble, run the following command:
 ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process. If you follow the proposition to organize the tools' directory, indicate "STM32MPU-Tools/STM32CubeProgrammer-2.0.0" as the installation directory, when it's requested by the installer

SetupSTM32CubeProgrammer-2.0.0.exe

User manual
Detailed release note
  • Details about the content of this tool version are available in ST Web Site Release Note .
  • If interested in previous releases, please go through the archives of the ecosystem release note.