1. Article purpose[edit source]
The purpose of this article is to explain how to integrate Amazon Web Service (AWS) IoT Greengrass [1] on top of OpenSTLinux, including the security part that enables the connection to a hardware security module (TPMv2.0).
This article explains step by step how to add the yocto "meta-st-stm32mpu-app-aws" layer on top of OpenSTLinux distribution, how to configure, build and install the image, how to execute the AWS Greengrass certification testing and configure the target for a secure connection with the AWS cloud.
2. Prerequisites[edit source]
Knowledge of the AWS IoT Greengrass and AWS cloud account configuration is required. Follow the process described in "AWS amazon site"[2].
2.1. Hardware prerequisites[edit source]
The process has been verified with the STM32MP157C-DK2 Discovery kit and STM32MP157F-DK2 Discovery kit .
- STM32MP157C-DK2
For more information about this STM32 Discovery board and how to start using it, jump to section Getting started with STM32MP157x-DK2
- STPM4RasPI Expansion board[3]
The STPM4RasPI is an official Extension board to connect the ST33 TPM products to the Raspberry Pi® device. It is designed for development, proof of concept or demonstration activities. The board is shipped with one trusted platform module soldered, the ST33TPHF20SPI, that implement TPM V2.0 specification.
2.2. Software prerequisites[edit source]
The STM32MP1 Distribution Package must be installed on your host. The process has been verified with ecosystem release v2.0.0 of the OpenSTlinux distribution.
3. Software update with meta-st-stm32mpu-app-aws[edit source]
.
.
1.Clone the following STMicroelectronics git repository
cd [your STM32MP1 Distribution path]/layers/meta-st git clone https://github.com/STMicroelectronics/meta-st-stm32mpu-app-aws.git cd meta-st-stm32mpu-app-aws git checkout remotes/origin/dunfell
2. Add TPM2 recipes
cd [your STM32MP1 Distribution path]/layers git clone git://git.yoctoproject.org/meta-security cd meta-security git checkout remotes/origin/dunfell
3.Setup the build environment
Execute the following command on the host:
cd [your STM32MP1 Distribution path] DISTRO=openstlinux-weston MACHINE=stm32mp1-demo-aws source layers/meta-st/scripts/envsetup.sh
4.Enable TPM build
Apply the following patch in the file ([your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/include/openstlinux.in)
DISTRO_FEATURES_append = " tpm2 "
5.Add Virtualization (docker) to the OpenSTLinux distribution
Execute the following command on the host:
cd [your STM32MP1 Distribution path]/layers git clone git://git.yoctoproject.org/meta-virtualization git checkout remotes/origin/dunfell cd [your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws bitbake-layers add-layer [your STM32MP1 Distribution path]/layers/meta-virtualization
Update the file ([your STM32MP1 Distribution path]/layers/meta-st/meta-st-openstlinux/conf/distro/openstlinux-weston.conf)
DISTRO_FEATURES_append = "virtualization"
6.Add Java-jdk To do this, follow the installation process described in the article How to install JAVA JDK.
7.Increase the Rootfs partition size Update the file ([your STM32MP1 Distribution path]/ layers/meta-st/meta-st-stm32mp/conf/machine/include/st-machine-common-stm32mp.inc)
IMAGE_ROOTFS_MAXSIZE = "2097152"
8.Build the image
In the folder ([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws), executes the following command :
bitbake st-image-demo-aws
9.Flash the SDcard
Use the programmer tool STM32CubeProgrammer
For example, the tsv file (FlashLayout_sdcard_ stm32mp157c-demo-aws-mx-trusted.tsv) is located in ([your STM32MP1 Distribution path]/build-openstlinuxweston-stm32mp1-demo-aws/tmp-glibc/deploy/images/stm32mp1-demo-aws/flashlayout_st-image-demo-aws)
4. AWS greengrass target initialization[edit source]
1. WiFi configuration
A internet connection on the target is required. Refer to the article How to setup wifi connection for how to configure and activate the WiFi in order to connect the target to your WiFi access point.
2.Configuration of the target
If extra target configurations are required, run the following scripts (to be executed only once after the first boot):
source /greengrass/tpm_update.sh
If the image has been configured for the execution of the AWS greengrass certification testing:
source /greengrass/awsgreengrass_certif.sh
3.TPM token initialization
Note: If something goes wrong, reset the TPM and PKCS11 store using the following commands:
cd /usr/bin ./tpm2_clear -Q rm -rf /usr/local/pkcs11_tpm/*
Executes the commands below on the target:
cd /tools ./tpm2_ptool init --primary-auth=123456 --path=$TPM2_PKCS11_STORE ./tpm2_ptool addtoken --pid=1 --sopin=123456 --userpin=123456 --label=greengrass --path $TPM2_PKCS11_STORE ./tpm2_ptool addkey --algorithm=rsa2048 --label="greengrass" --userpin=123456 --key-label=greenkey --path=$TPM2_PKCS11_STORE
OPTIONA :Verification using pkcs11-tool
Executes the following command on the target to verify the token created.
pkcs11-tool --module /usr/lib/libtpm2_pkcs11.so.0 -L
Example of expected output:
Available slots: Slot 0 (0x1): greengrass STMicro token label : greengrass token manufacturer : STMicro token model : token flags : login required, rng, token initialized, PIN initialized hardware version : 1.38 firmware version : 74.8 serial num : 0000000000000000 pin min/max : 5/128
AT THIS STEP, THE CONFIGURATION OF THE BOARD IS COMPLETE AND READY TO BE USED:
- With AWS IoT Device Tester to perform the AWS greengrass certification testing, see the paragraph Process to execute the AWS Greengrass certification testing
- For a secure connection with AWS cloud, see the paragraph Process to create a Certificat Signature Request using the hardware-protected private key
5. Process to execute the AWS Greengrass certification testing[edit source]
1.Install the AWS IoT Device Tester.
Go to the AWS Amazon site to [AWS IoT Device Tester for AWS IoT Greengrass Versions] [4]
2.Configure your ssh connection (ssh keys)
Go to the AWS Amazon site to [Configure Your Host Computer to Access Your Device Under Test][5]
3.Configure the IDT
Example of the install config folder for Windows. C:\devicetester_greengrass_win\devicetester_greengrass_win\configs\
Go to the AWS Amazon site [Setting Configuration to Run the AWS IoT Greengrass Qualification Suite][6]
There is a IDT configuration file example installed on your Host : /[your STM32MP1 Distribution path]/layers/meta-st/meta-st-demo-aws/recipes-aws/greengrasstests/greengrasstests/device-hsm.json
Note : With this example the certification tests are performed in Root.
4.Execute the tests
Go to the AWS Amazon site to [Running Tests][7]
6. Process to create a Certificat Signature Request using the hardware-protected private key[edit source]
1.Update openssl configuration to use module tpm2_pkcs11
add the following lines in /etc/ssl/openssl.cnf at the beginning of the file (after "HOME = . ")
openssl_conf = openssl_init [openssl_init] engines=engine_section [engine_section] pkcs11 = pkcs11_section [pkcs11_section] engine_id = pkcs11 dynamic_path = /usr/lib/engines-1.1/pkcs11.so MODULE_PATH = /usr/lib/libtpm2_pkcs11.so.0 init = 0
2. How to create a CSR "Certificat Signature Request" with openssl (Prerequisite : openssl installed) Executes the command, on target :
openssl req -engine pkcs11 -new -key "pkcs11:token=greengrass;object=greenkey;type=private;pin-value=123456" -keyform engine -out /usr/local/req.csr
This CSR "/usr/local/req.csr" is used to create clients certificats on the AWS amazon Cloud to store on the board.
There is a greengrass configuration file example to update with your AWS account parameter and certificats created, on the target : /greengrass/config/config_secu_example.json
You need also to download the root CA on Amazon site and stored it on the target greengrass/certs/root.ca.pem.
For more information about HSM (Hardware Secure Module) integration for AWS greengrass, go to AWS Amazon site [Hardware Security Integration][8]
3.Connection to Amazon cloud
Before starting the greengrass core on the target you need to set the TPM2_PKCS11_STORE environment variable.
Executes the commands on the target :
export TPM2_PKCS11_STORE=/usr/local/pkcs11_tpm cd /greengrass/ggc/core/ ./greengrassd start
7. References[edit source]
- ↑ https://aws.amazon.com/fr/greengrass/
- ↑ What is AWS IoT Greengrass?
- ↑ STPM4RasPI expansion board
- ↑ Supported versions of AWS IoT Device Tester for AWS IoT Greengrass
- ↑ Configure your host computer to access your device under test
- ↑ Setting configuration to run the AWS IoT Greengrass qualification suite
- ↑ Running tests
- ↑ Hardware security integration