1. Overview[edit source]
The STM32 MPU embeds tamper detection management. Tamper management and configuration have been added into the secure OS to configure and detect events.
STM32MP15 offers 5 internals and 3 externals tampers.
Internal tampers are:
- RTC voltage domain monitoring
- LSE monitoring
- HSE monitoring
- RTC calendar overflow (rtc_calovf)
- Monotonic counter overflow
External tampers can be configured to be passive or active.
On a tamper event detection, the backup registers are cleared with SRAM.
2. Software configuration[edit source]
Internal tampers and external tampers have to be configured into:
- TAMP device tree configuration
- Secure OS main security configuration file .
This second part is statically defined and must be customized depending on the application needs. The file contains two static tables, one for internal tampers, another for external ones.
2.1. Internal tampers[edit source]
Here is the structure that registers internal tamper.
struct stm32_tamp_int { int id; void (*func)(int id); };
Internal tamper structure contains:
- an ID (linked to the SoC internal tamper defined)
- a function that will be called on the detected event. This function can be customized, default one just print the tamper ID and reset the SoC.
A static defined list of tampers is automatically registers during the main security loop.
static struct stm32_tamp_int int_tamp[PLAT_MAX_TAMP_INT] = {
{
.id = ITAMP1,
.func = stm32mp1_tamper_action,
},
...
}
By default, only internal tampers 1, 2, 3 and 4 are enabled.
2.2. External tampers[edit source]
Here is the structure that register external tampers.
struct stm32_tamp_ext { int id; uint8_t mode; uint8_t erase; uint8_t evt_mask; void (*func)(int id); };
External tamper structure contains:
- an ID (linked to the SoC external tamper)
- a mode (Could be passive or active tamper)
- a erase mode (Erase or no erase)
- an event mask (Default mask)
- a function pointer (Function that will be called when tamper is detected)
Here is a configuration example for two external tampers enabled
static struct stm32_tamp_ext ext_tamp[PLAT_MAX_TAMP_EXT] = { { .id = EXT_TAMP1, // External tamper 1 .mode = TAMP_TRIG_ON, // Tamper trigger event .erase = TAMP_NOERASE, // Not erasing the backup registers .evt_mask = TAMP_NO_EVT_MASK, // Mask is not set .func = NULL, // No function }, { .id = EXT_TAMP2, // External tamper 2 .mode = TAMP_ACTIVE, // Active tamper selected .erase = TAMP_NOERASE, // Not erasing the backup registers and backup sram .evt_mask = TAMP_NO_EVT_MASK, // Mask is not set .func = NULL, // No function }, TAMP_UNUSED, }