This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains how import OpenSTLinux projects into STM32CubeIDE version 1.4.0 on Linux workstation.
1. Overview[edit source]
It is possible to import into an existing STM32MP15x Project some OpenSTLinux projects inside the Cortex-A (in CA7) hierarchical project. This support is starting with OpenSTLinux version 2.0 a.k.a. 5.4-dunfell.
This is done with Import an OpenSTLinux project... contextual menu.
2. OpenSTLinux Project Structure[edit source]
The integration of OpenSTLinux project from yocto into Eclipse environment follows the
==Linux Project==
==U-Boot Project==
==TF-A Project==
==Optee Project==
![]() |
Coming soon |