How to install Yocto SDK in STM32CubeIDE

Revision as of 11:28, 25 August 2020 by Registered User

This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.

1. Overview[edit source]

Two flavors are proposed for installing Yocto SDK:

  • Yocto SDK is already installed on host workstation, after a download of the STM32MP1 OpenSTLinux Developer Package. In that case, only a setup is needed for STM32CubeIDE to use it.
  • Yocto SDK is not present on host workstation, it can be installed via STM32CubeIDE:
    • embedded inside the STM32CubeIDE; Yocto SDK removal is managed by STM32CubeIDE
    • external, on host workstation disk, outside STM32CubeIDE scope; Yocto SDK removal is under final user responsibility


2. Using already installed Yocto SDK[edit source]

OpenSTLinux SDK Installation Menu

3. Installing Yocto SDK via STM32CubeIDE[edit source]

Warning white.png Warning
OpenSTLinux development requires specific packages on host workstation. See PC_prerequisites

.