This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.
1. Overview[edit source]
Two flavors are proposed for installing Yocto SDK:
- the Yocto SDK is already installed on the host machine, after a download of the STM32MP1 OpenSTLinux Developer Package. In that case, only a setup is needed for STM32CubeIDE to use it.
- the Yocto SDK is not present on the host platform, it can be installed via STM32CubeIDE:
- embedded inside the STM32CubeIDE; Yocto SDK removal is managed by STM32CubeIDE
- on host platform disk, outside STM32CubeIDE scope; Yocto SDK removal under final user responsibility
2. Using already installed Yocto SDK[edit source]
We suppose here
3. Installing Yocto SDK from STM32CubeIDE[edit source]
.