This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article explains the way STM32CubeIDE is managing Yocto SDK provided by OpenSTLinux.
1. Overview[edit source]
The Yocto SDK can already be installed on the host machine, after a download of the STM32MP1 OpenSTLinux Developer Package In that case, only a setup is needed for STM32CubeIDE to use it. This saves the corresponding Eclipse plugin download and also some space on the disk.
.