1. Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the STM peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when necessary, how to configure the STM peripheral.
2. Peripheral overview[edit source]
The STM peripheral is used to log STM trace into the embedded trace FIFO (ETF). This trace can include hardware events (the list is given in the STM32MP15 reference manuals) or direct 'printf like' log from the Cortex®-A7. Once in the ETF buffer, the trace can directly be dumped from the Cortex®-A7 or to the trace port interface unit (TPIU), connected to an external probe able to decode it.
2.1. Component description[edit source]
The debug features are based on Arm® CoreSight™ components:
• SWJ-DP: JTAG/Serial-wire debug port
• AXI-AP: AXI access port
• AHB-AP: AHB access port
• APB-AP: APB access port
• ITM: Instrumentation Trace Macrocell
• DWT: Data Watchpoint and Trace
• ETM: Embedded Trace Macrocell
• ETF: Embedded Trace FIFO
• TPIU: Trace Port Interface Unit
• SWO: Serial Wire Output
• CTI: Cross Trigger Interface
• CTM: Cross Trigger Matrix
• Timestamp Generator
• STM: System Trace Macrocell
More information about these components can be found in the Arm® documents referenced [1]
2.2. Features[edit source]
Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are really implemented.
2.3. Security support[edit source]
The STM is a non secure peripheral.
3. Peripheral usage and associated software[edit source]
3.1. Boot time[edit source]
The STM is not used at boot time.
3.2. Runtime[edit source]
3.2.1. Overview[edit source]
The STM can be assigned to the Cortex®-A7 non-secure for using in Linux with coresight framework.
This driver allows to select the hardware events (listed in the STM32MP15 reference manuals) to log via the STM peripheral into the ETF and dump it in the Linux console for analysis.
3.2.2. Software frameworks[edit source]
Domain | Peripheral | Software frameworks | Comment | ||
---|---|---|---|---|---|
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Trace & Debug | STM | Linux Coresight framework |
3.2.3. Peripheral configuration[edit source]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
3.2.4. Peripheral assignment[edit source]
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Trace & Debug | STM | STM | ☐ |
4. References[edit source]
- ↑ [1. IHI 0031C (ID080813) - Arm® Debug Interface Architecture Specification ADIv5.0 to
ADIv5.2, Issue C, 8th Aug 2013.
2. DDI 0480F (ID100313) - Arm® CoreSight™ SoC-400 r3p1 Technical Reference Manual, Issue F, 26th Sept 2013.
3. DDI 0461B (ID010111) - Arm® CoreSight™ Trace Memory Controller r0p1 Technical Reference Manual, Issue B, 10 Dec 2010
4. DDI 0314H - Arm® CoreSight™ Components Technical Reference Manual, Issue H, 10 July, 2009
5. DDI 0403D (ID100710) - Arm® v7-M Architecture Reference Manual, Issue Derrata2010_Q3, November 2010
6. DDI 0468A (ID101712) - Arm® CoreSight™ ETM™-A7 r0p0, Issue A, 12 Sept 2011
7. DDI 0440C (ID070610) - Arm® CoreSight™ ETM™-M4 r0p1 Technical Reference Manual, Issue C, 29 June 2012
8. DDI 0528B (ID062514) - Arm® CoreSight™ STM-500 System Trace Macrocell r0p1 Technical Reference Manual, Issue B, 11 March 2014
9. DDI 0464F (ID051113) - Arm® Cortex®-A7 MPCore™ r0p5 Technical Reference Manual, Issue F, 11 April 2013],Arm® documents referenced