This article explains how to experiment armNN[1] applications for object detection based on COCO SSD MobileNet v1 model using TensorFlow Lite parser.
1. Description[edit source]
The object detection[2] neural network model allows identification and localization of a known object within an image.
The application demonstrate a computer vision use case for object detection where frames are grabbed from a camera input (/dev/videox) and analyzed by a neural network model interpreted by the TensorFlow Lite[3] framework.
Gstreamer pipeline is used to stream camera frames (using v4l2src), to display a preview (using waylandsink) and to execute neural network inference (using appsink).
The result of the inference is displayed on the preview. The overlay is done using GTK widget with cairo.
This combination is quite simple and efficient in term of CPU consumption.
The model used with this application is the COCO SSD MobileNet v1 downloaded from downloaded from the object detection overview[2].
2. Installation[edit source]
2.1. Install from the OpenSTLinux AI package repository[edit source]
After having configured the AI OpenSTLinux package you can install X-LINUX-AI components for this application:
apt-get install tflite-cv-apps-object-detection-c++
And restart the demo launcher:
systemctl restart weston@root
2.2. Source code location[edit source]
- in the Openembedded OpenSTLinux distribution:
- <Distribution Package installation directory>/layers/meta-st/meta-st-stm32mpu-ai/recipes-samples/tflite-cv-apps/files/object-detection/src
- on GitHub:
2.3. Re-generate the package from OpenSTLinux distribution (optional)[edit source]
Using the Openembedded OpenSTLinux distribution, you are able to rebuild the application.
- Before doing so, you need to install the X-LINUX-AI expansion package.
- Then you can execute the following bitbake comand to rebuild the application:
bitbake tflite-cv-apps-object-detection-c++ -c compile
- The generated binary is available here:
<Distribution Package installation directory>/<build directory>/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi/tflite-cv-apps-object-detection-c++/1.0-r0/tflite-cv-apps-object-detection-c++-1.0/object-detection/src/
3. How to use it[edit source]
3.1. Launch application via the demo launcher[edit source]
3.2. Or execute with command line[edit source]
The objdetect_tfl_gst_gtk C/C++ application is located in the userfs partition:
/usr/local/demo-ai/computer-vision/tflite-object-detection/bin/objdetect_tfl_gst_gtk
It accepts the following input parameters:
Usage: ./objdetect_tfl_gst_gtk -m <model .tflite> -l <label .txt file> -m --model_file <.tflite file path>: .tflite model to be executed -l --label_file <label file path>: name of file containing labels -i --image <directory path>: image directory with image to be classified -v --video_device <n>: video device (default /dev/video0) --crop: if set, the nn input image is cropped (with the expected nn aspect ratio) before being resized, else the nn imput image is only resized to the nn input size (could cause picture deformation). --frame_width <val>: width of the camera frame (default is 640) --frame_height <val>: height of the camera frame (default is 480) --framerate <val>: framerate of the camera (default is 15fps) --input_mean <val>: model input mean (default is 127.5) --input_std <val>: model input standard deviation (default is 127.5) --help: show this help
3.3. Testing with COCO SSD MobileNet V1[edit source]
The model used for test is the detect.tflite downloaded from object detection overview[2]
To ease launching of the application, two shell scripts are available:
- launch object detection based on camera frame inputs
/usr/local/demo-ai/computer-vision/tflite-object-detection/bin/launch_bin_objdetect_tfl_coco_ssd_mobilenet.sh
- launch object detection based on the pictures located in /usr/local/demo-ai/computer-vision/models/mobilenet/testdata directory
/usr/local/demo-ai/computer-vision/tflite-object-detection/bin/launch_bin_objdetect_tfl_coco_ssd_mobilenet_testdata.sh