1. Introduction[edit source]
The coprocessor firmware can be loaded and started:
- either by the second stage boot loader = U-Boot (see Boot_chains_overview for details) or
- by the Linux® kernel (see Linux_remoteproc_framework_overview for details)
This article explains how this coprocessor firmware is loaded by U-Boot and started before the Linux kernel.
2. Location of the coprocessor firmware[edit source]
Note: the default name for this firmware used in this WIKI is rproc-m4-fw.elf
U-Boot searches and loads the needed binaries in the first bootable partition (generic DISTRO configuration) which is bootfs in the OpenSTLinux distribution (see STM32MP15_Flash_mapping).
So the coprocessor firmware must be installed in that bootfs partition. The simplest way to do this, consists in copying the firmware from the rootfs partition to the bootfs partition as follows:
mount /dev/mmcblk0p4 /boot cp rproc-m4-fw.elf /boot/ sync
As an alternate method, you can also use the Eclipse IDE, or transfer the firmware over the serial console or over the network.
3. Starting the coprocessor firmware[edit source]
U-Boot can boot the coprocessor before the kernel (coprocessor early boot) with remoteproc uclass :
- Manual start by using rproc commands
- Automatic start, at each boot by using
- the bootcmd (needing U-Boot recompilation)
- a generic DISTRO boot script
- the FIT image
3.1. Manual start[edit source]
You can load and start the coprocessor firmware by using the rproc command in the U-Boot console (to access to the U-boot console: press any key during the U-Boot execution).
rproc rproc - Control operation of remote processors in an SoC Usage: rproc [init|list|load|start|stop|reset|is_running|ping] Where: [addr] is a memory address <id> is a numerical identifier for the remote processor provided by 'list' command. Note: Remote processors must be initalized prior to usage Note: Services are dependent on the driver capability 'list' command shows the capability of each device Subcommands: init - Enumerate and initalize the remote processors list - list available remote processors load <id> [addr] [size]- Load the remote processor with image stored at address [addr] in memory start <id> - Start the remote processor(must be loaded) stop <id> - Stop the remote processor reset <id> - Reset the remote processor is_running <id> - Reports if the remote processor is running ping <id> - Ping the remote processor for communication
In this example, the firmware is loaded from SDCARD in RAM (at ${kernel_addr_r}), and then started
ext4load mmc 0:4 ${kernel_addr_r} rproc-m4-fw.elf -> SDCARD is mmc 0, bootfs is ext4 partition number 4) rproc init -> initializes all coprocessors rproc load 0 ${kernel_addr_r} ${filesize} -> loads firmware for coprocessor 0 (code part found in .elf) rproc start 0 -> starts coprocessor 0
You can then resume the normal boot process:
run bootcmd
3.2. Automatic start[edit source]
3.2.1. Start from the bootcmd[edit source]
You can update the bootcmd which is exectued automatically: modify CONFIG_EXTRA_ENV_SETTINGS in include/configs/stm32mp1.h and then recompile U-Boot.
Example : boot a firmware on the SDCARD:
#define CONFIG_EXTRA_ENV_SETTINGS \ "stdin=serial\0" \ "stdout=serial\0" \ "stderr=serial\0" \ ... BOOTENV \ "m4fw_name=rproc-m4-fw.elf\0" \ "m4fw_addr=${kernel_addr_r}\0" \ "boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \ "boot_m4_mmc0=if ext4load mmc 0:4 ${m4fw_addr} ${m4fw_name} ; then run boot_m4fw; fi;\0" "bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0"
NB: check STM32MP15_U-Boot for compilation.
3.2.2. Start from a generic DISTRO boot script[edit source]
Without U-boot recompilation, you can also use a DISTRO boot script boot.scr.uimg to automatically load and run the firmware.
For example, use the following script for boot from mmc 0, boot.scr.cmd:
env set m4fw_name "rproc-m4-fw.elf" env set m4fw_addr ${kernel_addr_r} #load M4 firmware if ext4load mmc 0:4 ${m4fw_addr} ${m4fw_name} then rproc init rproc load 0 ${m4fw_addr} ${filesize} rproc start 0 fi #load kernel and device tree ext4load mmc 0:4 ${kernel_addr_r} uImage ext4load mmc 0:4 ${fdt_addr_r} ${board_name}.dtb # start kernel env set bootargs root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 bootm ${kernel_addr_r} - ${fdt_addr_r}
Then generate associated image using mkimage U-Boot tool:
mkimage -T script -C none -A arm -d boot.scr.cmd boot.scr.uimg
Finally, install boot.scr.uimg in the bootfs partition (following the same procedure used for coprocessor firmware)
sudo cp boot.scr.uimg /media/$USER/bootfs sync
sudo rm -r /media/$USER/bootfs/extlinux sync
3.2.3. Start from the FIT image[edit source]
The coprocessor firmware can be also included in the new U-Boot image format = Flattened uImage Tree (FIT) and then this firmware will be loaded automatically when detected by U-Boot.
See chapter 'Coprocessor firmware' in board/st/stm32mp1/README :
- example of '.its' file is provided < U-Boot directory>/board/st/stm32mp1/fit_copro_kernel_dtb.its
- you generate the FIT with U-Boot mkimage tool:
mkimage -f fit_copro_kernel_dtb.its fit_copro_kernel_dtb.itb
You can load the generated FIT with:
- 'bootm' command (see doc/uImage.FIT/command_syntax_extensions.txt )
- extlinux.conf in bootfs in extlinux directory to automatically load the FIT by generic DISTRO,
for example: < U-Boot directory>/board/st/stm32mp1/extlinux.conf
To go deeper:
- doc/README.pxe
- doc/uImage.FIT/howto.txt
- support of firmware in FIT is done in board_stm32copro_image_process() function in board/st/stm32mp1/stm32mp1.c associated to image type IH_TYPE_STM32COPRO.
4. Synchronize the remote firmware with Linux[edit source]
The STM32MPU Embedded Software distribution provides the ability to detect and manage a firmware loaded by U-Boot thanks to the remoteproc Linux framework.
The developer should pay attention to how he implements the Cortex-M4 firmware if the RPMsg is used for communication with the Linux. In this case a synchronization is required. The cortex-M4 has to wait until the Linux is booted, to start RPMsg communication. When the Linux is ready, the Linux kernel automatically updates the vdev status in the resource table) and sends a signal to the Cortex-M4 using the IPCC peripheral.
Two methods can be implemented to wait for the synchronization:
- Blocking method: The firmware is blocked on MX_OPENAMP_Init call (by the rproc_virtio_wait_remote_ready function) until the Linux kernel is ready to communicate (update of the vdev status in the resource table).
- Non-blocking method: The Linux Kernel generates an interruption on Cortex-M4 using the IPCC peripheral when it is ready to communicate. This interrupt can be used by the Cortex-M4 firmware to initialize the OpenAMP middleware and start the RPMsg protocol.