How to exchange large data buffers with the coprocessor - principle

Revision as of 17:03, 15 November 2019 by Registered User (→‎Introduction)

1. Introduction[edit source]

As explained in "Exchanging_buffers_with_the_coprocessor", the rpmsg protocol can not be enough efficient to directly exchange large buffers between the Cortexes. In this case it is recommended to implement the indirect buffer exchange mode:

  • Allocate contiguous buffers to store the data to exchange,
  • use RPMsg to exchange reference to these buffers with the remote processor.

This article gives an example of mechanism that can be put in place to exchange indirect buffers between a main processor and a coprocessor.

2. Architecture overview[edit source]

This architecture example is mainly relying on a the rpmsg_sdb linux driver.

Copro-sw-ipc-big-data.png

  • On Cortex-A:
  • The rpmsg_sdb driver implements on Linux side the service to allocate and share buffers with the Cortex-M
  • the Linux Application requests and mmaps the buffers to have be able to accesses to the associated memory.
  • On Cortex-M:
  • Application has to implement the "rpmsg-sdb-channel" rpmsg service to manage the buffer information.
  • a DMA can be used to transfer data to/from DDR.

For example, refer to How to exchange large data buffers with the coprocessor - example article.

3. rpmsg_sdb driver[edit source]

The RPMsg shared data buffer driver example in in charge of:

  • allocating large buffers in contiguous memory(DDR) and mmap them for an application usage.
  • implementing the RPMsg service to share buffer information (address, size) with the coprocessor.
  • send event to Linux Application (relying on eventfd interface}) when buffers are available (on RPMsg related message reception).
Info white.png Information
This drivers is only provided as example, Only the transfer from Cortex-M to cortex-A is implemented in the rpmsg_sdb driver

3.1. Configuration[edit source]

3.1.1. Kernel configuration[edit source]

No kernel configuration is needed. The rpmsg_sdb Linux driver is proposed as module and can be installed thanks to the associated Yocto recipe.

3.1.2. Device tree[edit source]

No device tree device tree declaration is needed. The rpmsg_sdb driver is registered as a rpmsg driver. it is probed when the remote processor creates the "rpmsg-sdb-channel" service

3.1.3. Source code[edit source]

the source code is available in the rpsmg-sdb-mod Yocto recipe.

3.2. How to use[edit source]

3.2.1. User space interface[edit source]

The rpmsg_sdb driver exposes a "/dev/rpmsg_sdb" sysfs that offers an interface to allocate and manage the shared buffers.

  • open/close: get/release file descriptor.
  int fd;
  fd= open('/dev/rpmsg_sdb');
  close(fd);
  • mmap: allocate and map memories
  void *buff0_id, *buff1_id;
 
  buff0_id = mmap(NULL, size,  PROT_READ | PROT_WRITE, 	MAP_PRIVATE, fd, 0);
  buff1_id = mmap(NULL, size,  PROT_READ | PROT_WRITE, 	MAP_PRIVATE, fd, 0);
  • ioctrl
  • RPMSG_SDB_IOCTL_SET_EFD
register event for a buffer
  typedef struct
  {
  	int bufferId, eventfd;
  } rpmsg_sdb_ioctl_set_efd;
  
  int efd[NB_BUF];
  rpmsg_sdb_ioctl_set_efd q_set_efd;

  for (i=0;i<NB_BUF;i++){
	/* Create the evenfd, and sent it to kernel driver, for notification of buffer full */
	efd[i] = eventfd(0, 0);
  }
  q_set_efd.bufferId = i;  /* i is the index of the buffer */
  q_set_efd.eventfd = efd[i];
  
  ioctrl(fd, RPMSG_SDB_IOCTL_SET_EFD, buff0_id, &q_set_efd);
  • RPMSG_SDB_IOCTL_GET_DATA_SIZE
get the size of a buffer
  typedef struct
  {
  	int bufferId;
  	uint32_t size;
  } rpmsg_sdb_ioctl_get_data_size;
  
  rpmsg_sdb_ioctl_get_data_size q_get_data_size;

  ioctrl(fd, RPMSG_SDB_IOCTL_GET_DATA_SIZE, buff0_id, eventfd);
  • manage event
  while (1) {
	ret = poll(fds, NB_BUF, TIMEOUT * 1000);
	if (ret < 0) {
		perror("poll()");
		break;
	} else if (ret) {
		printf("Data is available now.\n");
	} else if (ret == 0) {
		printf("No data within five seconds.\n");
		break;
	}
	for (j=0;j<NB_BUF;j++){
		if (fds[j].revents & POLLIN) {
			/* Event received for the buffer j: New data is available for buffer j */
		}
	}
}

3.2.2. RPMsg messaging[edit source]

The RPMsg protocol is used for the communication with the Cortex-M:

  • Information on buffer allocated and mmaped is sent to the Cortex-M.
The message is structured in a string with following format: "BxAyyyyyyyyLzzzzzzzz"
  • x: buffer index,
  • yyyyyyyy: address of the buffer in DDR ( 32 bits format),
  • zzzzzzzz: length of the buffer (32 bits format)
  • Buffer filled event received from the Cortex-M:
When the Cortex-M4 has filled a buffer it can inform the Linux Application by sending a RPMsg with following string Format : "BxLzzzzzzzz"'.
  • x: buffer index,
  • zzzzzzzz: length of the buffer (32 bits format)
On this message reception the rpmsg_sdb driver sends an event to application .
No categories assignedEdit