This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.This article briefly describes the STM32MP15x lines support in U-Boot.
1. STM32MP15x lines support[edit source]
For detailed information, please read the file in the delivered U-Boot code = board/st/stm32mp1/README
Also available in official U-Boot Git.
Code :
- arch/arm/mach-stm32mp : arch specific code for all STM32 Arm® Cortex® MPUs
- board/st/stm32mp1: generic STMicroelectronics board for STM32MP1 Series
- drivers/*/*stm32* : drivers
Configuration Files:
- defconfig file
- configs/stm32mp15_basic_defconfig
- configs/stm32mp15_optee_defconfig
- configs/stm32mp15_trusted_defconfig
- config files
- include/configs/stm32mp1.h
- Device tree
- arch/arm/dts/stm32mp157*-<board>.dts : same as kernel
- arch/arm/dts/stm32mp157*-<board>-u-boot.dtsi : addition for u-boot ( <<device tree>>-u-boot.dtsi automatically included in build process)
2. Selecting targets : choose defconfig and Device Tree[edit source]
Each boot chain is supported by one U-Boot configuration with defconfig
Boot chain | defconfig | FSBL | SSBL | TEE support |
---|---|---|---|---|
Trusted Boot | stm32mp15_trusted_defconfig | TF-A | U-Boot u-boot.stm32 |
- |
Trusted Boot with OP-TEE | stm32mp15_optee_defconfig | TF-A | U-Boot u-boot.stm32 |
yes |
Basic Boot | stm32mp15_basic_defconfig | SPL u-boot-spl.stm32 |
U-Boot u-boot.img |
- |
Several targets/ boards are supported with the associated device-tree (same name as kernel):
Board part number | Description | Device tree |
---|---|---|
STM32MP157C-EV1 Evaluation board | MB1262+MB1263 | stm32mp157c-ev1 |
STM32MP157C-ED1 Evaluation daughterboard | MB1263 | stm32mp157c-ed1 |
STM32MP157A-DK1 Discovery kit | MB1272 | stm32mp157a-dk1 |
STM32MP157C-DK2 Discovery kit | MB1272+MB1407 | stm32mp157c-dk2 |
3. Compilation[edit source]
see U-Boot_overview#U-Boot_build
With <mode> = 'basic', 'trusted' or 'optee'
make stm32mp15_<mode>_defconfig make DEVICE_TREE=<device tree name> all
- DEVICE_TREE: select in arch/arm/dts the device tree that is used
- KBUILD_OUTPUT: change the destination directory for the build
- EXT_DTB: select external device tree
4. Examples[edit source]
4.1. STM32MP157C-EV1 Evaluation board trusted boot[edit source]
make stm32mp15_trusted_defconfig make DEVICE_TREE=stm32mp157c-ev1 all
4.2. STM32MP157C-DK2 Discovery kit trusted boot[edit source]
Using export to select the device tree
export KBUILD_OUTPUT=../build/trusted export DEVICE_TREE=stm32mp157c-dk2 make stm32mp15_trusted_defconfig make all
4.3. STM32MP157C-ED1 Evaluation daughterboard basic boot[edit source]
export KBUILD_OUTPUT=../build/basic make stm32mp15_basic_defconfig make DEVICE_TREE=stm32mp157c-ed1 all
4.4. Trusted boot chain with external device tree[edit source]
make stm32mp15_trusted_defconfig
make EXT_DTB=boot/stm32mp157c-myboard.dtb all