This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. STM32MP15 in U-Boot[edit source]
For detailed information, please read the file in the delivered U-Boot code = board/st/stm32mp1/README
Also available in official U-Boot Git: board/st/stm32mp1/README
1.1. STM32MP15 support[edit source]
Code :
- arch/arm/mach-stm32mp : arch specific code for all STM32 ArmTemplate:Sup CortexTemplate:Sup MPUs
- board/st/stm32mp1: generic STMicroelectronics board for STMP32MP1
- drivers/*/*stm32* : drivers
Configuration Files:
- defconfig file
- configs/stm32mp15_basic_defconfig
- configs/stm32mp15_optee_defconfig
- configs/stm32mp15_trusted_defconfig
- config files
- include/configs/stm32mp1.h
- Device tree
- arch/arm/dts/stm32mp157*-<board>.dts : same than kernel
- arch/arm/dts/stm32mp157*-<board>-u-boot.dtsi : addition for u-boot ( <<device tree>>-u-boot.dtsi automatically include in build process)
1.2. Selecting targets : choose defconfig and Device Tree[edit source]
Each boot chain is supported by one U-Boot configuration with defconfig
Boot chain | defconfig | FSBL | SSBL | TEE support |
---|---|---|---|---|
Trusted Boot | stm32mp15_trusted_defconfig | TF-A | U-Boot u-boot.stm32 |
- |
Trusted Boot with OP-TEE | stm32mp15_optee_defconfig | TF-A | U-Boot u-boot.stm32 |
yes |
Basic Boot | stm32mp15_basic_defconfig | SPL u-boot-spl.stm32 |
U-Boot u-boot.img |
- |
Several targets/ boards are supported with the associated device-tree (same name than kernel):
Board part number | Description | Device tree |
---|---|---|
STM32MP157C-EV1 | Evaluation board PMIC = MB1262+MB1263 |
stm32mp157c-ev1 |
STM32MP157C-ED1 | Evaluation daughter board PMIC = MB1263 |
stm32mp157c-ed1 |
STM32MP157A-DK1 | Discovery kit MB1272 |
stm32mp157a-dk1 |
STM32MP157C-DK2 | Discovery kit MB1272 + DSI screen |
stm32mp157c-dk2 |
1.3. Compilation[edit source]
see U-Boot_overview#U-Boot_build
With <mode> = 'basic', 'trusted' or 'optee'
$> make stm32mp15_<mode>_defconfig $> make DEVICE_TREE=<device tree name> all
- DEVICE_TREE: select the used device tree in arch/arm/dts
- KBUILD_OUTPUT: change the destination directory for the build
- EXT_DTB: select external device tree
2. Examples[edit source]
2.1. EV1 trusted boot[edit source]
$> make stm32mp15_trusted_defconfig $> make DEVICE_TREE=stm32mp157c-ev1 all
2.2. DK2 trusted boot[edit source]
Using export to select the device tree
$> export KBUILD_OUTPUT=../build/trusted $> export DEVICE_TREE=stm32mp157c-dk2 $> make stm32mp15_trusted_defconfig $> make all
2.3. ED1 basic boot[edit source]
$> export KBUILD_OUTPUT=../build/basic $> make stm32mp15_basic_defconfig $> make DEVICE_TREE=stm32mp157c-ed1 all
2.4. Trusted boot chain with external device tree[edit source]
$> make stm32mp15_trusted_defconfig
$> make EXT_DTB=boot/stm32mp157c-myboard.dtb all