This article explains how to build tee components, except the OP-TEE drivers. The latter are part of the Linux build process and are compiled as loadable modules, please refer to How to build kernel for Android. It is intended for Distribution Package users.
The OP-TEE Security feature is composed of several parts:
- OP-TEE drivers: it is include in the Linux Kernel
- OP-TEE OS: is part of bootloader image.
- OP-TEE Client: the OP-TEE userland client and is part of the STM32MPU distribution for Android™.
- OP-TEE Tests: OP-TEE Tests suite with dedicated trusted applications part of the STM32MPU distribution for Android™.
- This module proposes a tests suite for OP-TEE
- Only available when NOT in user building profile
For detail, you can refer to OP-TEE overview page.
1. Prerequisites[edit source]
The environment must be installed using the Distribution Package adapted to your selected microprocessor device. See the list of Android Distribution Package.
To be able to execute the following instructions, you need to work from your distribution root directory, initialize your environment and then run lunch
:
source build/envsetup.sh
bspsetup
lunch aosp-<BoardId>-userdebug
2. Partition layout[edit source]
The OP-TEE OS is separated in three different partitions teeh
, teed
and teex
to allow managing paging.
The OP-TEE TA (Trusted Applications) are integrated in the vendor
partition.
The binaries are available in device/stm/<STM32Series>-tee/prebuilt
.
For the complete partition layout please see STM32MP15 Flash mapping for Android.
3. Load the tee sources[edit source]
By default, the OP-TEE sources are not part of the STM32MPU distribution for Android™. To load the sources, execute the following command:
load_tee
The loaded sources can then be accessed at the device/stm/<STM32Series>-tee/optee_os-<STM32Series>
directory.
4. Build the tee[edit source]
After retrieving the OP-TEE sources you can build them using:
build_tee
This command generate OP-TEE for every available boards. To only generate for one board:
build_tee --board <BoardId>
or
build_tee --current
For more information check the command usage:
build_tee -h
Usage: build_tee [Options] [Board] [Command] This script allows building the OP-TEE OS source Options: -h/--help: print this message -i/--install: update prebuilt images -v/--version: get script version --verbose <level>: enable verbosity (1 or 2 depending on level of verbosity required) Board: Optional (default = all) -c/--current: build only for current configuration (board and memory) or -b/--board <name>: set board name = eval or disco Command: Optional, only one command at a time supported clean: execute make clean on targeted module
5. Integrate the tee[edit source]
To integrate the new OP-TEE solution within your distribution, you have first to update the prebuilt images:
build_tee -i
Then you have to build the full distribution
make -j
Then you can update associated partitions on your device. Please refer to Flashing the built image
6. Build Trusted Applications[edit source]
You can customize trusted applications that need to be built. For that purpose, you have to change the configuration file android_tabuild.config
located in device/stm/<STM32Series>-tee/source
.
To build trusted applications, execute:
build_ta
This script generates every applications for all available boards. To only generate for one board:
build_ta --board <BoardId>
or
build_ta --current
For more information check the command usage:
build_ta -h
Usage: build_ta [Options] [Board options]
This script allows building the trust applications (TA) source listed in android_tabuild.config file
Options:
-h/--help: print this message
-i/--install: update prebuilt images
-v/--version: get script version
--verbose <level>: enable verbosity (1 or 2 depending on level of verbosity required)
Board options:
-c/--current: build only for current configuration (board and memory)
or
-b/--board <name>: set board name = eval or disco (default: all)
7. Integrate Trusted Applications[edit source]
To integrate the new trusted applications within your distribution, you have first to update the prebuilt images:
build_ta -i
Then you have to update the file device.mk
copying the trusted application in the /vendor/lib/optee_armtz
directory.
PRODUCT_COPY_FILES += \ device/stm/<STM32Series>-tee/prebuilt/<BoardId>/ta/<UUID>.ta:$(TARGET_COPY_OUT_VENDOR)/lib/optee_armtz/<UUID>.ta
Then you have to build the full distribution
make -j
Then you can update associated partitions on your device. Please refer to How to populate boards for Android