This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User No edit summary |
Registered User mNo edit summary |
||
Line 19: | Line 19: | ||
rect 260 229 356 286 [[U-Boot overview]] | rect 260 229 356 286 [[U-Boot overview]] | ||
rect 364 229 461 287 [[STM32MP15 Linux kernel overview]] | rect 364 229 461 287 [[STM32MP15 Linux kernel overview]] | ||
poly 255 203 359 203 359 289 140 289 140 224 255 224 [[ | poly 255 203 359 203 359 289 140 289 140 224 255 224 [[Boot_chain_overview|Boot chain overview]] | ||
rect 32 198 469 296 [[OpenSTLinux BSP architecture overview]] | rect 32 198 469 296 [[OpenSTLinux BSP architecture overview]] | ||
rect 364 62 461 121 [[Linux application frameworks overview]] | rect 364 62 461 121 [[Linux application frameworks overview]] |
Latest revision as of 11:12, 25 September 2020
The OpenSTLinux distribution encompasses the following components:
- The OpenSTLinux BSP that offers services, to the application frameworks in the same context, from:
- The boot chain based on TF-A and U-Boot
- The OP-TEE secure OS running on the Cortex-A in secure mode
- The Linux® kernel running on the Arm® Cortex®-A in non-secure mode
- The Application frameworks that rely on the services provided by the OpenSTLinux BSP, to provide particular functionalities (code libraries, APIs, tool sets...) to facilitate the development of software applications:
- The Linux application frameworks (aka Linux middlewares) running on the user space of the Linux OS: e.g. libusb C library for a generic access to USB devices, ALSA user-space bundle for audio functionalities, GStreamer multimedia framework...
- The OP-TEE application frameworks running on the user space of the secure OS: e.g. TEE Internal core API for the development of Trusted Applications (TA)
- The U-Boot application frameworks: e.g. configuration scripts
The figure below is clickable so that the user can directly jump to one of the sub-levels listed above.

OpenSTLinux architecture overview