This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(2 intermediate revisions by one other user not shown) | |||
Line 28: | Line 28: | ||
rect 345 24 420 150 [[Dmaengine overview]] | rect 345 24 420 150 [[Dmaengine overview]] | ||
rect 693 190 768 280 [[DRM KMS overview]] | rect 693 190 768 280 [[DRM KMS overview]] | ||
rect 96 215 171 269 [[I2C overview]] | rect 96 215 171 269 [[I2C overview]] | ||
rect 693 306 767 496 [[IIO overview]] | rect 693 306 767 496 [[IIO overview]] | ||
Line 40: | Line 39: | ||
rect 438 115 504 144 [[WLAN overview]] | rect 438 115 504 144 [[WLAN overview]] | ||
rect 438 154 504 184 [[Bluetooth overview]] | rect 438 154 504 184 [[Bluetooth overview]] | ||
rect 273 216 | rect 273 216 428 359 [[Power overview]] | ||
rect | rect 432 307 507 359 [[Thermal overview]] | ||
rect 432 216 507 303 [[Regulator overview]] | rect 432 216 507 303 [[Regulator overview]] | ||
rect 179 118 253 169 [[Reset overview]] | rect 179 118 253 169 [[Reset overview]] | ||
rect 95 118 170 169 [[RTC overview]] | rect 95 118 170 169 [[RTC overview]] |
Latest revision as of 19:22, 11 January 2021
This section gives an overview of Linux® kernel drivers (UPPERCASE in the figure) implemented for the STM32MP15 support, with their respective software frameworks (lowercase in the figure).
The components are grouped per functional domains.
Each Linux framework is further described in Linux operating system category articles.
Each STM32 MPU peripheral is introduced in peripherals overview articles.
Both those sections are reusing the same functional domain split.
The color code, explained in the legend, allows to see the code origin for each component.

STM32MP15 Linux kernel overview