This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Registered User mNo edit summary |
Registered User mNo edit summary |
||
(4 intermediate revisions by the same user not shown) | |||
Line 1: | Line 1: | ||
MB1263 board overview. | |||
== Board overview == | == Board overview == | ||
'''Daughterboard MB1263''' ( | '''Daughterboard MB1263''' (STM32MP157x 18x18 with PMIC and DDR3), revision C-0.1: part of the {{Board | type=157x-EV1}}. | ||
{{ | {{ | ||
ImageMap|Image:MB1263_front_side.png {{!}} thumb{{!}}500px{{!}} center{{!}} MB1263 front side | ImageMap|Image:MB1263_front_side.png {{!}} thumb{{!}} 500px{{!}} center{{!}} MB1263 front side (picture is not contractual) | ||
rect | rect 34 34 73 91 [[#Reset button | Reset button]] | ||
rect | rect 73 17 93 82 [[#LED 2 | User LED (red LD2)]] | ||
rect | rect 93 18 113 82 [[#User button 13 | User button (PA13)]] | ||
rect | rect 127 18 147 82 [[#LED 3 | User LED (green LD3)]] | ||
rect | rect 147 18 167 82 [[#User button 14 | User button (PA14)]] | ||
rect | rect 167 18 180 82 [[#LED 5 | User LED (blue LD5)]] | ||
rect | rect 180 18 193 82 [[#LED 4 | User LED (orange LD4)]] | ||
rect | rect 193 18 213 82 [[#Wakeup button | Wakeup button]] | ||
rect | rect 258 18 291 53 [[#LED 1 | Power LED (green LD1)]] | ||
rect | rect 392 23 472 84 [[#Power | Power 5V-3A]] | ||
rect | rect 26 100 109 157 [[#Boot | Boot mode selection]] | ||
rect | rect 142 82 191 128 [[#JP4 JP5 Jumpers | Jumpers to connect the UART4 to the ST-LINK/V2-1 or to the mother board USB micro-AB]] | ||
rect | rect 223 86 325 193 [[#PMIC | PMIC (STPMIC1A)]] | ||
rect | rect 415 84 472 106 [[#LED 6 | ST-LINK/V2-1 LED (bicolor LD6)]] | ||
rect | rect 380 106 472 156 [[#ST-LINK USB | USB micro-B (ST-LINK/V2-1)]] | ||
rect | rect 130 252 251 374 [[#STM32MP157x | STM32MP157x 18x18]] | ||
rect | rect 291 274 363 348 [[#eMMC | eMMC]] | ||
rect | rect 130 395 204 614 [[#DDR3L | 2 x DDR3L 16 bits]] | ||
rect 283 542 472 632 [[#MicroSD | microSD 3.0 card]] | |||
}} | }} | ||
Line 40: | Line 33: | ||
{{ | {{ | ||
ImageMap|Image:MB1263_back_side.png {{!}} thumb{{!}}500px{{!}} center{{!}} MB1263 back side | ImageMap|Image:MB1263_back_side.png {{!}} thumb{{!}}500px{{!}} center{{!}} MB1263 back side (picture is not contractual) | ||
rect 454 31 | rect 454 31 585 177 [[#Battery | Lithium battery 3V]] | ||
rect | rect 119 200 186 264 [[#ST-LINK | ST-LINK/V2-1]] | ||
rect | rect 28 264 585 500 [[#Samtec | 2 x Samtec connectors]] | ||
rect 28 666 178 810 [[#MicroSD slot | microSD 3.0 card]] | |||
}} | }} | ||
== Links == | == Links == | ||
[[STM32MP15 resources#MB1263 schematics|MB1263 schematics]] | [[STM32MP15 resources#MB1263 schematics|MB1263 schematics]] | ||
<noinclude> | |||
{{PublicationRequestId | 7568 | 2018-06-19 | AlainF}} | |||
[[Category:STM32MP15 Evaluation boards]] | |||
[[Category:STM32MP15]] | |||
[[Category:ST boards]] | |||
</noinclude> |
Latest revision as of 12:52, 15 June 2020
MB1263 board overview.
1. Board overview[edit source]
Daughterboard MB1263 (STM32MP157x 18x18 with PMIC and DDR3), revision C-0.1: part of the STM32MP157x-EV1 Evaluation board .
Details of some LEDs:
- LD1: green if power connection established
- LD6: red flashing if ST-LINK/V2-1 connection not established, else green
- LD2, LD3, LD4, LD5: some user LEDs are used to reflect the system activity, whereas the others are left free and can be directly used by the application, as explained in the LEDs and buttons on STM32 MPU boards article
2. Links[edit source]