deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
==Article purpose== | ==Article purpose== | ||
The main goal of this article is to describe how to customize images to fit application requirements.<br> | The main goal of this article is to describe how to customize images to fit application requirements.<br> | ||
Line 24: | Line 17: | ||
├── {{Highlight|meta}} | ├── {{Highlight|meta}} | ||
│ ├── {{Highlight|classes}} | │ ├── {{Highlight|classes}} | ||
│ ├── {{ | │ ├── {{HighlightParam|core-image.bbclass}} | ||
│ ├── {{Highlight|recipes-core}} | │ ├── {{Highlight|recipes-core}} | ||
│ ├── {{Highlight|images}} | │ ├── {{Highlight|images}} | ||
│ ├── {{ | │ ├── {{HighlightParam|core-image-base.bb}} | ||
└── [...] | └── [...] | ||
Line 46: | Line 39: | ||
├── {{Highlight|recipes-st}} | ├── {{Highlight|recipes-st}} | ||
│ ├── {{Highlight|images}} | │ ├── {{Highlight|images}} | ||
│ ├── {{ | │ ├── {{HighlightParam|st-image-core.bb}} | ||
│ ├── st-image.inc | │ ├── st-image.inc | ||
│ ├── {{ | │ ├── {{HighlightParam|st-image-weston.bb}} | ||
│ ├── {{Highlight|packagegroups}} | │ ├── {{Highlight|packagegroups}} | ||
│ ├── {{ | │ ├── {{HighlightParam|packagegroup-framework-tools.bb}} | ||
└── [...] | └── [...] | ||
Line 62: | Line 55: | ||
├── {{Highlight|recipes-samples}} | ├── {{Highlight|recipes-samples}} | ||
│ ├── {{Highlight|images}} | │ ├── {{Highlight|images}} | ||
│ ├── {{ | │ ├── {{HighlightParam|st-example-image-qt.bb}} | ||
│ ├── {{ | │ ├── {{HighlightParam|st-example-image-x11.bb}} | ||
│ ├── {{ | │ ├── {{HighlightParam|st-example-image-xfce.bb}} | ||
│ │ [...] | │ │ [...] | ||
└── [...] | └── [...] | ||
Line 72: | Line 65: | ||
The way recommended and used by ST is to follow the method described in chapters '''Customizing Images Using Custom .bb Files''' and '''Customizing Images Using Custom Package Groups''' of Yocto Megamanual. | The way recommended and used by ST is to follow the method described in chapters '''Customizing Images Using Custom .bb Files''' and '''Customizing Images Using Custom Package Groups''' of Yocto Megamanual. | ||
<noinclude> | |||
{{PublicationRequestId | 8444 | 2018-09-20 | BrunoB}} | |||
[[Category:How to customize software]] | |||
</noinclude> |
Revision as of 11:44, 24 September 2019
1. Article purpose
The main goal of this article is to describe how to customize images to fit application requirements.
The idea is to add missing tools in the user file system.
Tools are related to kernel, network, audio, ui, ...
2. Prerequisites
The OpenSTLinux distribution delivery must be already installed.
3. Available ST images
3.1. OpenEmbedded images
The OpenEmbedded build system provides severals example images to satisfy different needs.
All details are explained Yocto Megamanual Reference Images
Some existing images are located here: <path of OpenSTLinux distribution delivery>/openembedded-core/meta/recipes-*/images/*.bb
The core-image-base can be a good starting points and a source or inspiration for creating user's own images:
Template:Highlight ├── Template:Highlight │ ├── Template:Highlight │ ├── core-image.bbclass │ ├── Template:Highlight │ ├── Template:Highlight │ ├── core-image-base.bb └── [...]
In addition OpenSTLinux Distribution provides even more images, still derived from OpenEmbedded, and that can be used as example and for demonstration.
Template:Warning
3.2. Official OpenSTLinux images
- st-image-weston : OpenSTLinux weston image with basic Wayland support (if enable in distro)
This image is located here : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-openstlinux/recipes-st/images/st-image-weston.bb
3.3. Others OpenSTLinux images
3.3.1. Supported images
- st-image-core : OpenSTLinux core image
This image is located here : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-openstlinux/recipes-st/images/st-image-core.bb
Template:Highlight ├── Template:Highlight │ ├── Template:Highlight │ ├── st-image-core.bb │ ├── st-image.inc │ ├── st-image-weston.bb │ ├── Template:Highlight │ ├── packagegroup-framework-tools.bb └── [...]
3.3.2. Images proposed as example-only
- st-example-image-qt : ST example of image based on QT framework (require 'openstlinux-eglfs' distro)
- st-example-image-x11 : ST example of image based on X11 (require 'openstlinux-x11' distro)
- st-example-image-xfce : ST example of image based on XFCE framework (require 'openstlinux-x11' distro)
More images are available here : <path of OpenSTLinux distribution delivery>/meta-st/meta-st-openstlinux/recipes-samples/images/
Template:Highlight ├── Template:Highlight │ ├── Template:Highlight │ ├── st-example-image-qt.bb │ ├── st-example-image-x11.bb │ ├── st-example-image-xfce.bb │ │ [...] └── [...]
4. Customizing images
Several ways are explained and described here Yocto Megamanual Customizing Images
The way recommended and used by ST is to follow the method described in chapters Customizing Images Using Custom .bb Files and Customizing Images Using Custom Package Groups of Yocto Megamanual.