This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.deleted>Frq08988 mNo edit summary |
Registered User mNo edit summary |
||
Line 1: | Line 1: | ||
<noinclude> | <noinclude> | ||
{{ArticleApprovedVersion | Jean-ChristopheT | NathalieS (23May'18, Done), BernardP (22 May'18, Pass) | No previous approved version | AlainF - 19Jun'18 - 7570 | 20Jun'18}} | {{ArticleApprovedVersion | Jean-ChristopheT | NathalieS (23May'18, Done), BernardP (22 May'18, Pass) | No previous approved version | AlainF - 19Jun'18 - 7570 | 20Jun'18}} | ||
[[Category:STM32MP15 Evaluation boards]] | [[Category:STM32MP15 Evaluation boards]] | ||
[[Category:STM32MP15]] | [[Category:STM32MP15]] | ||
Line 10: | Line 7: | ||
== Board overview == | == Board overview == | ||
'''Motherboard MB1262''', revision C: part of the | '''Motherboard MB1262''', revision C-0.1: part of the STM32MP157x-EV1 Evaluation board | ||
{{ | {{ | ||
ImageMap|Image:MB1262_front_side. | ImageMap|Image:MB1262_front_side.jpg {{!}} thumb{{!}} 500px{{!}} center{{!}} MB1262 front side (picture is not contractual) | ||
rect | rect 74 29 193 333 [[#Ethernet | Ethernet]] | ||
rect | rect 239 61 325 174 [[#Micro | Microphone MEMS daughterboard connector]] | ||
rect | rect 412 181 509 272 [[#Audio codec | Audio codec (Wolfson WM8994)]] | ||
rect | rect 389 44 449 181 [[#Speaker | Audio codec speaker]] | ||
rect | rect 451 44 509 181 [[#Headset | Audio codec headset]] | ||
rect | rect 509 16 589 195 [[#SPDIF RX | SPDIF RX (input)]] | ||
rect | rect 590 16 671 195 [[#SPDIF TX | SPDIF TX (output)]] | ||
rect | rect 772 69 892 206 [[#SmartCard | SmartCard]] | ||
rect | rect 969 60 1086 310 [[#Camera | Camera connector]] | ||
rect | rect 50 375 226 460 [[#Ethernet connector | Ethernet daughterboard connector]] | ||
rect | rect 332 375 740 451 [[#Samtec | 2 x Samtec connectors (daughterboard)]] | ||
rect | rect 486 451 591 540 [[#NAND | NAND Flash]] | ||
rect | rect 890 370 979 527 [[#Trace | Trace connector]] | ||
rect | rect 997 370 1086 527 [[#LTDC | RGB LTDC connector]] | ||
rect | rect 7 472 184 662 [[#UART | RS232]] | ||
rect | rect 184 503 266 615 [[#I2C EXT | External E2P connector]] | ||
rect | rect 20 662 133 718 [[#USB micro-AB | USB micro-AB (OTG)]] | ||
rect | rect 382 611 510 694 [[#QSPI | Quad SPI Flash]] | ||
rect | rect 823 527 906 734 [[#JTAG | JTAG connector]] | ||
rect | rect 906 619 1106 824 [[#CAN FD | CAN FD (Flexible Datarate)]] | ||
rect | rect 7 747 226 1010 [[#USB Type-A | 4 x USB Type-A (host)]] | ||
rect | rect 249 719 325 763 [[#MFX header | MFX header 4 pins]] | ||
rect | rect 370 725 484 845 [[#MFX | MFX (Multi Function eXpander)]] | ||
rect | rect 553 838 713 915 [[#DSI | DSI LCD connector]] | ||
rect | rect 388 1244 470 1323 [[#Reset button | Reset button]] | ||
rect | rect 527 1244 605 1323 [[#Joystick | Joystick]] | ||
rect | rect 936 1017 1008 1292 [[#Motor control | Motor control connector]] | ||
rect | rect 1010 1017 1086 1292 [[#GPIO | GPIO expansion]] | ||
}} | }} | ||
{{ | {{ | ||
ImageMap|Image:MB1262_back_side. | ImageMap|Image:MB1262_back_side.jpg {{!}} thumb{{!}} 500px{{!}} center{{!}} MB1262 back side (picture is not contractual) | ||
rect | rect 161 59 456 241 [[#SmartCard | SmartCard]] | ||
}} | }} | ||
== Links == | == Links == | ||
[[STM32MP15 resources#MB1262 schematics|MB1262 schematics]] | [[STM32MP15 resources#MB1262 schematics|MB1262 schematics]] |
Revision as of 11:02, 27 February 2019
Template:ArticleApprovedVersion
1. Board overview
Motherboard MB1262, revision C-0.1: part of the STM32MP157x-EV1 Evaluation board