This category groups together all articles that are applicable for the STM32MP13x lines
Subcategories
This category has the following 9 subcategories, out of 9 total.
A
M
O
S
X
Pages in category "STM32MP13x"
The following 200 pages are in this category, out of 587 total.
(previous page) (next page)H
- How to develop an OP-TEE Trusted Application with STM32CubeIDE
- How to develop an X-Linux Expansion Package
- How to diagnose a boot failure
- How to display an image using Weston
- How to display on HDMI
- How to enable earlycon for Linux kernel
- How to enable secure boot on STM32 MPU
- How to encrypt a disk with dm-crypt
- How to ensure data coherency when cache and MMU used in STM32CubeMP13
- How to find Linux kernel driver associated to a device
- How to get DRM KMS logs
- How to get name and current status of a DRM connector
- How to get started with STM32CubeIDE from scratch
- How to get Terminal
- How to get video details
- How to install JAVA JDK
- How to install OPC UA
- How to install the Yocto Project SDK in STM32CubeIDE
- How to install X-TouchGFX MPU Addon
- How to integrate an external software package
- How to load and start STM32CubeMP13 applications via eMMC storage
- How to load and start STM32CubeMP13 applications via microSD card
- How to load and start STM32CubeMP13 applications via SNOR flash
- How to load U-Boot with dfu-util
- How to load U-Boot with STM32CubeProgrammer
- How to make a camera preview
- How to make a screen capture in Weston
- How to make a video capture of Weston desktop
- How to manage OpenSTLinux projects in STM32CubeIDE
- How to manage OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure acceleration and orientation
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure performance of your NN models using the Coral Edge TPU
- How to measure temperature and humidity
- How to measure the DDR throughput
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to optimize the boot time
- How to perform digital signature with TPM
- How to perform ping test
- How to perform Secure Boot from Distribution package
- How to perform ssh connection
- How to play a video
- How to play audio
- How to populate the SD card with dd command
- How to prevent the year 2038 bug
- How to profile video framerate
- How to read or write peripheral registers
- How to record audio
- How to reproduce an example using PyCoral API
- How to run Coral Edge TPU inference using Python TensorFlow Lite API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to set up proxy and P2P Ethernet connection with STM32CubeIDE
- How to setup a WLAN connection
- How to setup target password in STM32CubeIDE
- How to stop and start Weston
- How to stream camera over network
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to transfer a file over network
- How to transfer a file over serial console
- How to update OTP with U-Boot
- How to use SPI from Linux userland with spidev
- How to use STM32CubeProgrammer to populate a board
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- How to use the RTC
- How to use the secure display feature
- How to use the Target Status widget in STM32CubeIDE
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
I
- I-LINUX-INFINEON-WLAN OpenSTLinux Expansion Package
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S device tree configuration
- I2S Linux driver
- Ifconfig
- IIO libiio
- IIO Linux kernel tools
- IIO overview
- Image classification
- Install the IDE
- Install the SDK
- Interrupt overview
- Introduction to Azure RTOS with STM32
- Introduction to FILEX
- Introduction to LEVELX
- Introduction to NETXDUO
- Introduction to THREADX
- Introduction to USBX
- IO expander hardware components
- IP Linux command line
- ISSI
- IWave Systems
- IWDG device tree configuration
- IWDG internal peripheral
L
M
N
O
- Object detection
- Octavo Systems
- Online Linux trainings
- OP-TEE Calibration PTA overview
- OP-TEE concepts overview
- OP-TEE configuration switches
- OP-TEE OTP overview
- OPC UA overview
- OpenEmbedded
- OpenEmbedded - devtool
- OpenSTLinux architecture overview
- OpenSTLinux BSP architecture overview
- OpenSTLinux directory structure
- OpenSTLinux distribution
- OpenSTLinux filesystem
- OpenSTLinux licenses
- LegalInformation:OpenSTLinux licenses - v4.0.0
- LegalInformation:OpenSTLinux licenses - v4.1.0
- LegalInformation:OpenSTLinux licenses - v5.0.0
- OTG device tree configuration
- OTG internal peripheral
- Overview of GPIO pins
P
- Package repository for OpenSTLinux distribution
- PC prerequisites
- Pengutronix
- Perf
- PHY overview
- PHYTEC
- Pinctrl device tree configuration
- Pinctrl overview
- PKA device tree configuration
- PKA internal peripheral
- PMIC hardware components
- Populate the target and boot the image
- Power overview
- Prevas
- PRG-TOOLBOX-DFU
- PRG-TOOLBOX-DFU release note
- PRG-TOOLBOX-FB
- PRG-TOOLBOX-FB release note
- ProvenRun
- Pseudo filesystem
- PWM overview
- PWR internal peripheral