This category groups together all articles that are applicable for the[STM32MP15_microprocessor:
- STM32MP151 line
- STM32MP153 line
- STM32MP157 line
Subcategories
This category has the following 8 subcategories, out of 8 total.
A
M
O
S
X
Pages in category "STM32MP15x"
The following 200 pages are in this category, out of 655 total.
(previous page) (next page)H
- How to configure U-Boot for your board
- How to configure U-Boot to support Fastboot mode
- How to configure UEFI boot with the Distribution Package
- How to configure uniprocessor mode
- How to configure Weston screen resolution
- How to control a GPIO in kernel space
- How to control a GPIO in userspace
- How to control a RNG in userspace
- How to convert a Tensorflow Lite model to ONNX using tf2onnx
- How to copy and paste in the STM32CubeIDE console
- How to create a compiled NN model using TVM
- How to create a new open embedded layer
- How to create an SDK for OpenSTLinux distribution
- How to create Signed FIT image from Distribution package
- How to create your board device tree
- How to create your own distribution
- How to create your own image
- How to create your own machine
- How to create your product from design to manufacturing
- How to cross-compile with the Developer Package
- How to cross-compile with the Distribution Package
- How to customize the Linux kernel
- How to debug a user space application with STM32CubeIDE
- How to debug a user space application with STM32CubeIDE/User space CDT project
- How to debug a user space application with STM32CubeIDE/User space GTK library project
- How to debug a user space application with STM32CubeIDE/User space project
- How to debug a user space application with STM32CubeIDE/User space shared library project
- How to debug a user space application with STM32CubeIDE/User space static library project
- How to debug OP-TEE
- How to debug TF-A BL2
- How to debug Weston
- How to debug with Serial Wire Viewer tracing on STM32MP15
- How to define your low-power strategy
- How to deploy SSP: a step-by-step approach
- How to deploy your NN model on STM32MPU
- How to detect memory leaks
- How to detect objects with AI
- How to develop a Rust Application
- How to develop an OP-TEE Trusted Application
- How to develop an OP-TEE Trusted Application with STM32CubeIDE
- How to develop an X-Linux Expansion Package
- How to diagnose a boot failure
- How to disable one CPU
- How to display an image using Weston
- How to display on HDMI
- How to enable earlycon for Linux kernel
- How to enable secure boot on STM32 MPU
- How to exchange data buffers with the coprocessor
- How to find Linux kernel driver associated to a device
- How to get DRM KMS logs
- How to get name and current status of a DRM connector
- How to get started with STM32CubeIDE from scratch
- How to get Terminal
- How to get video details
- How to install a simple web browser
- How to install JAVA JDK
- How to install Node-RED
- How to install OPC UA
- How to install the Yocto Project SDK in STM32CubeIDE
- How to integrate an external software package
- How to integrate Azure IoT Edge on OpenSTLinux
- How to launch glmark2 benchmark
- How to launch Khronos OpenGLES conformance tests
- How to load U-Boot with dfu-util
- How to load U-Boot with STM32CubeProgrammer
- How to make a camera preview
- How to make a screen capture in Weston
- How to make a video capture of Weston desktop
- How to manage OpenSTLinux projects in STM32CubeIDE
- How to manage OpenSTLinux projects in STM32CubeIDE/eMMC update with customized trusted image
- How to manage OpenSTLinux projects in STM32CubeIDE/NAND update with customized trusted image
- How to manage OpenSTLinux projects in STM32CubeIDE/NOR update with customized trusted image
- How to manage OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure acceleration and orientation
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure performance of your NN models using the Coral Edge TPU
- How to measure performance of your NN models using TVM runtime
- How to measure temperature and humidity
- How to measure the DDR throughput
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to monitor the GCNANO GPU load
- How to move from SW4STM32 to STM32CubeIDE
- How to optimize the boot time
- How to perform digital signature with TPM
- How to perform ping test
- How to perform Secure Boot from Distribution package
- How to perform ssh connection
- How to play a video
- How to play audio
- How to populate the SD card with dd command
- How to prevent the year 2038 bug
- How to profile video framerate
- How to protect the coprocessor firmware
- How to read or write peripheral registers
- How to record audio
- How to reproduce an example using PyCoral API
- How to retrieve Cortex-M4 logs after crash
- How to run Coral Edge TPU inference using Python TensorFlow Lite API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to set up proxy and P2P Ethernet connection with STM32CubeIDE
- How to setup a WLAN connection
- How to setup target password in STM32CubeIDE
- How to start the coprocessor from the bootloader
- How to stop and start Weston
- How to stream camera over network
- How to structure the software to develop STM32Cube examples
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to test and benchmark OpenGLES
- How to transfer a file over network
- How to transfer a file over serial console
- How to transfer files to Discovery kit using Tera Term on Windows PC
- How to tune a NN model using TVM
- How to update OTP with U-Boot
- How to use engineering and production modes
- How to use SPI from Linux userland with spidev
- How to use STM32CubeProgrammer to populate a board
- How to use TCP console in STM32CubeIDE
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- How to use the RTC
- How to use the Target Status widget in STM32CubeIDE
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
- HSEM device tree configuration
- HSEM internal peripheral
I
- I-LINUX-INFINEON-WLAN OpenSTLinux Expansion Package
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S device tree configuration
- I2S Linux driver
- Ifconfig
- IIO libiio
- IIO Linux kernel tools
- IIO overview
- IKS01A2 MEMS expansion board
- IKS01A3 MEMS expansion board
- Image classification
- Install the IDE
- Install the SDK
- Interrupt overview
- IO expander hardware components
- IP Linux command line
- IPCC device tree configuration
- IPCC internal peripheral
- ISSI
- IWave Systems
- IWDG device tree configuration
- IWDG internal peripheral
L
- LEDs and buttons on STM32 MPU boards
- LegalInformation:Legal notice
- Linaro
- Linux application frameworks overview
- Linux Mailbox framework overview
- Linux remoteproc framework overview
- Linux RPMsg framework overview
- Linux tracing, monitoring and debugging
- LPTIM device tree configuration
- LPTIM internal peripheral
- LPTIM Linux driver
- LTDC device tree configuration
- LTDC internal peripheral
- Ltrace
- LTTng