This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Using a custom project structure and custom hardware abstraction layer
1 Start with the reference project structure in the preferred IDE
- Use STM32 project templates or STM32 example projects as references for STM32C5 startup code and peripherals usage. STM32 example libray
2 Build the own API to access the STM32C5 features
- An application‑specific API can be built on top of STM32C5 HAL2 or LL drivers, which can be downloaded from the STM32CubeC5 embedded software package at the following link: STM32CubeC5 embedded software.
- Custom drivers can also be developed based on the STM32C5 hardware documentation.