Populate the target and boot the image


1. Overview[edit | edit source]

This stage explains how to get, install and boot the STM32MP15 Discovery kit with the Starter Package.



2. Open a terminal[edit | edit source]

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace
cd $HOME/STM32MPU_workspace

3. Check the host computer Internet access[edit | edit source]

  • An Internet access through http and https protocols must be provided.

The command below enables checking for Internet access through http/https protocols:

wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.

Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:

export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access using the command:

wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4. Install the tools[edit | edit source]

4.1. STM32CubeProgrammer[edit | edit source]

  • Create your "STM32MPU tools" directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
cd $HOME/STM32MPU_workspace/tmp


4.2. Installing the STM32CubeProgrammer tool[edit | edit source]

STM32CubeProgrammer for Linux® host PC STM32CubeProgrammer for Windows® host PC
Download
  • Go on st.com to download the STM32CubeProgrammer software

Version v2.20.0

  • Download the archive file on your host PC in a temporary directory
  • Uncompress the archive file to get the STM32CubeProgrammer installers:

unzip en.stm32cubeprog.zip

Installation
  • Execute the Linux installer, which guides you through the installation process.
$> ./SetupSTM32CubeProgrammer-2.20.0.linux
  • The path to the STM32CubeProgrammer binary must be added to the PATH environment variable
    • either in each Terminal program in which the STM32CubeProgrammer binary needs to be used, using the following command:
$> export PATH=<my STM32CubeProgrammer install directory>/bin:$PATH
  • or once for all by creating a link to the STM32CubeProgrammer binary in a directory already present in PATH. For example, if "/home/bin" is in the PATH environment variable, run the following command:
$> ln -s <my STM32CubeProgrammer install directory>/bin/STM32_Programmer_CLI /home/bin/STM32_Programmer_CLI
  • Execute the Windows installer, which guides you through the installation process.
User manual
Detailed release note
  • Details about the content of this tool version are available from ST web site at Release Note .


4.3. Preparing the USB serial link for flashing[edit | edit source]

It is recommended to use the USB (in DFU mode) for flashing rather than the UART, which is too slow.

Below indications on how to install the USB in DFU mode under Linux and Windows OS, respectively.

  • For Linux host PC or Windows host PC with VMWare:

The libusb1.0 package (including USB DFU mode) must be installed to be able to connect to the board via the USB port. This is achieved by typing the following command from the host PC terminal:

sudo apt-get install libusb-1.0-0

To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:

cd <your STM32CubeProgrammer install directory>/Drivers/rules 
sudo cp *.* /etc/udev/rules.d/
  • For Windows host PC:

Run the “STM32 Bootloader.bat” file to install the STM32CubeProgrammer DFU driver and activate the STM32 microprocessor device in USB DFU mode. This driver (installed by STM32 Bootloader.bat) is provided within the STM32CubeProgrammer release package. It is located in the DFU driver folder, \Drivers\DFU_Driver.

In case of issue, refer to How to proceed when the DFU driver installation fails on Windows host PC.

To validate the installation, the DFU driver functionality can be verified by following the FAQ instructions provided in how to check if the DFU driver is functional.


5. Test[edit | edit source]

  • Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

6. Download the image[edit | edit source]

6.1. For STM32MP1 series[edit | edit source]


  • The STM32MP1 image (binaries) is delivered through one tarball file named
    • FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz for STM32MP135x-DK More info green.png, STM32MP157x-DKx More info green.png and STM32MP157x-EV1 More info green.png

  • Download and install the STM32MP1 image (binaries):

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32MP1 Starter Package image - STM32MP1-Ecosystem-v6.1.0 release
Download
  • Go on st.com to download the STM32MP1 Starter Package image, FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz file.
Installation
cd <working directory path>/Starter-Package
  • Download the tarball file in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files:
tar xvf FLASH-stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz
Release note

Details of the content of this software package are available in the associated STM32 MPU OpenSTLinux release note.
Archive box.png If you are interested in older releases, please have a look into the section Archives

  • The binaries and the Flash layout files are in the <Starter Package installation directory>/stm32mp1-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/images/stm32mp1/ directory. The most important ones are:
stm32mp1
├── arm-trusted-firmware                                                               TF-A binaries
│   ├── bl2                                                                            TF-A binary for FIP binaries creation
│   │   ├── tf-a-<board name>-<boot chain>-<storage>.bin
│   │   └── [...]
│   ├── debug                                                                          Debug binaries for TF-A
│   │   ├── debug-tf-a-<board name>-<boot chain>-<storage>.stm32                       Debug file for FSBL
│   │   ├── tf-a-bl2-<soc name>-<boot chain>-<storage>.elf                             Debug symbol file for TF-A
│   │   └── [...]
│   ├── fwconfig                                                                       TF-A device tree for FIP binaries creation
│   │   ├── <board name>-fwconfig-<boot chain>-<storage>.dtb
│   │   └── [...]
│   ├── metadata.bin                                                                   Meta data binary for METADATA partition for the supported boards
│   ├── tf-a-<board name>-<boot chain>-<storage>.stm32                                 TF-A binary for FSBL partition
│   └── [...]
├── fip                                                                                FIP binaries for FIP partitions and supported boot chains
│   ├── fip-<board name>-<boot chain>-<storage>.bin                                    FIP binary for FIP partition
│   ├── fip-<board name>-<boot chain>-<storage>.txt                                    Configuration file for FIP binary content
│   └── [...]
├── flashlayout_st-image-weston                                                        Flash layout files (description of the partitions) for the supported boot chains on supported boot devices and boards
│   ├── extensible                                                                     Flash layout files for microSD card boot device with no userfs partition but a rootfs partition extended to microSD card size
│   │   ├── FlashLayout_sdcard_<board name>-extensible.tsv                             (recommended setup for package repository service) microSD card boot device with rootfs partition extended to microSD card size
│   │   └── [...]
│   ├── fastboot
│   │   ├── FlashLayout_<boot device>_<board name>-fastboot.tsv
│   │   └── [...]
│   ├── fastboot-opteemin
│   │   ├── FlashLayout_<boot device>_<board name>-fastboot-opteemin.tsv
│   │   └── [...]
│   ├── optee
│   │   ├── FlashLayout_<boot device>_<board name>-optee.tsv
│   │   └── [...]
│   └── opteemin
│       ├── FlashLayout_<boot device>_<board name>-opteemin.tsv
│       └── [...]
├── Kernel                                                                              Debug binaries for Linux kernel
│   ├── config-6.6.78                                                                   Reference config file for Linux kernel
│   ├── [...]
│   └── vmlinux                                                                         Image of the Linux kernel
├── optee                                                                               OPTEE-OS binaries
│   ├── debug                                                                           Debug binaries for OPTEE-OS
│   │   ├── tee-<board name>-<boot chain>.elf                                           Debug symbol file for OPTEE-OS
│   │   ├── tee-<board name>-<boot chain>-programmer.elf                                Debug symbol file for OPTEE-OS configured for usb/serial
│   │   └── [...]
│   ├── tee-header_v2-<board name>-<boot chain>.bin                                   OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-header_v2-<board name>-<boot chain>-programmer.bin                        OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pageable_v2-<board name>-<boot chain>.bin                                 OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pageable_v2-<board name>-<boot chain>-programmer.bin                      OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pager_v2-<board name>-<boot chain>.bin                                    OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pager_v2-<board name>-<boot chain>-programmer.bin                         OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   └── [...]
├── scripts
│   └── create_sdcard_from_flashlayout.sh
├── u-boot                                                                              U-BOOT binaries
│   ├── debug                                                                           Debug binaries for U-BOOT
│   │   ├── u-boot-<soc name>-<u-boot config>.elf                                       Debug symbol file for U-BOOT
│   │   └── [...]
│   ├── configuration-<soc name>-<u-boot config>_defconfig                              Reference configuration file for U-Boot
│   ├── u-boot-nodtb-<soc name>-<u-boot config>.bin                                   U-BOOT binary for FIP binaries creation
│   ├── u-boot-<board name>-<u-boot config>.dtb                                         U-BOOT device tree for FIP binaries creation
│   └── [...]
├── st-image-bootfs-openstlinux-weston-stm32mp1.bootfs.ext4                             Binary for bootfs partition on eMMC and microSD card devices
├── st-image-bootfs-openstlinux-weston-stm32mp1.bootfs.manifest
├── st-image-bootfs-efi-openstlinux-weston-stm32mp1.bootfs.vfat                         Binary for bootfs for EFI partition on eMMC and microSD card devices
├── st-image-bootfs-efi-openstlinux-weston-stm32mp1.bootfs.manifest
├── st-image-userfs-openstlinux-weston-stm32mp1.userfs.ext4                             Binary for userfs partition on eMMC and microSD card devices
├── st-image-userfs-openstlinux-weston-stm32mp1.userfs.manifest
├── st-image-vendorfs-openstlinux-weston-stm32mp1.vendorfs.ext4                         Binary for vendorfs partition on eMMC and microSD card devices
├── st-image-vendorfs-openstlinux-weston-stm32mp1.vendorfs.manifest
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs.ext4                             Binary for rootfs partition on eMMC and microSD card devices
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs.license
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs-license_content.html             License summary for all packages needed to feed all partitions
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs.manifest
├── st-image-weston-openstlinux-weston-stm32mp1.rootfs_nand_4_256_1024_multivolumde.ubi Binary for ubi partition on NAND device
└── [...]

Description:

<board name>:
* stm32mp135f-dk
* stm32mp157a-dk1, stm32mp157a-ev1, stm32mp157c-dk2, stm32mp157c-ed1, stm32mp157c-ev1, stm32mp157d-dk1, stm32mp157d-ev1, ,stm32mp157f-dk2, stm32mp157f-ed1, stm32mp157f-ev1
<soc name>:
* stm32mp13
* stm32mp15
<boot chain>:
* fastboot                  optee boot chain for flashing via fastboot
* fastboot-opteemin         opteemin boot chain for flashing via fastboot
* optee                     optee boot chain
* opteemin                  opteemin boot chain
<boot device>:
* emmc                      Boot via emmc storage
* nor-sdcard                Boot via nor storage for first stage (fsbl, fip) and files system are located on sdcard
* nand-4-256-1024-sdcard    Boot via nand storage for first stage (fsbl, fip) and files system are located on sdcard
* sdcard                    Boot via sdcard storage
* sdcard-EFI                Boot via sdcard storage and bootfs is configurated on EFI
<storage>:
* emmc                      emmc storage
* nor                       nor storage
* nand                      nand storage
* programmer-uart           storage programmation via UART
* programmer-usb            storage programmation via USB
* sdcard                    sdcard storage
<u-boot config>:
* default
* fastboot-emmc             Fastboot config enabled with MMC_DEV Id for emmc
* fastboot-sdcard           Fastboot config enabled with MMC_DEV Id for sdcard
* programmer                Programmer config enabled



6.2. For STM32MP2 series[edit | edit source]

Collapse

For A35-TD flavor More info green.png

  • The STM32MP2 image (binaries) is delivered through one tarball file named FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz applicable to STM32MP215F-DK Info.png, STM32MP257F-DK More info green.png for STM32MP23x lines evaluation Info.png, STM32MP257x-DK More info green.png and STM32MP257x-EV1 More info green.png

  • Download and install the STM32MP2 image (binaries):

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA0048). The detailed content licenses can be found here.

STM32MP2 Starter Package image - STM32MP2-Ecosystem-v6.1.0 release for A35-TD flavor More info green.png
Download

Go on st.com to download the STM32MP2 Starter Package image, FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz file.

Installation
cd <working directory path>/Starter-Package
  • Download the tarball file in this directory
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files:
tar xvf FLASH-stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11.tar.gz
Release note

Details of the content of this software package are available in the associated STM32 MPU OpenSTLinux release note.
Archive box.png If you are interested in older releases, please have a look into the section Archives

  • The binaries and the Flash layout files are in the <Starter Package installation directory>/stm32mp2-openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11/images/stm32mp2/ directory. The most important ones are:
stm32mp2
├── arm-trusted-firmware                                                               TF-A binaries for FSBL partitions and supported boot chains
│   ├── bl2                                                                            TF-A BL2 binary for FIP binaries creation
│   │   ├── tf-a-<board name>-<hardware security>-<boot chain>-<storage>.bin
│   │   └── [...]
│   ├── bl31                                                                           TF-A BL31 binary for FIP binaries creation
│   │   ├── debug                                                                      Debug binaries for BL31
│   │   │   ├── tf-a-bl31-<board name>-<hardware security>-<boot chain>-<storage>.elf      Debug symbol file for TF-A BL31
│   │   │   └── [...]
│   │   ├── <board name>-<hardware security>-<boot chain>-<storage>.dtb                TF-A BL31 device tree for FIP binaries creation
│   │   ├── tf-a-bl31-<board name>-<hardware security>-<boot chain>-<storage>.bin      TF-A BL31 binary for FIP binaries creation
│   │   └── [...]
│   ├── ddr                                                                            Trained DDR binary for FIP binaries creation
│   │   ├── ddr_pmu-<board name>-<hardware security>-<boot chain>-<storage>.bin
│   │   └── [...]
│   ├── debug                                                                          Debug binaries for TF-A
│   │   ├── debug-tf-a-<board name>-<hardware security>-<boot chain>-<storage>.stm32   Debug file for FSBL
│   │   ├── tf-a-bl2-<soc name>-<boot chain>-<storage>.elf                             Debug symbol file for TF-A
│   │   └── [...]
│   ├── fwconfig                                                                       TF-A device tree for FIP binaries creation
│   │   ├── <board name>-<hardware security>-fwconfig-<boot chain>-<storage>.dtb
│   │   └── [...]
│   ├── metadata.bin                                                                   Meta data binary for METADATA partition for the supported boards
│   ├── tf-a-<board name>-<hardware security>-<boot chain>-<storage>.stm32             TF-A binary for FSBL partition
│   └── [...]
├── arm-trusted-firmware-m                                                             TF-M binaries
│   ├── debug                                                                          Debug binaries for TF-M
│   │   ├── tfm-<board name>-<hardware security>_s.elf                                 Debug symbol file for TF-M
│   │   └── [...]
│   ├── tfm-<board name>-<hardware security>_s.bin                                    TF-M binary for m33 firmware as copro
│   └── [...]
├── fip                                                                                FIP binaries for FIP partitions and supported boot chains
│   ├── fip-<board name>-<hardware security>-ddr-<boot chain>-<storage>.bin            FIP binary for FIP DDR partition
│   ├── fip-<board name>-<hardware security>-<boot chain>-<storage>.bin                FIP binary for FIP partition
│   └── [...]
├── flashlayout_st-image-weston                                                        Flash layout files (description of the partitions) for the supported boot chains on supported boot devices and boards
│   ├── [...]
│   ├── extensible                                                                     Flash layout files for microSD card boot device with no userfs partition but a rootfs partition extended to microSD card size
│   │   ├── FlashLayout_sdcard_<board name>-<hardware security>-extensible.tsv         (recommended setup for package repository service) microSD card boot device with rootfs partition extended to microSD card size
│   │   └── [...]
│   ├── fastboot                                                                       Flash layout files for flashing via fastboot with optee boot chain
│   │   ├── FlashLayout_<boot device>_<board name>-<hardware security>-fastboot.tsv   
│   │   └── [...]
│   ├── fastboot-opteemin                                                              Flash layout files for flashing via fastboot with opteemin boot chain
│   │   ├── FlashLayout_<boot device>_<board name>-<hardware security>-fastboot-opteemin.tsv   
│   │   └── [...]
│   ├── optee                                                                          Flash layout files for optee boot chain
│   │   ├── FlashLayout_<boot device>_<board name>-<hardware security>-optee.tsv
│   │   └── [...]
│   └── opteemin                                                                       Flash layout files for opteemin boot chain
│       ├── FlashLayout_<boot device>_<board name>-<hardware security>-opteemin.tsv
│       └── [...]
├── Kernel                                                                             Debug binaries for Linux kernel
│   ├── config-6.6.78                                                              Reference config file for Linux kernel
│   └── vmlinux                                                                        Image of the Linux kernel
├── optee                                                                              OPTEE-OS binaries
│   ├── debug                                                                          Debug binaries for OPTEE-OS
│   │   ├── tee-<board name>-<hardware security>-<boot chain>.elf                      Debug symbol file for OPTEE-OS
│   │   ├── tee-<board name>-<hardware security>-<boot chain>-programmer.elf           Debug symbol file for OPTEE-OS configured for usb/serial
│   │   └── [...]
│   ├── tee-header_v2-<board name>-<hardware security>-<boot chain>.bin              OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-header_v2-<board name>-<hardware security>-<boot chain>-programmer.bin   OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pageable_v2-<board name>-<hardware security>-<boot chain>.bin            OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pageable_v2-<board name>-<hardware security>-<boot chain>-programmer.bin OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   ├── tee-pager_v2-<board name>-<hardware security>-<boot chain>.bin               OPTEE-OS binary for FIP binaries creation (FIP partition)
│   ├── tee-pager_v2-<board name>-<hardware security>-<boot chain>-programmer.bin    OPTEE-OS binary for FIP binaries creation (FIP-BOOT partition)
│   └── [...]
├── scripts
│   └── create_sdcard_from_flashlayout.sh
├── u-boot                                                                             U-BOOT binaries
│   ├── debug                                                                          Debug binaries for U-BOOT
│   │   ├── u-boot-<soc name>-<u-boot config>.elf                                      Debug symbol file for U-BOOT
│   │   └── [...]
│   ├── configuration-<soc name>-<u-boot config>_defconfig                             Reference configuration file for U-Boot
│   ├── u-boot-nodtb-<soc name>-<u-boot config>.bin                                  U-BOOT binary for FIP binaries creation
│   ├── u-boot-<board name>-<hardware security>-<u-boot config>.dtb                    U-BOOT device tree for FIP binaries creation
│   └── [...]
├── st-image-bootfs-openstlinux-weston-stm32mp2.bootfs.ext4                            Binary for bootfs partition on eMMC and microSD card devices
├── st-image-bootfs-openstlinux-weston-stm32mp2.bootfs.manifest
├── st-image-bootfs-efi-openstlinux-weston-stm32mp2.bootfs.vfat                        Binary for bootfs for EFI partition on eMMC and microSD card devices
├── st-image-bootfs-efi-openstlinux-weston-stm32mp2.bootfs.manifest
├── st-image-userfs-openstlinux-weston-stm32mp2.userfs.ext4                            Binary for userfs partition on eMMC and microSD card devices
├── st-image-userfs-openstlinux-weston-stm32mp2.userfs.manifest
├── st-image-vendorfs-openstlinux-weston-stm32mp2.vendorfs.ext4                        Binary for vendorfs partition on eMMC and microSD card devices
├── st-image-vendorfs-openstlinux-weston-stm32mp2.vendorfs.manifest
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs.ext4                            Binary for rootfs partition on eMMC and microSD card devices
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs.license
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs-license_content.html            License summary for all packages needed to feed all partitions
├── st-image-weston-openstlinux-weston-stm32mp2.rootfs.manifest
└── [...]

Description:

<soc name>:
* stm32mp21
* stm32mp23
* stm32mp25
<board name>:
* stm32mp215-df, stm32mp235f-dk, stm32mp257f-dk, stm32mp257f-ev1
<hardware security>:
* if nothing declared then there is a minimal hardware configuration for RIFF profile OPEN
* ca35tdcid-ostl                 custom hardware configuration (can be different following use-case and hardware) for RIFF profile  CUSTOM (CLOSED)
* ca35tdcid-ostl-m33-examples    custom hardware configuration (can be different following use-case and hardware) for RIFF profile CUSTOM (CLOSED)
<boot chain>:
* fastboot                  optee boot chain for flashing via fastboot
* fastboot-opteemin         opteemin boot chain for flashing via fastboot
* optee                     optee boot chain
* opteemin                  opteemin boot chain
<storage>:
* emmc                            eMMC storage
* nand                            NAND storage
* nor                             NOR storage
* programmer-uart                 storage programmation via UART
* programmer-usb                  storage programmation via USB
* sdcard                          microSD card storage
<boot device>:
* emmc                            boot via emmc storage
* nand-4-256-1024 (nand-x-y-z)    boot via nand storage
* nand-4-256-1024-sdcard          boot via nand storage for first stage (fsbl, fip) and files system are located on sdcard
* nor                             boot via nor storage
* nor-sdcard                      boot via nor storage for first stage (fsbl, fip) and files system are located on sdcard
* sdcard                          boot via sdcard storage
* sdcard-EFI                      boot via sdcard but bootfs is configurated on EFI
<u-boot config>:
* default
* fastboot-emmc             Fastboot config enabled with MMC_DEV Id for emmc
* fastboot-sdcard           Fastboot config enabled with MMC_DEV Id for sdcard
* programmer                Programmer config enabled


For M33-TD flavor More info green.png


7. Populate the SDCard[edit | edit source]

  • Set the boot switches (located at the back of the board) to the off position
boot switches position to flash the board
  • Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the STM32MP157C-DK2 board
  • Power up the board
  • Press the reset button to reset the board
  • Launch STM32CubeProgrammer to get the GUI
  • On the right, select USB (not STLINK, set by default) in the connection picklist and click on "Refresh" button. Serial Number is displayed if USB is detected. Click on "Connect"
  • Select "Open File" tab and select $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.x.0/stm32mp1-openstlinux-xx-yy-zz/images/stm32mp1/flashlayout_st-image-weston the FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv, in the Starter Package installation folder.
  • Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1
  • Click on "Download" to start the flashing process.
  • Progress is displayed with progress bar till completion popup message.

8. Boot the board[edit | edit source]

  • Set the boot switches (located at the back of the board) to the ON position
boot switches position to boot the board
  • Power up the board
  • Press the "Reset "button to reset the board
  • After few seconds, the board starts and automatically goes through the following screens
UBoot splash screen
Linux splash screen
Weston desktop
GTK demo launcher
  • If the board power supply doesn't supply enough current (3A), the red LED indicates the issue following the rules below:
blink console message boot process
2 times WARNING 500mA power supply detected

Current too low, use a 3A power supply!

Continue and red LED stays ON
3 times WARNING 1500mA power supply detected

Current too low, use a 3A power supply!

Continue and red LED stays ON
forever ERROR USB TYPE-C connection in unattached mode

Check that USB TYPE-C cable is correctly plugged

stop
forever USB TYPE-C charger not compliant with USB specification stop